<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Remove login prompt in Yocto kernel build in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Remove-login-prompt-in-Yocto-kernel-build/m-p/392853#M57347</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to figure out how to disable the following login prompt after the kernel boots:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Poky (Yocto Project Reference Distro) 1.8.1 nitrogen6x /dev/ttymxc3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; nitrogen6x login:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the LTIB environment (L3.0.35_4.1.0), there was an option in the LTIB configuration to disable the login prompt:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LTIB configuration -&amp;gt; Options -&amp;gt; [ ] boot up with a tty and login&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;I'm looking to do the same in the Yocto environment. The point of this is for an application to autolaunch after the kernel boots. I did that in the LTIB environment by disabling the login prompt and launching the application through rc.local. I'm using kernel 3.14.28 with an imx6q processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Nov 2015 21:06:55 GMT</pubDate>
    <dc:creator>aznjaput</dc:creator>
    <dc:date>2015-11-06T21:06:55Z</dc:date>
    <item>
      <title>Remove login prompt in Yocto kernel build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Remove-login-prompt-in-Yocto-kernel-build/m-p/392853#M57347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to figure out how to disable the following login prompt after the kernel boots:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Poky (Yocto Project Reference Distro) 1.8.1 nitrogen6x /dev/ttymxc3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; nitrogen6x login:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the LTIB environment (L3.0.35_4.1.0), there was an option in the LTIB configuration to disable the login prompt:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LTIB configuration -&amp;gt; Options -&amp;gt; [ ] boot up with a tty and login&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;I'm looking to do the same in the Yocto environment. The point of this is for an application to autolaunch after the kernel boots. I did that in the LTIB environment by disabling the login prompt and launching the application through rc.local. I'm using kernel 3.14.28 with an imx6q processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Nov 2015 21:06:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Remove-login-prompt-in-Yocto-kernel-build/m-p/392853#M57347</guid>
      <dc:creator>aznjaput</dc:creator>
      <dc:date>2015-11-06T21:06:55Z</dc:date>
    </item>
    <item>
      <title>Re: Remove login prompt in Yocto kernel build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Remove-login-prompt-in-Yocto-kernel-build/m-p/392854#M57348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Solution for this is posted at:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/317656"&gt;Reg: Auto-Login and run a script Automatically&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Nov 2015 04:16:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Remove-login-prompt-in-Yocto-kernel-build/m-p/392854#M57348</guid>
      <dc:creator>aznjaput</dc:creator>
      <dc:date>2015-11-16T04:16:04Z</dc:date>
    </item>
  </channel>
</rss>