<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックYocto openssh</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-openssh/m-p/392367#M57274</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I'm working with Yocto fsl-relese-bsp.&lt;/P&gt;&lt;P&gt;I'm baking fsl-image-qt5, and I added the ssh-server-openssh EXTRA_IMAGE_FEATURES to the recipe.&lt;/P&gt;&lt;P&gt;The bitbake worked well, but after the startup the root user ask me for a password.&lt;/P&gt;&lt;P&gt;Before adding ssh-server-openssh the root password was empty.&lt;/P&gt;&lt;P&gt;What is the standard password for this package?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 May 2015 15:25:21 GMT</pubDate>
    <dc:creator>LPs</dc:creator>
    <dc:date>2015-05-25T15:25:21Z</dc:date>
    <item>
      <title>Yocto openssh</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-openssh/m-p/392367#M57274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I'm working with Yocto fsl-relese-bsp.&lt;/P&gt;&lt;P&gt;I'm baking fsl-image-qt5, and I added the ssh-server-openssh EXTRA_IMAGE_FEATURES to the recipe.&lt;/P&gt;&lt;P&gt;The bitbake worked well, but after the startup the root user ask me for a password.&lt;/P&gt;&lt;P&gt;Before adding ssh-server-openssh the root password was empty.&lt;/P&gt;&lt;P&gt;What is the standard password for this package?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 May 2015 15:25:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-openssh/m-p/392367#M57274</guid>
      <dc:creator>LPs</dc:creator>
      <dc:date>2015-05-25T15:25:21Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto openssh</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-openssh/m-p/392368#M57275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello LPs,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may find useful to see the EXTRA_IMAGE_FEATURES section on the Yocto reference manual (link below). Especially the debug-tweaks feature which sets the ssh root access to a blank password.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.yoctoproject.org/docs/1.7/ref-manual/ref-manual.html#var-EXTRA_IMAGE_FEATURES"&gt;http://www.yoctoproject.org/docs/1.7/ref-manual/ref-manual.html#var-EXTRA_IMAGE_FEATURES&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you’re looking for a more permanent solution you should patch the source code to add the desired username and password.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2015 15:25:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-openssh/m-p/392368#M57275</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-06-02T15:25:14Z</dc:date>
    </item>
  </channel>
</rss>