<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCIe endpoint driver with DMA support in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-endpoint-driver-with-DMA-support/m-p/392244#M57217</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class="x_MsoNormal"&gt;Hi,&lt;/P&gt;&lt;P class="x_MsoNormal"&gt;&lt;/P&gt;&lt;P class="x_MsoNormal"&gt;Is i.mx6 quad validated with PCIe end point mode in Linux? Is DMA implementation already available for PCIe end point?&lt;/P&gt;&lt;P class="x_MsoNormal"&gt;We have a high throughput requirement (output 720P30, YUV422) over PCIe. Will i.mx6 quad be sufficient enough to do so?&lt;/P&gt;&lt;P class="x_MsoNormal"&gt;&lt;/P&gt;&lt;P class="x_MsoNormal"&gt;Thanks and Regards,&lt;/P&gt;&lt;P class="x_MsoNormal"&gt;Shabbir&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Jun 2015 13:14:49 GMT</pubDate>
    <dc:creator>shabbirlimdiwal</dc:creator>
    <dc:date>2015-06-11T13:14:49Z</dc:date>
    <item>
      <title>PCIe endpoint driver with DMA support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-endpoint-driver-with-DMA-support/m-p/392244#M57217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class="x_MsoNormal"&gt;Hi,&lt;/P&gt;&lt;P class="x_MsoNormal"&gt;&lt;/P&gt;&lt;P class="x_MsoNormal"&gt;Is i.mx6 quad validated with PCIe end point mode in Linux? Is DMA implementation already available for PCIe end point?&lt;/P&gt;&lt;P class="x_MsoNormal"&gt;We have a high throughput requirement (output 720P30, YUV422) over PCIe. Will i.mx6 quad be sufficient enough to do so?&lt;/P&gt;&lt;P class="x_MsoNormal"&gt;&lt;/P&gt;&lt;P class="x_MsoNormal"&gt;Thanks and Regards,&lt;/P&gt;&lt;P class="x_MsoNormal"&gt;Shabbir&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2015 13:14:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-endpoint-driver-with-DMA-support/m-p/392244#M57217</guid>
      <dc:creator>shabbirlimdiwal</dc:creator>
      <dc:date>2015-06-11T13:14:49Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe endpoint driver with DMA support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-endpoint-driver-with-DMA-support/m-p/392245#M57218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shabbir&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes it is validated&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95014"&gt;i.MX6Q PCIe EP/RC Validation System&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please also check attached document sect.35.5 i.MX 6Quad SD PCIe RC/EP Validation System&lt;/P&gt;&lt;P&gt;included in &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.0.35_4.1.0_ER_SOURCE_BSP&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jun 2015 02:56:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-endpoint-driver-with-DMA-support/m-p/392245#M57218</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-12T02:56:58Z</dc:date>
    </item>
  </channel>
</rss>