<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCustom Imx6 + Qt5 and GUI application warnings</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Custom-Imx6-Qt5-and-GUI-application-warnings/m-p/391916#M57156</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom imx6 board loaded with Freescale's fsl-image-qt5 and for application development I'm using Qt Creator (Qt 5.2.1) on Ubuntu 14.04. When I make a GUI application and run it on the custom board from Qt Creator on my desktop I get the following warnings:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ML debugging is enabled. Only use this in a safe environment.&lt;/P&gt;&lt;P&gt;Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.&lt;/P&gt;&lt;P&gt;Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.&lt;/P&gt;&lt;P&gt;file:///root/qml/untitled1/main.qml: File not found &lt;/P&gt;&lt;P&gt;Warning: EGL suggested using X Visual ID 33 (RGB565) for EGL config 5 (RGB444), but this is incompatable&lt;/P&gt;&lt;P&gt;Unable to find an X11 visual which matches EGL config 5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have no idea where to start on this and have Googled for a few hours so any advice would be appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Oct 2015 21:51:01 GMT</pubDate>
    <dc:creator>edwardtyrrell</dc:creator>
    <dc:date>2015-10-12T21:51:01Z</dc:date>
    <item>
      <title>Custom Imx6 + Qt5 and GUI application warnings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-Imx6-Qt5-and-GUI-application-warnings/m-p/391916#M57156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom imx6 board loaded with Freescale's fsl-image-qt5 and for application development I'm using Qt Creator (Qt 5.2.1) on Ubuntu 14.04. When I make a GUI application and run it on the custom board from Qt Creator on my desktop I get the following warnings:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ML debugging is enabled. Only use this in a safe environment.&lt;/P&gt;&lt;P&gt;Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.&lt;/P&gt;&lt;P&gt;Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.&lt;/P&gt;&lt;P&gt;file:///root/qml/untitled1/main.qml: File not found &lt;/P&gt;&lt;P&gt;Warning: EGL suggested using X Visual ID 33 (RGB565) for EGL config 5 (RGB444), but this is incompatable&lt;/P&gt;&lt;P&gt;Unable to find an X11 visual which matches EGL config 5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have no idea where to start on this and have Googled for a few hours so any advice would be appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Oct 2015 21:51:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-Imx6-Qt5-and-GUI-application-warnings/m-p/391916#M57156</guid>
      <dc:creator>edwardtyrrell</dc:creator>
      <dc:date>2015-10-12T21:51:01Z</dc:date>
    </item>
    <item>
      <title>Re: Custom Imx6 + Qt5 and GUI application warnings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-Imx6-Qt5-and-GUI-application-warnings/m-p/391917#M57157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;It may be useful to apply to QT experts.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Nevertheless, below is some link, which – hope – can help.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;A class="jive-link-external-small" href="https://mail-index.netbsd.org/pkgsrc-bugs/2014/01/26/msg053405.html" rel="nofollow"&gt;https://mail-index.netbsd.org/pkgsrc-bugs/2014/01/26/msg053405.html&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Oct 2015 07:09:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-Imx6-Qt5-and-GUI-application-warnings/m-p/391917#M57157</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-10-26T07:09:47Z</dc:date>
    </item>
  </channel>
</rss>