<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCan CAAM be used at user level using /dev/crypto in linux? if yes, how to create blob at user level?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-CAAM-be-used-at-user-level-using-dev-crypto-in-linux-if-yes/m-p/391598#M57099</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are three queries.&lt;/P&gt;&lt;P&gt;1. Linux has support for /dev/crypto i.e. cryptodev feature with which hardware accelerators can be accessed at user level. Is same thing possible for CAAM?&lt;/P&gt;&lt;P&gt;2. If yes, is there any demo code available to create encapsulated blob? and is it possible to modify keys at CAAM register level.&lt;/P&gt;&lt;P&gt;3. Are all the algorithms supported by CAAM available at user space library like openSSL?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using Yocto project Daisy with kernel 3.10.17 on wandboard-quad. I can see CAAM algorithms available in /proc/crypto. please refer attached output.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Oct 2015 19:05:33 GMT</pubDate>
    <dc:creator>swapnilpendhare</dc:creator>
    <dc:date>2015-10-13T19:05:33Z</dc:date>
    <item>
      <title>Can CAAM be used at user level using /dev/crypto in linux? if yes, how to create blob at user level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-CAAM-be-used-at-user-level-using-dev-crypto-in-linux-if-yes/m-p/391598#M57099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are three queries.&lt;/P&gt;&lt;P&gt;1. Linux has support for /dev/crypto i.e. cryptodev feature with which hardware accelerators can be accessed at user level. Is same thing possible for CAAM?&lt;/P&gt;&lt;P&gt;2. If yes, is there any demo code available to create encapsulated blob? and is it possible to modify keys at CAAM register level.&lt;/P&gt;&lt;P&gt;3. Are all the algorithms supported by CAAM available at user space library like openSSL?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using Yocto project Daisy with kernel 3.10.17 on wandboard-quad. I can see CAAM algorithms available in /proc/crypto. please refer attached output.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Oct 2015 19:05:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-CAAM-be-used-at-user-level-using-dev-crypto-in-linux-if-yes/m-p/391598#M57099</guid>
      <dc:creator>swapnilpendhare</dc:creator>
      <dc:date>2015-10-13T19:05:33Z</dc:date>
    </item>
    <item>
      <title>Re: Can CAAM be used at user level using /dev/crypto in linux? if yes, how to create blob at user level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-CAAM-be-used-at-user-level-using-dev-crypto-in-linux-if-yes/m-p/391599#M57100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp;&amp;nbsp; Please refer to section 9 (Security) of “i.MX_Linux_User's_Guide.pdf”.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;“The CAAM drivers are accelerated through the CryptoDev interface”.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; For blob, please use U-boot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 03:26:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-CAAM-be-used-at-user-level-using-dev-crypto-in-linux-if-yes/m-p/391599#M57100</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-10-14T03:26:05Z</dc:date>
    </item>
    <item>
      <title>Re: Can CAAM be used at user level using /dev/crypto in linux? if yes, how to create blob at user level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-CAAM-be-used-at-user-level-using-dev-crypto-in-linux-if-yes/m-p/391600#M57101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi , &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply. I am looking for develop General blob write/read operation in linux; something like &lt;A href="https://community.nxp.com/thread/309852"&gt;How to Create Blob&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;As mentioned in the mentioned link, it can be done through platform SDK only. Is it possible to do same thing from linux user pace. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and second query is,&lt;/P&gt;&lt;P&gt;link &lt;SPAN style="color: #017bba; font-weight: inherit; font-family: inherit; font-style: inherit;"&gt;Page not found&lt;/SPAN&gt; ​mentioned in post&amp;nbsp;&amp;nbsp; &lt;A href="https://community.nxp.com/thread/343151"&gt;iMX6 (CAAM, TrustZone) Hardware Security Blocks Use.&lt;/A&gt; is not accessible. Can you provide more details on this. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Oct 2015 14:56:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-CAAM-be-used-at-user-level-using-dev-crypto-in-linux-if-yes/m-p/391600#M57101</guid>
      <dc:creator>swapnilpendhare</dc:creator>
      <dc:date>2015-10-18T14:56:23Z</dc:date>
    </item>
    <item>
      <title>Re: Can CAAM be used at user level using /dev/crypto in linux? if yes, how to create blob at user level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-CAAM-be-used-at-user-level-using-dev-crypto-in-linux-if-yes/m-p/391601#M57102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please use section 52.5 (API Interface Level) of the "i.MX_Linux_Reference_Manual.pdf".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/Download?colCode=L3.14.38_6UL_LINUX_DOCS" title="http://www.freescale.com/webapp/Download?colCode=L3.14.38_6UL_LINUX_DOCS"&gt;http://www.freescale.com/webapp/Download?colCode=L3.14.38_6UL_LINUX_DOCS&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; Please refer to Encrypted Boot explanations in “HABCST_UG.pdf” of the CST.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx-software-and-tools/i.mx-design-tools:IMX_DESIGN" rel="nofollow"&gt;http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx-software-and-tools/i.mx-design-tools:IMX_DESIGN&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Oct 2015 03:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-CAAM-be-used-at-user-level-using-dev-crypto-in-linux-if-yes/m-p/391601#M57102</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-10-19T03:57:18Z</dc:date>
    </item>
  </channel>
</rss>