<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6dl boot source</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6dl-boot-source/m-p/390705#M56875</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With imx6, is there any possibility to check from which interface ROM loaded boot stream ?&lt;/P&gt;&lt;P&gt;I need to know in u-boot from which device it was loaded.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;AK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jan 2015 15:38:15 GMT</pubDate>
    <dc:creator>arkadiuszkaras</dc:creator>
    <dc:date>2015-01-07T15:38:15Z</dc:date>
    <item>
      <title>imx6dl boot source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6dl-boot-source/m-p/390705#M56875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With imx6, is there any possibility to check from which interface ROM loaded boot stream ?&lt;/P&gt;&lt;P&gt;I need to know in u-boot from which device it was loaded.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;AK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 15:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6dl-boot-source/m-p/390705#M56875</guid>
      <dc:creator>arkadiuszkaras</dc:creator>
      <dc:date>2015-01-07T15:38:15Z</dc:date>
    </item>
    <item>
      <title>Re: imx6dl boot source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6dl-boot-source/m-p/390706#M56876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arkadiusz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, this could be done using &lt;/P&gt;&lt;P&gt;SRC Boot Mode Register 1 (SRC_SBMR1,2)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jan 2015 00:47:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6dl-boot-source/m-p/390706#M56876</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-08T00:47:59Z</dc:date>
    </item>
  </channel>
</rss>