<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Last frame freezing while streaming video</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Last-frame-freezing-while-streaming-video/m-p/390308#M56798</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you please share the commands/bootargs that you are applying for configuring the clone screens?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;/Carlos.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Dec 2014 18:26:42 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2014-12-15T18:26:42Z</dc:date>
    <item>
      <title>Last frame freezing while streaming video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Last-frame-freezing-while-streaming-video/m-p/390305#M56795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am working on a project which is based on i.MX6Q board . It has a camera module which is on MIPI CSI2 interface .&lt;/P&gt;&lt;P&gt;When i stream a video using gstreamer command the last frame is freezing when i use CTRL+C to terminate the streaming.&lt;/P&gt;&lt;P&gt;when i use mfw_vl4sink with device=/dev/video17 it's working fine but when i change it to video16 or video18 or video19 it freezes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gst-launch mfw_v4lsrc device=/dev/video1 capture-mode=4&amp;nbsp; ! mfw_v4lsink device=/dev/video17 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And also we want to display a video on LCD and HDMI both using a single source using gstreamer command.In that case also it not clearing the last frame of buffer.&lt;/P&gt;&lt;P&gt;Some where in source code of vl4_sink it's given to clear it using system("cat /dev/zero &amp;gt; /dev/fb2\n"); but still not able to get it done.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Command for multi display(LCD+HDMI)&lt;/P&gt;&lt;P&gt;gst-launch mfw_v4lsrc device=/dev/video1 capture-mode=4 ! tee name=splitter ! queue ! mfw_v4lsink device=/dev/video17 splitter. ! queue ! mfw_v4lsink device=/dev/video18 &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Dec 2014 10:17:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Last-frame-freezing-while-streaming-video/m-p/390305#M56795</guid>
      <dc:creator>Subodh_K</dc:creator>
      <dc:date>2014-12-04T10:17:35Z</dc:date>
    </item>
    <item>
      <title>Re: Last frame freezing while streaming video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Last-frame-freezing-while-streaming-video/m-p/390306#M56796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, could you please specify which board and BSP are you using in order to try to recreate your issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;/Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Dec 2014 23:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Last-frame-freezing-while-streaming-video/m-p/390306#M56796</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2014-12-09T23:01:55Z</dc:date>
    </item>
    <item>
      <title>Re: Last frame freezing while streaming video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Last-frame-freezing-while-streaming-video/m-p/390307#M56797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;I am using imx6Q sabresd board and kernel version is 3.10-17 of Yocto 1.6 daisy branch&amp;nbsp; SDK.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Dec 2014 04:11:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Last-frame-freezing-while-streaming-video/m-p/390307#M56797</guid>
      <dc:creator>Subodh_K</dc:creator>
      <dc:date>2014-12-10T04:11:59Z</dc:date>
    </item>
    <item>
      <title>Re: Last frame freezing while streaming video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Last-frame-freezing-while-streaming-video/m-p/390308#M56798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you please share the commands/bootargs that you are applying for configuring the clone screens?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;/Carlos.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Dec 2014 18:26:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Last-frame-freezing-while-streaming-video/m-p/390308#M56798</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2014-12-15T18:26:42Z</dc:date>
    </item>
    <item>
      <title>Re: Last frame freezing while streaming video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Last-frame-freezing-while-streaming-video/m-p/390309#M56799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have internally discussed this case with our experts, and they say that video18 is BG, frame buffer is default open, you need to turn of it manually with: echo 1 &amp;gt; /sys/class/graphics/fb0/blank&lt;/P&gt;&lt;P&gt;Or you can show second video to /dev/video19, which is the FG, will turn off when close v4l2 device, but this is the overlay, performance is worse than video18.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Dec 2014 16:50:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Last-frame-freezing-while-streaming-video/m-p/390309#M56799</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2014-12-19T16:50:52Z</dc:date>
    </item>
  </channel>
</rss>