<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: sb_loader error(-13) during download</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/sb-loader-error-13-during-download/m-p/389993#M56755</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Javier&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you should check how generated karo uboot.bin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;elftosb can generate encrypted and not encrypted image, this depends&lt;/P&gt;&lt;P&gt;what fuses are blown on chip. You can compare fuses on KARO board&lt;/P&gt;&lt;P&gt;with own using &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;IMX_OBDS&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt;&amp;nbsp; (running stmp_otp.c example with jtag).&lt;/P&gt;&lt;P&gt;The output boot image is by default not encrypted. To encrypt the boot image&lt;/P&gt;&lt;P&gt;you need to provide one or more keys. Use the -z switch to add a&lt;/P&gt;&lt;P&gt;key that consists of all zeroes. This is the default state of the hardware key in&lt;/P&gt;&lt;P&gt;a chip that has not yet had its OTP key burned.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Oct 2014 12:33:51 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-10-14T12:33:51Z</dc:date>
    <item>
      <title>sb_loader error(-13) during download</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sb-loader-error-13-during-download/m-p/389990#M56752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm developing a new board based on the IMX287.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to load the u-boot from the KARO startekit-5 V3 (my design is based in this board) with the provided sb_loader executable and I get the following output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking for a STMP HID device for 10 seconds...&lt;/P&gt;&lt;P&gt;&amp;nbsp; Found USB#VID_15A2&amp;amp;PID_004F#7&amp;amp;2EE36394&amp;amp;0&amp;amp;3.&lt;/P&gt;&lt;P&gt;Downloading uboot.bin to device.&lt;/P&gt;&lt;P&gt;&amp;nbsp; .&amp;nbsp; Error(-13) during download.&lt;/P&gt;&lt;P&gt;Quitting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know what I am doing wrong? Any clue about that error?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Oct 2014 10:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sb-loader-error-13-during-download/m-p/389990#M56752</guid>
      <dc:creator>jrrguzman</dc:creator>
      <dc:date>2014-10-14T10:45:19Z</dc:date>
    </item>
    <item>
      <title>Re: sb_loader error(-13) during download</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sb-loader-error-13-during-download/m-p/389991#M56753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Javier&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sb_loader needs *.sb file (generated by elftosb utility), for example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sb_loader.exe /f imx28_uboot.sb&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check sect.5.3.1 USB Boot attached doc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;IMX_ELFTOSB_TOOL&lt;/A&gt;: Tool to convert ELF format executable files and other source files&lt;/P&gt;&lt;P&gt;into the encrypted boot images used by the i.MX23 and i.MX28. Includes Windows&lt;/P&gt;&lt;P&gt;and Linux binaries, full source code, and all related documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Oct 2014 11:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sb-loader-error-13-during-download/m-p/389991#M56753</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-14T11:58:55Z</dc:date>
    </item>
    <item>
      <title>Re: sb_loader error(-13) during download</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sb-loader-error-13-during-download/m-p/389992#M56754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is how I call sb_loader:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;sb_loader.exe /F uboot.bin&lt;/P&gt;&lt;P&gt;Looking for a STMP HID device for 10 seconds...&lt;/P&gt;&lt;P&gt;&amp;nbsp; Found USB#VID_15A2&amp;amp;PID_004F#7&amp;amp;2EE36394&amp;amp;0&amp;amp;3.&lt;/P&gt;&lt;P&gt;Downloading uboot.bin to device.&lt;/P&gt;&lt;P&gt;&amp;nbsp; .&amp;nbsp; Error(-13) during download.&lt;/P&gt;&lt;P&gt;Quitting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to load the image in the KARO board, it works without problems. But I can't make it work with my own board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll try with the .sb extension but I don't think I'll get anything different.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Oct 2014 12:05:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sb-loader-error-13-during-download/m-p/389992#M56754</guid>
      <dc:creator>jrrguzman</dc:creator>
      <dc:date>2014-10-14T12:05:58Z</dc:date>
    </item>
    <item>
      <title>Re: sb_loader error(-13) during download</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sb-loader-error-13-during-download/m-p/389993#M56755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Javier&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you should check how generated karo uboot.bin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;elftosb can generate encrypted and not encrypted image, this depends&lt;/P&gt;&lt;P&gt;what fuses are blown on chip. You can compare fuses on KARO board&lt;/P&gt;&lt;P&gt;with own using &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;IMX_OBDS&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt;&amp;nbsp; (running stmp_otp.c example with jtag).&lt;/P&gt;&lt;P&gt;The output boot image is by default not encrypted. To encrypt the boot image&lt;/P&gt;&lt;P&gt;you need to provide one or more keys. Use the -z switch to add a&lt;/P&gt;&lt;P&gt;key that consists of all zeroes. This is the default state of the hardware key in&lt;/P&gt;&lt;P&gt;a chip that has not yet had its OTP key burned.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Oct 2014 12:33:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sb-loader-error-13-during-download/m-p/389993#M56755</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-14T12:33:51Z</dc:date>
    </item>
  </channel>
</rss>