<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: problem with booting</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-booting/m-p/389871#M56728</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I now everything works. the problem was one way to memory. I would like to ask if there is any simple program to test the external RAM memory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Oct 2014 08:40:51 GMT</pubDate>
    <dc:creator>mistrlukáš</dc:creator>
    <dc:date>2014-10-29T08:40:51Z</dc:date>
    <item>
      <title>problem with booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-booting/m-p/389867#M56724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I made my own board and I can run Linux on it from sdcard. I tried SD card that works well on the board Olinuxino-maxi, but when testing on my board is not working and will output: (Arch Linux 2.6.35.8&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46740i91178B5AED6B013C/image-size/large?v=v2&amp;amp;px=999" title="Archlinux2.6.35-8.jpg" alt="Archlinux2.6.35-8.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I then tried Linux created using pages &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://archlinuxarm.org/platforms/armv5/olinuxino"&gt;http://archlinuxarm.org/platforms/armv5/olinuxino&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;which is the output&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46741i7B288DE8520E0EF8/image-size/large?v=v2&amp;amp;px=999" title="Archlinux 3.jpg" alt="Archlinux 3.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you give me some advice?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Oct 2014 12:04:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problem-with-booting/m-p/389867#M56724</guid>
      <dc:creator>mistrlukáš</dc:creator>
      <dc:date>2014-10-14T12:04:48Z</dc:date>
    </item>
    <item>
      <title>Re: problem with booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-booting/m-p/389868#M56725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mistr&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest to check sources for "SD card that works well on the board&lt;/P&gt;&lt;P&gt;Olinuxino-maxi" and add debug prinfs to bootlets, this will give you place in&lt;/P&gt;&lt;P&gt;program where brownout occured. Also recommended to check schematic - it&lt;/P&gt;&lt;P&gt;should strictly follow schematic for which this image was generated.&lt;/P&gt;&lt;P&gt;Since PMU is fully programmable module, some settings may be changed&lt;/P&gt;&lt;P&gt;for new board. Also if another DDR used, then use tool below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/341487"&gt;Re: i.mx28 u-boot dram configuration for dram replacement.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Oct 2014 03:53:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problem-with-booting/m-p/389868#M56725</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-15T03:53:25Z</dc:date>
    </item>
    <item>
      <title>Re: problem with booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-booting/m-p/389869#M56726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Arial, Helvetica, sans-serif; background-color: #f0f4f7;"&gt;I have now solved the problems with the board and found problems with the power supply.&amp;nbsp; Otherwise I have two different systems and they stuck me in the following steps.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Arial, Helvetica, sans-serif; background-color: #f0f4f7;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Arial, Helvetica, sans-serif; background-color: #f0f4f7;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47090i9634813A4073C46B/image-size/large?v=v2&amp;amp;px=999" title="Archlinux 3.16.3-1-2.jpg" alt="Archlinux 3.16.3-1-2.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Arial, Helvetica, sans-serif; background-color: #f0f4f7;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Arial, Helvetica, sans-serif; background-color: #f0f4f7;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47091iEB3444CF46267BBB/image-size/large?v=v2&amp;amp;px=999" title="Archlinux2.6.35-8-2.jpg" alt="Archlinux2.6.35-8-2.jpg" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Oct 2014 09:15:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problem-with-booting/m-p/389869#M56726</guid>
      <dc:creator>mistrlukáš</dc:creator>
      <dc:date>2014-10-27T09:15:53Z</dc:date>
    </item>
    <item>
      <title>Re: problem with booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-booting/m-p/389870#M56727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When enabled, the ROM will output a single character on the debug UART &lt;/P&gt;&lt;P&gt;for every boot command it executes, with no whitespace between characters. &lt;/P&gt;&lt;P&gt;See the table below for the characters output for each command. &lt;/P&gt;&lt;P&gt;The result of a successful boot looks something like "LLFLLLJ".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Char&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Command&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Notes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;J&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Jump&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; After a jump, the application that was jumped to can re-use &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; the memory in on-chip RAM (which ROM was using), since ROM will not &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; expect this application to return.&amp;nbsp; This is the key difference between a Call and a Jump, &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; the ROM expects an application that was called to return.&lt;/P&gt;&lt;P&gt;C&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Call&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ROM expects the application to return. &lt;/P&gt;&lt;P&gt;L&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Load&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;F&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Fill&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;H&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Header&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;T&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Tag&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Tag was encountered while parsing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for power supplies suggest to check&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4199.pdf?fasp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;AN4199&lt;/A&gt; Using the i.MX28 Power Management Unit and Battery Charger&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;IMX28_EVK_DESIGN_FILES_R10&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : i.MX28 EVK Design Files: Hardware Schematics&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Oct 2014 11:26:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problem-with-booting/m-p/389870#M56727</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-27T11:26:52Z</dc:date>
    </item>
    <item>
      <title>Re: problem with booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-booting/m-p/389871#M56728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I now everything works. the problem was one way to memory. I would like to ask if there is any simple program to test the external RAM memory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Oct 2014 08:40:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problem-with-booting/m-p/389871#M56728</guid>
      <dc:creator>mistrlukáš</dc:creator>
      <dc:date>2014-10-29T08:40:51Z</dc:date>
    </item>
    <item>
      <title>Re: problem with booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-booting/m-p/389872#M56729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Uboot has command mtest - simple RAM read/write test.&lt;/P&gt;&lt;P&gt;ddr_test.c in &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;IMX_OBDS&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : On-Board Diagnostic Suit for the i.MX28. &lt;/P&gt;&lt;P&gt;Also below links&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-1455"&gt;Board Bring-up and DDR Initialization Tools&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="321913" data-objecttype="2" href="https://community.nxp.com/message/321913#321913"&gt;https://community.freescale.com/message/321913#321913&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Oct 2014 10:11:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problem-with-booting/m-p/389872#M56729</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-29T10:11:13Z</dc:date>
    </item>
  </channel>
</rss>