<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: EIM Signals and Boot Configuration</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/EIM-Signals-and-Boot-Configuration/m-p/389642#M56656</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Durmuş&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. one can connect them directly to ground&lt;/P&gt;&lt;P&gt;2. if these signals are used as outputs, they can not be grounded.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; They can be pull-ed with resistor. You may wish to look at&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sect.4.6.2 "General Purpose I/O (GPIO) DC Parameters" &lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQCEC&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Aug 2014 06:50:43 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-08-29T06:50:43Z</dc:date>
    <item>
      <title>EIM Signals and Boot Configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-Signals-and-Boot-Configuration/m-p/389641#M56655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In our design based on SABRE SDP, we try to implement 3 configurations for boot selection:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;eMMC via USDHC3&lt;/LI&gt;&lt;LI&gt;external SD/MMC card via USDHC1&lt;/LI&gt;&lt;LI&gt;SPI NOR flash via ECSPI1&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Out of 32 EIM signals related with boot configuration, we are using only 2 in our design, specifically EIM_EB2 (E22) as SPI1_CS0 and EIM_EB3 (F23) as UART1_RI_B.&lt;/P&gt;&lt;P&gt;I already removed the series bus isolation resistors (4.7k) because they are not connected to anywhere, except for those two above. I have 2 questions to make sure what I did is correct:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the reference manual for the related signals for boot selections. When I guarantee that the boot-up process will occur either from USDHC1, USDHC3 or ECSPI1; &lt;/P&gt;&lt;P&gt;1) Do I have to connect other unrelated boot signals to ground via 10k resistors? Or can I connect them directly to ground?&lt;/P&gt;&lt;P&gt;2) Since EIM_EB2 and EIM_EB3 are irrelevant for the mentioned boot selections, do I need any isolation or pull-down for them? (since I'm using them as low active signals, it would not be correct to pull them down)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Durmus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Aug 2014 06:25:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-Signals-and-Boot-Configuration/m-p/389641#M56655</guid>
      <dc:creator>durmus</dc:creator>
      <dc:date>2014-08-29T06:25:05Z</dc:date>
    </item>
    <item>
      <title>Re: EIM Signals and Boot Configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-Signals-and-Boot-Configuration/m-p/389642#M56656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Durmuş&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. one can connect them directly to ground&lt;/P&gt;&lt;P&gt;2. if these signals are used as outputs, they can not be grounded.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; They can be pull-ed with resistor. You may wish to look at&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sect.4.6.2 "General Purpose I/O (GPIO) DC Parameters" &lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQCEC&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Aug 2014 06:50:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-Signals-and-Boot-Configuration/m-p/389642#M56656</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-08-29T06:50:43Z</dc:date>
    </item>
  </channel>
</rss>