<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX28 USB bus powered device with no power switch in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-USB-bus-powered-device-with-no-power-switch/m-p/389465#M56627</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;I'm working on a custom i.mx28 board powered just by external 5v of USB bus. After several bootup starts of u-boot-2011.12 I found out that the system hangs on mx28_power_setup_5v_detect() function. Have you applied different tunings during spl code of u-boot? Could you give me any tips?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Francesco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Sep 2015 13:00:47 GMT</pubDate>
    <dc:creator>francescoluccon</dc:creator>
    <dc:date>2015-09-02T13:00:47Z</dc:date>
    <item>
      <title>i.MX28 USB bus powered device with no power switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-USB-bus-powered-device-with-no-power-switch/m-p/389462#M56624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have planned USB bus powered device using i.MX28.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The product does not have a power switch.&lt;/P&gt;&lt;P&gt;Since it connected with USB-HOST, it begins boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Though we are going to design according to "VDD5V source only" of AN4199, it is not known how we should do a PSWITCH pin.&lt;/P&gt;&lt;P&gt;Is what is necessary just to tied to VDD3V3 or GND?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Nov 2014 02:00:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-USB-bus-powered-device-with-no-power-switch/m-p/389462#M56624</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2014-11-10T02:00:21Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 USB bus powered device with no power switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-USB-bus-powered-device-with-no-power-switch/m-p/389463#M56625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; There is no need for a POWER button in a 5V only configuration. If a&lt;/P&gt;&lt;P&gt;5V source is present on the VDD5V pin, the i.MX device will automatically&lt;/P&gt;&lt;P&gt;power up. In such case the PSWITCH should be pulled down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Nov 2014 02:48:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-USB-bus-powered-device-with-no-power-switch/m-p/389463#M56625</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-11-10T02:48:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 USB bus powered device with no power switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-USB-bus-powered-device-with-no-power-switch/m-p/389464#M56626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thnaks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Nov 2014 03:56:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-USB-bus-powered-device-with-no-power-switch/m-p/389464#M56626</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2014-11-10T03:56:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 USB bus powered device with no power switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-USB-bus-powered-device-with-no-power-switch/m-p/389465#M56627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;I'm working on a custom i.mx28 board powered just by external 5v of USB bus. After several bootup starts of u-boot-2011.12 I found out that the system hangs on mx28_power_setup_5v_detect() function. Have you applied different tunings during spl code of u-boot? Could you give me any tips?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Francesco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 13:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-USB-bus-powered-device-with-no-power-switch/m-p/389465#M56627</guid>
      <dc:creator>francescoluccon</dc:creator>
      <dc:date>2015-09-02T13:00:47Z</dc:date>
    </item>
  </channel>
</rss>