<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックTVE output not working</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/TVE-output-not-working/m-p/171559#M5659</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anyone explain what I have to enable in the linux kernel v2.6.35.3 provided by Freescale to enable video output on TVE?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I've a i.MX53 QSB. Video is working on the VGA connector if I use the provided image on the SD card that was included in the board. I just had to change the boot params to video=mxcdi1fb:GBR24,XGA di1_primary tve&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, I don't use the linux kernel in combination with ltib.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think there must be some enabled options in the kernel support TVE output on the VGA connector, but unfortunately I don't find them...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rooney&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jun 2012 17:50:40 GMT</pubDate>
    <dc:creator>Rooney</dc:creator>
    <dc:date>2012-06-28T17:50:40Z</dc:date>
    <item>
      <title>TVE output not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TVE-output-not-working/m-p/171559#M5659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anyone explain what I have to enable in the linux kernel v2.6.35.3 provided by Freescale to enable video output on TVE?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I've a i.MX53 QSB. Video is working on the VGA connector if I use the provided image on the SD card that was included in the board. I just had to change the boot params to video=mxcdi1fb:GBR24,XGA di1_primary tve&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, I don't use the linux kernel in combination with ltib.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think there must be some enabled options in the kernel support TVE output on the VGA connector, but unfortunately I don't find them...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rooney&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jun 2012 17:50:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TVE-output-not-working/m-p/171559#M5659</guid>
      <dc:creator>Rooney</dc:creator>
      <dc:date>2012-06-28T17:50:40Z</dc:date>
    </item>
    <item>
      <title>Re: TVE output not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TVE-output-not-working/m-p/171560#M5660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;video=mxcdi1fb: YUV444,TV-1080P30 di1_primary tve&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at BSP11.09 Release Notes I found another video parameter to be used with TVE. There is a list of supported resolution as well, please take a look.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you´ve been taking kernel from git.freescale I believe the config file has already TVE enabled by default.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What rootfs do you use? (I´m just curious, I don´t think it matter for you issue)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2012 14:17:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TVE-output-not-working/m-p/171560#M5660</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2012-06-29T14:17:01Z</dc:date>
    </item>
    <item>
      <title>Re: TVE output not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TVE-output-not-working/m-p/171561#M5661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;That works!!! Thanks a lot!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, I'm using Debian Squeeze as rootfs, created with debootstrap.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jul 2012 14:22:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TVE-output-not-working/m-p/171561#M5661</guid>
      <dc:creator>Rooney</dc:creator>
      <dc:date>2012-07-09T14:22:13Z</dc:date>
    </item>
  </channel>
</rss>