<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Multi-display on yocto-linux</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Multi-display-on-yocto-linux/m-p/389027#M56562</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Charles, the fb1 is the overlay, so it can be any resolution, for fb2, it is the main display, so its resolution is fixed, for this case, the mfw_v4lsink can only render in full screen mode. If you want to play video in window mode on main frame buffer, you can use the mfw_isink.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the mfw_isink performance is poor than mfw_v4lsink, because it need combine the video with main frame buffer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Dec 2014 09:36:25 GMT</pubDate>
    <dc:creator>qiang_li-mpu_se</dc:creator>
    <dc:date>2014-12-19T09:36:25Z</dc:date>
    <item>
      <title>Multi-display on yocto-linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multi-display-on-yocto-linux/m-p/389026#M56561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We would like to multi-display on 3 different interface, HDMI、LCD and LVDS&lt;/P&gt;&lt;P&gt;We use this command to play video on specific framebuffer&lt;/P&gt;&lt;P&gt;"gst-launch filesrc location=/test.avi typefind=true ! aiurdemux ! queue ! vpudec ! mfw_v4lsink device=/dev/video16"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We found that if we put lvds on fb1&lt;/P&gt;&lt;P&gt;Using the above-mentioned command, it can play video correctly on specific framebuffer(fb1).&lt;/P&gt;&lt;P&gt;But if we found that if we play video on fb2(hdmi), the video size on fb2 is not correct &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you tell me how to solve this problem?&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Nov 2014 01:13:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multi-display-on-yocto-linux/m-p/389026#M56561</guid>
      <dc:creator>charleshuang</dc:creator>
      <dc:date>2014-11-10T01:13:24Z</dc:date>
    </item>
    <item>
      <title>Re: Multi-display on yocto-linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multi-display-on-yocto-linux/m-p/389027#M56562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Charles, the fb1 is the overlay, so it can be any resolution, for fb2, it is the main display, so its resolution is fixed, for this case, the mfw_v4lsink can only render in full screen mode. If you want to play video in window mode on main frame buffer, you can use the mfw_isink.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the mfw_isink performance is poor than mfw_v4lsink, because it need combine the video with main frame buffer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Dec 2014 09:36:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multi-display-on-yocto-linux/m-p/389027#M56562</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2014-12-19T09:36:25Z</dc:date>
    </item>
  </channel>
</rss>