<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: qt camera in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/qt-camera/m-p/388281#M56405</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you are using the SABRE board, then change your sink Pipeline from&amp;nbsp; imxeglVivsink, since this one use the Vivante GPU module, which it is causing the problem. You can use the mfw_isink: mfw_isink: Freescale: i_sink or something like:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gst-launch v4l2src ! autovideosink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And you can check your camera interface with mxcv4l2 test.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Jan 2015 14:32:49 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2015-01-08T14:32:49Z</dc:date>
    <item>
      <title>qt camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/qt-camera/m-p/388280#M56404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a question. I use the Qt5.3.2 the arm environment is imxSABRE6Q .the GStreamer version is 1.0&amp;nbsp; src：imxv4l2src sink：imxeglvivsink .&lt;/P&gt;&lt;P&gt;&amp;nbsp; 1. when start camera, the screen only a frame .&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2. then I trigger event that the camera stop. Then I again trigger one event ,the camera start working is OK, but after about 30s the screen display video stop .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need some suggestion about it.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jan 2015 08:56:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/qt-camera/m-p/388280#M56404</guid>
      <dc:creator>wangyhwang</dc:creator>
      <dc:date>2015-01-06T08:56:49Z</dc:date>
    </item>
    <item>
      <title>Re: qt camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/qt-camera/m-p/388281#M56405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you are using the SABRE board, then change your sink Pipeline from&amp;nbsp; imxeglVivsink, since this one use the Vivante GPU module, which it is causing the problem. You can use the mfw_isink: mfw_isink: Freescale: i_sink or something like:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gst-launch v4l2src ! autovideosink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And you can check your camera interface with mxcv4l2 test.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jan 2015 14:32:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/qt-camera/m-p/388281#M56405</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2015-01-08T14:32:49Z</dc:date>
    </item>
  </channel>
</rss>