<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to remove unwanted Apps from Android system build in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-remove-unwanted-Apps-from-Android-system-build/m-p/387527#M56250</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a imx6sl running Android KitKat as an appliance. I am in a memory constrained situation and would like to remove unneeded Apps from the Android build system. Is there any way to control what gets built into the system. For example I have no need for the Deskclock app and would like to not have it loaded at Android start start time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I edited device/fsl/imx6/imx6.mk to remove unwanted apps from PRODUCT_PACKAGES +=&amp;nbsp; section of the file and did a clean rebuild but that did not seem to remove the apps from the Android System.img file.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Oct 2014 19:49:21 GMT</pubDate>
    <dc:creator>bcraig</dc:creator>
    <dc:date>2014-10-13T19:49:21Z</dc:date>
    <item>
      <title>How to remove unwanted Apps from Android system build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-remove-unwanted-Apps-from-Android-system-build/m-p/387527#M56250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a imx6sl running Android KitKat as an appliance. I am in a memory constrained situation and would like to remove unneeded Apps from the Android build system. Is there any way to control what gets built into the system. For example I have no need for the Deskclock app and would like to not have it loaded at Android start start time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I edited device/fsl/imx6/imx6.mk to remove unwanted apps from PRODUCT_PACKAGES +=&amp;nbsp; section of the file and did a clean rebuild but that did not seem to remove the apps from the Android System.img file.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Oct 2014 19:49:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-remove-unwanted-Apps-from-Android-system-build/m-p/387527#M56250</guid>
      <dc:creator>bcraig</dc:creator>
      <dc:date>2014-10-13T19:49:21Z</dc:date>
    </item>
    <item>
      <title>Re: How to remove unwanted Apps from Android system build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-remove-unwanted-Apps-from-Android-system-build/m-p/387528#M56251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you try to remove the Deskclock folder in packages/apps/?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Oct 2014 09:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-remove-unwanted-Apps-from-Android-system-build/m-p/387528#M56251</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2014-10-14T09:57:00Z</dc:date>
    </item>
  </channel>
</rss>