<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Flicker and black screen clear while starting Xorg</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Flicker-and-black-screen-clear-while-starting-Xorg/m-p/387009#M56120</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reply. Yes, you are right. Need to configure ipu in u-boot and avoid changing it afterwards however that requires lot of work as you mentioned on some other post. I found the patch to do it but it is for older kernel. see below the threads.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/472960#472960"&gt;https://community.freescale.com/message/472960#472960&lt;/A&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-98109"&gt;https://community.freescale.com/docs/DOC-98109&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Using "&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: #1f497d;"&gt;“-sharevts&lt;/SPAN&gt;" to xorg command line fixes the flicker which we observed while xorg starts.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Vikash&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Apr 2015 11:56:48 GMT</pubDate>
    <dc:creator>vikaspatil</dc:creator>
    <dc:date>2015-04-09T11:56:48Z</dc:date>
    <item>
      <title>Flicker and black screen clear while starting Xorg</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flicker-and-black-screen-clear-while-starting-Xorg/m-p/387007#M56118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on to implement the splash screen on i.MX6 solo based custom platform using Linux 3.10.17. I am able to display custom splash screen using u-boot and linux framebuffer console(i.e. fbcon, linux logo). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have also written one frame-buffer application where it writes splash image to /dev/fb1 and enabled global alpha and set it to 0x00 for /dev/fb0 to make &lt;/P&gt;&lt;P&gt;/dev/fb1 (splash) visible just before the xorg starts and just after starting the UserInterface, another application again sets global alpha of /dev/fb0 to 0xFF and after that disables the global alpha for /dev/fb0 to make /dev/fb0 (UserInterface) to visible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My understanding was if I use /dev/fb1 to display splash image and as Xorg uses /dev/fb0, splash image would remain intact/untouched while xorg starts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So in this sequence I am observing flicker and screen clear with black by Xorg. I have tried modifying xorg-server-1.14.4 and xserver-xorg-video-imx-viv-3.10.17-1.0.0 in various ways but it didn't help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How could I avoid this flicker and black screen clear while xorg starts? &lt;/P&gt;&lt;P&gt;Do you have any suggestions/ideas to avoid/remove this flicker and clear?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Vikash&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Apr 2015 10:23:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flicker-and-black-screen-clear-while-starting-Xorg/m-p/387007#M56118</guid>
      <dc:creator>vikaspatil</dc:creator>
      <dc:date>2015-04-08T10:23:26Z</dc:date>
    </item>
    <item>
      <title>Re: Flicker and black screen clear while starting Xorg</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flicker-and-black-screen-clear-while-starting-Xorg/m-p/387008#M56119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi vikash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;flicker occurs since linux uses different than uboot IPU settings, so&lt;/P&gt;&lt;P&gt;ideally you should configure IPU in uboot and do not touch it in linux.&lt;/P&gt;&lt;P&gt;Possible solution may be to be fast enough in the bootloader and show&lt;/P&gt;&lt;P&gt;a splash screen under Linux only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Apr 2015 10:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flicker-and-black-screen-clear-while-starting-Xorg/m-p/387008#M56119</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-09T10:43:51Z</dc:date>
    </item>
    <item>
      <title>Re: Flicker and black screen clear while starting Xorg</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flicker-and-black-screen-clear-while-starting-Xorg/m-p/387009#M56120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reply. Yes, you are right. Need to configure ipu in u-boot and avoid changing it afterwards however that requires lot of work as you mentioned on some other post. I found the patch to do it but it is for older kernel. see below the threads.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/472960#472960"&gt;https://community.freescale.com/message/472960#472960&lt;/A&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-98109"&gt;https://community.freescale.com/docs/DOC-98109&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Using "&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: #1f497d;"&gt;“-sharevts&lt;/SPAN&gt;" to xorg command line fixes the flicker which we observed while xorg starts.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Vikash&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Apr 2015 11:56:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flicker-and-black-screen-clear-while-starting-Xorg/m-p/387009#M56120</guid>
      <dc:creator>vikaspatil</dc:creator>
      <dc:date>2015-04-09T11:56:48Z</dc:date>
    </item>
  </channel>
</rss>