<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Using IMX6D with 24 but parallel bus for full HD resolution</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-IMX6D-with-24-but-parallel-bus-for-full-HD-resolution/m-p/386596#M56026</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Semir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using the latest datasheet available?:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf" title="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please take a look at page 5, you can have:&lt;/P&gt;&lt;P&gt;One Parallel 24-bit display port, up to 225 Mpixels/sec (for example, WUXGA at 60 Hz or dual HD1080 and WXGA at 60 Hz)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sergio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Feb 2015 16:40:05 GMT</pubDate>
    <dc:creator>SergioSolis</dc:creator>
    <dc:date>2015-02-24T16:40:05Z</dc:date>
    <item>
      <title>Using IMX6D with 24 but parallel bus for full HD resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-IMX6D-with-24-but-parallel-bus-for-full-HD-resolution/m-p/386595#M56025</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are in phase of evaluating IMX6D Lite for our application.&lt;/P&gt;&lt;P&gt;Due to space restriction, we intend to use LPDDRAM2 (dual channel in one body).&lt;/P&gt;&lt;P&gt;We indent to use only 24bit parallel interface&lt;/P&gt;&lt;P&gt;In data sheet is noted&amp;nbsp; support up to (2 x 1366 x 768), meanwhile in IMX6 Solo/Dual Lite ref manual&lt;/P&gt;&lt;P&gt;is written (chapter&amp;nbsp; 38.1.2.1.2 Display Ports)&amp;nbsp; :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: TimesLTStd-Roman; font-size: 14pt; font-style: normal;"&gt; Parallel video interface (for synchronous access) - up to 24-bit data bus.&lt;BR /&gt;&lt;SPAN style="color: #000000; font-family: TimesLTStd-Roman; font-size: 14pt; font-style: normal;"&gt;• Compatible with MIPI-DPI standard .&lt;BR /&gt;&lt;SPAN style="color: #000000; font-family: TimesLTStd-Roman; font-size: 14pt; font-style: normal;"&gt;• Control protocol - follows Sharp HR and generic TFT definitions&lt;BR /&gt;&lt;SPAN style="color: #000000; font-family: TimesLTStd-Roman; font-size: 14pt; font-style: normal;"&gt;• Supports BT.656 (8-bit) and BT.1120 (16-bit) protocols&lt;BR /&gt;&lt;SPAN style="color: #000000; font-family: TimesLTStd-Roman; font-size: 14pt; font-style: normal;"&gt;• Supports HDTV standards SMPTE274 (1080i/p) and SMPTE296 (720p)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: TimesLTStd-Roman; font-size: 14pt; font-style: normal;"&gt;For synchronous access with one cycle/pixel, this enables, e.g (including 35% blanking&lt;BR /&gt;&lt;SPAN style="color: #000000; font-family: TimesLTStd-Roman; font-size: 14pt; font-style: normal;"&gt;intervals)&lt;BR /&gt;&lt;SPAN style="color: #000000; font-family: TimesLTStd-Roman; font-size: 14pt; font-style: normal;"&gt;• 1080p (1920x1080) @ 60 fps&lt;BR /&gt;&lt;SPAN style="color: #000000; font-family: TimesLTStd-Roman; font-size: 14pt; font-style: normal;"&gt;• WSXGA+ (1680x1050) @ 60 fps&lt;BR /&gt;&lt;SPAN style="color: #000000; font-family: TimesLTStd-Roman; font-size: 14pt; font-style: normal;"&gt;• The combined rate for the two ports is up to 240 MP/sec&lt;BR /&gt;&lt;SPAN style="color: #000000; font-family: TimesLTStd-Roman; font-size: 14pt; font-style: normal;"&gt;The interface includes the following additional features:&lt;BR /&gt;&lt;SPAN style="color: #000000; font-family: TimesLTStd-Roman; font-size: 14pt; font-style: normal;"&gt;• Screen size: up to 4096 x 2048 pixels, programmable by software.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: TimesLTStd-Roman; font-size: 14pt; font-style: normal;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Now I am not sure. Can anyone confirm that I can have at 24 bit RGB full HD (1920 x 1080)&amp;nbsp; at RGB parallel port?&lt;/P&gt;&lt;P&gt;Does using LPDDRAM2 instead of DDRAM3 could impact it ?&lt;/P&gt;&lt;P&gt;Thank in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Feb 2015 13:45:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-IMX6D-with-24-but-parallel-bus-for-full-HD-resolution/m-p/386595#M56025</guid>
      <dc:creator>semirfazlagic</dc:creator>
      <dc:date>2015-02-19T13:45:28Z</dc:date>
    </item>
    <item>
      <title>Re: Using IMX6D with 24 but parallel bus for full HD resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-IMX6D-with-24-but-parallel-bus-for-full-HD-resolution/m-p/386596#M56026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Semir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using the latest datasheet available?:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf" title="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please take a look at page 5, you can have:&lt;/P&gt;&lt;P&gt;One Parallel 24-bit display port, up to 225 Mpixels/sec (for example, WUXGA at 60 Hz or dual HD1080 and WXGA at 60 Hz)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sergio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Feb 2015 16:40:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-IMX6D-with-24-but-parallel-bus-for-full-HD-resolution/m-p/386596#M56026</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2015-02-24T16:40:05Z</dc:date>
    </item>
    <item>
      <title>Re: Using IMX6D with 24 but parallel bus for full HD resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-IMX6D-with-24-but-parallel-bus-for-full-HD-resolution/m-p/386597#M56027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK Sergio thank you&lt;/P&gt;&lt;P&gt;Yes I read this, but I had also some other documents (for example one flayer with comparation various IMX6) where I had this info.&lt;BR /&gt;I think anyway it is offical specification.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2015 11:46:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-IMX6D-with-24-but-parallel-bus-for-full-HD-resolution/m-p/386597#M56027</guid>
      <dc:creator>semirfazlagic</dc:creator>
      <dc:date>2015-02-25T11:46:34Z</dc:date>
    </item>
  </channel>
</rss>