<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSingle Camera output</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Single-Camera-output/m-p/386382#M55985</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are currently working on imx6 with Linux kernel .As we require to capture video from one camera and use the same video for displaying in another board at the same time on the current board .so multiple output with single camera .Is it possible .if so what are the software changes to be done in Kernel level .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Aug 2014 06:47:52 GMT</pubDate>
    <dc:creator>deepanrajanbara</dc:creator>
    <dc:date>2014-08-28T06:47:52Z</dc:date>
    <item>
      <title>Single Camera output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Camera-output/m-p/386382#M55985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are currently working on imx6 with Linux kernel .As we require to capture video from one camera and use the same video for displaying in another board at the same time on the current board .so multiple output with single camera .Is it possible .if so what are the software changes to be done in Kernel level .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Aug 2014 06:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Camera-output/m-p/386382#M55985</guid>
      <dc:creator>deepanrajanbara</dc:creator>
      <dc:date>2014-08-28T06:47:52Z</dc:date>
    </item>
    <item>
      <title>Re: Single Camera output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Camera-output/m-p/386383#M55986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Deeparaj,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please take a look at this thread,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/308383"&gt;Re: IPU multiple video out + Overlay&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Aug 2014 16:48:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Camera-output/m-p/386383#M55986</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2014-08-28T16:48:18Z</dc:date>
    </item>
  </channel>
</rss>