<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I.MX6 HS200 support in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-HS200-support/m-p/386144#M55919</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastien&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6QD, SDL do not support HS200 mode for either boot or in normal BSP operation.&lt;/P&gt;&lt;P&gt;i.MX6SL the uSDHC controller IP was upgraded to support HS200. &lt;/P&gt;&lt;P&gt;Before L3.10 release, eMMC4.5 can not work on HS200 for i.MX6SL since the SW does not support it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Nov 2014 09:54:48 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-11-07T09:54:48Z</dc:date>
    <item>
      <title>I.MX6 HS200 support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-HS200-support/m-p/386143#M55918</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i'm using iMx6 Quad core, a Linux 3.035 and i would like to configure my eMMC in HS200 mode.&lt;/P&gt;&lt;P&gt;I back-ported HS200 patch (&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/drivers/mmc/core?id=a4924c71aa43d4f8a3f342b1f71788349472e684" title="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/drivers/mmc/core?id=a4924c71aa43d4f8a3f342b1f71788349472e684"&gt;linux-2.6-imx.git - Freescale i.MX Linux Tree&lt;/A&gt;) but i had to adapt it (as my linux is 3.035)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When running the code i get an error -EBADMSG coming from mmc_switch when having call:&lt;/P&gt;&lt;P&gt; mmc_switch(card, EXT_CSD_CMD_SET_NORMAL, EXT_CSD_HS_TIMING, 2, 0)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DO you have idea on why this message is not recognized ? Am i missing another patch to back-port ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Br&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Seb&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Nov 2014 08:26:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-HS200-support/m-p/386143#M55918</guid>
      <dc:creator>seb38</dc:creator>
      <dc:date>2014-11-07T08:26:02Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 HS200 support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-HS200-support/m-p/386144#M55919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastien&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6QD, SDL do not support HS200 mode for either boot or in normal BSP operation.&lt;/P&gt;&lt;P&gt;i.MX6SL the uSDHC controller IP was upgraded to support HS200. &lt;/P&gt;&lt;P&gt;Before L3.10 release, eMMC4.5 can not work on HS200 for i.MX6SL since the SW does not support it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Nov 2014 09:54:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-HS200-support/m-p/386144#M55919</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-11-07T09:54:48Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 HS200 support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-HS200-support/m-p/386145#M55920</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks fro your answer. One more question, does Freescale advise any eMMC to get maximum throughput on iMX6-Q&lt;/P&gt;&lt;P&gt;Currently mine (MICRON)&amp;nbsp; is providing me 77Mbytes/s in sequential read (theoretical value should be 80Mbytes/s) in DDR mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would need better perf especially to improve my boot time and also platform globally.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sebastien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Nov 2014 10:19:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-HS200-support/m-p/386145#M55920</guid>
      <dc:creator>seb38</dc:creator>
      <dc:date>2014-11-11T10:19:54Z</dc:date>
    </item>
  </channel>
</rss>