<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Errors with ltib when trying to include QT embedded in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Errors-with-ltib-when-trying-to-include-QT-embedded/m-p/171338#M5588</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The link above seems to be broken.&amp;nbsp; Is there a new link to follow?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Sep 2013 19:37:36 GMT</pubDate>
    <dc:creator>dougschwanke</dc:creator>
    <dc:date>2013-09-11T19:37:36Z</dc:date>
    <item>
      <title>Errors with ltib when trying to include QT embedded</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Errors-with-ltib-when-trying-to-include-QT-embedded/m-p/171336#M5586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class="discussion"&gt;&lt;DIV class="description"&gt;&lt;DIV class="xg_user_generated"&gt;&lt;P&gt;So I am trying to add QT embedded to my root file system using ltib.&amp;nbsp; With the other packages I simply select them, run ltib, and no problems (it adds them to the rootfs).&amp;nbsp; However, when I tried the QT embedded it had errors in finding the package at the &lt;A href="http://www.bitshrine.org" rel="nofollow"&gt;www.bitshrine.org&lt;/A&gt;.&amp;nbsp; (qt-everywhere-opensource-src-4.6.0.tar.gz).&amp;nbsp; I manually checked and sure enough its gone.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;After some googling - I saw where one said that I could simply go get this package myself and put it in the /opt/freescale/pkgs directory and re-run tlib.&amp;nbsp; I did this but then I get a lot of errors with it can find the libraries (like libpng, etc...).&amp;nbsp; I verified the libraries do in fact exist.&amp;nbsp; It also gives a warning of:&lt;/P&gt;&lt;P&gt;"Build path taken because: directory build, no prebuilt rpm,"&amp;nbsp; and&lt;/P&gt;&lt;P&gt;"You have not explicitly asked to use pkg-config and are cross-compiling."&lt;/P&gt;&lt;P&gt;Do I need to specify in the spec file or other? where the libraries live - or is there a better way of doing this?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bills&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2012 01:27:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Errors-with-ltib-when-trying-to-include-QT-embedded/m-p/171336#M5586</guid>
      <dc:creator>blsousan</dc:creator>
      <dc:date>2012-06-29T01:27:36Z</dc:date>
    </item>
    <item>
      <title>Re: Errors with ltib when trying to include QT embedded</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Errors-with-ltib-when-trying-to-include-QT-embedded/m-p/171337#M5587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Got it done by compiling QT outside of ltib.&amp;nbsp; Followed this link and had to hack at it a bit more:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://imxcommunity.org/forum/topics/qt-4-7-4-embedded-spec-on-i-mx28" target="_blank"&gt;http://imxcommunity.org/forum/topics/qt-4-7-4-embedded-spec-on-i-mx28&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jul 2012 18:10:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Errors-with-ltib-when-trying-to-include-QT-embedded/m-p/171337#M5587</guid>
      <dc:creator>blsousan</dc:creator>
      <dc:date>2012-07-02T18:10:22Z</dc:date>
    </item>
    <item>
      <title>Re: Errors with ltib when trying to include QT embedded</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Errors-with-ltib-when-trying-to-include-QT-embedded/m-p/171338#M5588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The link above seems to be broken.&amp;nbsp; Is there a new link to follow?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Sep 2013 19:37:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Errors-with-ltib-when-trying-to-include-QT-embedded/m-p/171338#M5588</guid>
      <dc:creator>dougschwanke</dc:creator>
      <dc:date>2013-09-11T19:37:36Z</dc:date>
    </item>
  </channel>
</rss>