<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: What to do with CSI0_DATA_EN input when connection camera without this signal.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/What-to-do-with-CSI0-DATA-EN-input-when-connection-camera/m-p/384396#M55671</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Perfect, thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Oct 2014 14:01:43 GMT</pubDate>
    <dc:creator>camz</dc:creator>
    <dc:date>2014-10-14T14:01:43Z</dc:date>
    <item>
      <title>What to do with CSI0_DATA_EN input when connection camera without this signal.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-to-do-with-CSI0-DATA-EN-input-when-connection-camera/m-p/384392#M55667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am looking for information on what to do with the CSI0_DATA_EN input on the i.MX6 when connecting a camera that only provides PIXCLK, HSYNC, and VSYNC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The CSI0 interface will be configured for greyscale/generic 16-bit data mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Camz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Oct 2014 18:11:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-to-do-with-CSI0-DATA-EN-input-when-connection-camera/m-p/384392#M55667</guid>
      <dc:creator>camz</dc:creator>
      <dc:date>2014-10-10T18:11:56Z</dc:date>
    </item>
    <item>
      <title>Re: What to do with CSI0_DATA_EN input when connection camera without this signal.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-to-do-with-CSI0-DATA-EN-input-when-connection-camera/m-p/384393#M55668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CSI0_DATA_EN input should be active for normal operation.&lt;/P&gt;&lt;P&gt;Usually in such cases this signal is selected with IOMUX&lt;/P&gt;&lt;P&gt;to some pad, with enabled pad pull-up. Also polarity can be changed &lt;/P&gt;&lt;P&gt;with IPUx_CSIx_SENS_CONF bit CSIx_DATA_EN_POL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Oct 2014 23:59:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-to-do-with-CSI0-DATA-EN-input-when-connection-camera/m-p/384393#M55668</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-10T23:59:57Z</dc:date>
    </item>
    <item>
      <title>Re: What to do with CSI0_DATA_EN input when connection camera without this signal.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-to-do-with-CSI0-DATA-EN-input-when-connection-camera/m-p/384394#M55669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I guess I wasn't as clear with my question as I could have been.&amp;nbsp; I am not looking for a software answer, this was not a question about how to configure the iomux.&amp;nbsp; This was a hardware connection question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a camera that provides data, pixel clock, h-sync, and v-sync signals (actually the sync signals are also called frame enable and line enable).&amp;nbsp; It *does not* provide a data enable signal.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The question is what to do with the physical pin that would normally be connected via the iomux to data enable?&lt;/P&gt;&lt;P&gt;Should it be left unconnected?&amp;nbsp;&amp;nbsp; Tied high or low?&amp;nbsp; Should it be connected to the h-sync / line enable signal?&amp;nbsp; Should it be connected to the v-sync / frame enable signal?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Camz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Oct 2014 13:17:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-to-do-with-CSI0-DATA-EN-input-when-connection-camera/m-p/384394#M55669</guid>
      <dc:creator>camz</dc:creator>
      <dc:date>2014-10-14T13:17:31Z</dc:date>
    </item>
    <item>
      <title>Re: What to do with CSI0_DATA_EN input when connection camera without this signal.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-to-do-with-CSI0-DATA-EN-input-when-connection-camera/m-p/384395#M55670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can tie physical pin high or low or left unconnected (then enable&lt;/P&gt;&lt;P&gt;internal pin pull-up), necessary polarity can be changed &lt;/P&gt;&lt;P&gt;with IPUx_CSIx_SENS_CONF bit CSIx_DATA_EN_POL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Oct 2014 13:57:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-to-do-with-CSI0-DATA-EN-input-when-connection-camera/m-p/384395#M55670</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-14T13:57:28Z</dc:date>
    </item>
    <item>
      <title>Re: What to do with CSI0_DATA_EN input when connection camera without this signal.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-to-do-with-CSI0-DATA-EN-input-when-connection-camera/m-p/384396#M55671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Perfect, thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Oct 2014 14:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-to-do-with-CSI0-DATA-EN-input-when-connection-camera/m-p/384396#M55671</guid>
      <dc:creator>camz</dc:creator>
      <dc:date>2014-10-14T14:01:43Z</dc:date>
    </item>
  </channel>
</rss>