<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Question, i.MX233 power supply</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX233-power-supply/m-p/383878#M55554</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi AVNET JAPAN FAE &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;shortly, yes in general understanding is right. Also one&lt;/P&gt;&lt;P&gt;needs to set DISABLE_STEPPING and set TRG -&lt;/P&gt;&lt;P&gt;voltage level of the linreg supply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Aug 2014 10:48:07 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-08-27T10:48:07Z</dc:date>
    <item>
      <title>Question, i.MX233 power supply</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX233-power-supply/m-p/383877#M55553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about power supply feature of i.MX233.&lt;/P&gt;&lt;P&gt;Could you show me the settings for using internal linear regulator outputs of i.MX233 and stopping internal DCDC outputs?&lt;/P&gt;&lt;P&gt;In my customer’s understanding, to stop DCDC output;&lt;/P&gt;&lt;P&gt;- ENABLE_DCDC bit should be cleared.&lt;/P&gt;&lt;P&gt;To use internal linear regulators;&lt;/P&gt;&lt;P&gt;- 5V should be present.&lt;/P&gt;&lt;P&gt;- ENABLE_LINREG bit should be set.&lt;/P&gt;&lt;P&gt;To adjust offset voltage of the linear regulator output;&lt;/P&gt;&lt;P&gt;- set LINREG_OFFSET bits&lt;/P&gt;&lt;P&gt;&amp;nbsp; 00 : no offset&lt;/P&gt;&lt;P&gt;&amp;nbsp; 01 : +25mV&lt;/P&gt;&lt;P&gt;&amp;nbsp; 1x : -25mV&lt;/P&gt;&lt;P&gt;Is above correct?&lt;/P&gt;&lt;P&gt;If any missing, please let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Aug 2014 10:07:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX233-power-supply/m-p/383877#M55553</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2014-08-27T10:07:54Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX233 power supply</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX233-power-supply/m-p/383878#M55554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi AVNET JAPAN FAE &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;shortly, yes in general understanding is right. Also one&lt;/P&gt;&lt;P&gt;needs to set DISABLE_STEPPING and set TRG -&lt;/P&gt;&lt;P&gt;voltage level of the linreg supply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Aug 2014 10:48:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX233-power-supply/m-p/383878#M55554</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-08-27T10:48:07Z</dc:date>
    </item>
  </channel>
</rss>