<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Three camera inputs for i.MX6Quad in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Three-camera-inputs-for-i-MX6Quad/m-p/383089#M55352</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We would like to connect three cameras to i.MX6.&lt;BR /&gt;(CSI Parallel port 2ch + MIPI-CSI port 1ch)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to i.MX 6 Series Firmware Guide, MIPI and parallel seem to be exclusive. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX 6 Series Firmware Guide Rev.0:&lt;BR /&gt; - 21.5 IOMUX pin mapping&lt;BR /&gt; - Table 21-4. Camera interface mode setting&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can three ports be inputted simultaneously? &lt;BR /&gt;If so, Could you teach the value of Bit19-20 of IOMUXC_GPR1 register which should be set up?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Nov 2014 09:35:43 GMT</pubDate>
    <dc:creator>yuuki</dc:creator>
    <dc:date>2014-11-06T09:35:43Z</dc:date>
    <item>
      <title>Three camera inputs for i.MX6Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Three-camera-inputs-for-i-MX6Quad/m-p/383089#M55352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We would like to connect three cameras to i.MX6.&lt;BR /&gt;(CSI Parallel port 2ch + MIPI-CSI port 1ch)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to i.MX 6 Series Firmware Guide, MIPI and parallel seem to be exclusive. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX 6 Series Firmware Guide Rev.0:&lt;BR /&gt; - 21.5 IOMUX pin mapping&lt;BR /&gt; - Table 21-4. Camera interface mode setting&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can three ports be inputted simultaneously? &lt;BR /&gt;If so, Could you teach the value of Bit19-20 of IOMUXC_GPR1 register which should be set up?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Nov 2014 09:35:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Three-camera-inputs-for-i-MX6Quad/m-p/383089#M55352</guid>
      <dc:creator>yuuki</dc:creator>
      <dc:date>2014-11-06T09:35:43Z</dc:date>
    </item>
    <item>
      <title>Re: Three camera inputs for i.MX6Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Three-camera-inputs-for-i-MX6Quad/m-p/383090#M55353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;IMG style="font-family: 'Verdana','sans-serif';" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;It is possible to connect three cams to i.MX6.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;You may look at Figure 19-1 (CSI2IPU gasket connectivity) of the i.MX6 DQ Reference Manual.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="MIPI_CSI.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46564i5A99CBABD71C3285/image-size/large?v=v2&amp;amp;px=999" role="button" title="MIPI_CSI.jpg" alt="MIPI_CSI.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Nov 2014 05:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Three-camera-inputs-for-i-MX6Quad/m-p/383090#M55353</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-11-07T05:17:57Z</dc:date>
    </item>
  </channel>
</rss>