<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAbout installing additional packages in ltib</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-installing-additional-packages-in-ltib/m-p/382421#M55167</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;M able to build Kernel image from ltib for imx35 board on Ubuntu 12.04 host. But when i try to select additional packages than the default selected ones, The packages are not building as ltib pkgs do not contain them. It tries to search from INTERNET but fails, though INTERNET connection is fine. Please help if anyone know about the issue. M stuck badly.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Nov 2014 07:01:58 GMT</pubDate>
    <dc:creator>shalinikp</dc:creator>
    <dc:date>2014-11-06T07:01:58Z</dc:date>
    <item>
      <title>About installing additional packages in ltib</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-installing-additional-packages-in-ltib/m-p/382421#M55167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;M able to build Kernel image from ltib for imx35 board on Ubuntu 12.04 host. But when i try to select additional packages than the default selected ones, The packages are not building as ltib pkgs do not contain them. It tries to search from INTERNET but fails, though INTERNET connection is fine. Please help if anyone know about the issue. M stuck badly.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Nov 2014 07:01:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-installing-additional-packages-in-ltib/m-p/382421#M55167</guid>
      <dc:creator>shalinikp</dc:creator>
      <dc:date>2014-11-06T07:01:58Z</dc:date>
    </item>
    <item>
      <title>Re: About installing additional packages in ltib</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-installing-additional-packages-in-ltib/m-p/382422#M55168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi shalini&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, not all ltib packages may be compiled.&lt;/P&gt;&lt;P&gt;pdk2009_12_mx35_Linux_RM.pdf shows allowable selections.&lt;/P&gt;&lt;P&gt;So you should carefully check all dependecies and fix them package by package.&lt;/P&gt;&lt;P&gt;I do not think that there is universal fix, which would solved all build problems.&lt;/P&gt;&lt;P&gt;One can look at pdk2009_12_imx35_Linux_HelloWorld_AN.pdf&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=IMX35_PDK0912_LINUXDOCS_BUNDLE&amp;amp;location=null&amp;amp;fasp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz&amp;amp;Parent_nodeId=1240327141887725998192&amp;amp;Parent_pageType=product"&gt;IMX35_PDK0912_LINUXDOCS_BUNDLE&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt;&lt;/P&gt;&lt;P&gt;it shows how to add new application to ltib. For package procedure is&lt;/P&gt;&lt;P&gt;similar. Note one needs to use latest i.MX35 official Freescale BSP:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX35PDK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L2.6.31_09.12.01_SDK_SOURCE&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : Linux 2.6.31 Source Code Files 2009.12&lt;/P&gt;&lt;P&gt;Release support i.MX23, i.MX25, i.MX35, i.MX51&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Nov 2014 08:20:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-installing-additional-packages-in-ltib/m-p/382422#M55168</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-11-06T08:20:27Z</dc:date>
    </item>
  </channel>
</rss>