<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to control the USB_OTG_PWR_CTL_WAKE and USB_OTG_ID of i.MX6 in Linux BSP in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-control-the-USB-OTG-PWR-CTL-WAKE-and-USB-OTG-ID-of-i-MX6/m-p/382374#M55161</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you teach about USB_OTG_PWR_CTL_WAKE and USB_OTG_ID in i.MX6 Linux BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For USB_OTG_ID&lt;BR /&gt;In MX6DL-SABRE-SDP, USB_OTG_ID are connected as follows.&lt;BR /&gt;USB_OTG_ID =&amp;gt; ENET_RX_ER(W23)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I understand Hardware processes this signal.&lt;BR /&gt;(ALT0 mode of ENET_RX_ER is used)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is my understanding right?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;For USB_OTG_PWR_CTL_WAKE&lt;BR /&gt;I was not able to find this signal with a schematic of the SABRE.&lt;BR /&gt;USB_OTG_PWR_CTL_WAKE is multiplexed by GPIO_8.&lt;BR /&gt;However, GPIO_8 is used as DISP0_SER_RS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What kind of case is USB_OTG_PWR_CTL_WAKE used in?&lt;/P&gt;&lt;P&gt;Does Linux BSP support USB_OTG_PWR_CTL_WAKE?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Jan 2015 02:33:56 GMT</pubDate>
    <dc:creator>yuuki</dc:creator>
    <dc:date>2015-01-28T02:33:56Z</dc:date>
    <item>
      <title>How to control the USB_OTG_PWR_CTL_WAKE and USB_OTG_ID of i.MX6 in Linux BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-control-the-USB-OTG-PWR-CTL-WAKE-and-USB-OTG-ID-of-i-MX6/m-p/382374#M55161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you teach about USB_OTG_PWR_CTL_WAKE and USB_OTG_ID in i.MX6 Linux BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For USB_OTG_ID&lt;BR /&gt;In MX6DL-SABRE-SDP, USB_OTG_ID are connected as follows.&lt;BR /&gt;USB_OTG_ID =&amp;gt; ENET_RX_ER(W23)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I understand Hardware processes this signal.&lt;BR /&gt;(ALT0 mode of ENET_RX_ER is used)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is my understanding right?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;For USB_OTG_PWR_CTL_WAKE&lt;BR /&gt;I was not able to find this signal with a schematic of the SABRE.&lt;BR /&gt;USB_OTG_PWR_CTL_WAKE is multiplexed by GPIO_8.&lt;BR /&gt;However, GPIO_8 is used as DISP0_SER_RS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What kind of case is USB_OTG_PWR_CTL_WAKE used in?&lt;/P&gt;&lt;P&gt;Does Linux BSP support USB_OTG_PWR_CTL_WAKE?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jan 2015 02:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-control-the-USB-OTG-PWR-CTL-WAKE-and-USB-OTG-ID-of-i-MX6/m-p/382374#M55161</guid>
      <dc:creator>yuuki</dc:creator>
      <dc:date>2015-01-28T02:33:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to control the USB_OTG_PWR_CTL_WAKE and USB_OTG_ID of i.MX6 in Linux BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-control-the-USB-OTG-PWR-CTL-WAKE-and-USB-OTG-ID-of-i-MX6/m-p/382375#M55162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuuki&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. yes this understanding is right.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. USB_OTG_PWR_CTL_WAKE is an output asserted by the USB controller &lt;/P&gt;&lt;P&gt;whenever the USB controller and PHY wake up due to a software resume or &lt;/P&gt;&lt;P&gt;a USB remote wakeup. It can be used as a USB wakeup signal to the rest &lt;/P&gt;&lt;P&gt;of the system. It is not used in Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jan 2015 04:31:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-control-the-USB-OTG-PWR-CTL-WAKE-and-USB-OTG-ID-of-i-MX6/m-p/382375#M55162</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-28T04:31:05Z</dc:date>
    </item>
  </channel>
</rss>