<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Buildroot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Buildroot/m-p/170915#M5512</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Has anyone used buildroot for i.mx53? &amp;nbsp;I plan on trying it out for learning purposes, first on this board and then for a separate ARM board which was used for an embedded Linux class I took about a year ago.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 17 Sep 2011 00:26:21 GMT</pubDate>
    <dc:creator>JoseOchoa</dc:creator>
    <dc:date>2011-09-17T00:26:21Z</dc:date>
    <item>
      <title>Buildroot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Buildroot/m-p/170915#M5512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Has anyone used buildroot for i.mx53? &amp;nbsp;I plan on trying it out for learning purposes, first on this board and then for a separate ARM board which was used for an embedded Linux class I took about a year ago.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Sep 2011 00:26:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Buildroot/m-p/170915#M5512</guid>
      <dc:creator>JoseOchoa</dc:creator>
      <dc:date>2011-09-17T00:26:21Z</dc:date>
    </item>
    <item>
      <title>Re: Buildroot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Buildroot/m-p/170916#M5513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can use this post as a starting point: &lt;A href="http://boundarydevices.com/blogs/using-buildroot-on-nitrogen" target="_blank"&gt;http://boundarydevices.com/blogs/using-buildroot-on-nitrogen&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Nitrogen board is a MX51 based hardware from Boundary Devices.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Sep 2011 17:56:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Buildroot/m-p/170916#M5513</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2011-09-17T17:56:03Z</dc:date>
    </item>
    <item>
      <title>Re: Buildroot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Buildroot/m-p/170917#M5514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes/no.&lt;/P&gt;&lt;P&gt;I am building for an i.mx53 QSB. I am not using buildroot to build the kernel or u-boot. Though I probably could.&lt;/P&gt;&lt;P&gt;I am using it to build the toolchain and the rootfs - though I typically do a fair amount of post build customization of buildroot rootfs's as I do not like their initialization scheme and revert to a more traditional one with start/stop scripts in /etc/init.d and links in /etc/rcS.d for those that are enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All the typical buildroot (and pretty much every build environment) caveats apply.&lt;/P&gt;&lt;P&gt;Don't run buildroot as root, don't build it from /usr/src, frequently some choices of libraries gcc versions, cpu's .... are incompatible. As an example I beleive some versions of gcc 4.6 will not build some libraries.&lt;/P&gt;&lt;P&gt;Overall i like buildroot better than LTIB, but nothing is perfect.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jan 2012 19:44:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Buildroot/m-p/170917#M5514</guid>
      <dc:creator>dhlii</dc:creator>
      <dc:date>2012-01-10T19:44:31Z</dc:date>
    </item>
  </channel>
</rss>