<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Re: iMX28 eMMC v5.0 support</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-eMMC-v5-0-support/m-p/381683#M55035</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did the following modificat&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;ion in the kernel 3.10 (&lt;SPAN style="color: black; font-size: 10pt;"&gt;drivers\mmc\core\mmc.c)&lt;/SPAN&gt; to skip the error message and the eMMC v5&lt;/SPAN&gt;.0 seems to work fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;EM&gt;if (card-&amp;gt;ext_csd.rev &amp;gt; &lt;STRONG style="color: #ff0000;"&gt;7&lt;/STRONG&gt;) {&lt;/EM&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt; &lt;/TD&gt;&lt;TD&gt;&lt;EM&gt;&amp;nbsp; pr_err("%s: unrecognised EXT_CSD revision %d\n",&lt;/EM&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt; &lt;/TD&gt;&lt;TD&gt;&lt;EM&gt;&amp;nbsp; mmc_hostname(card-&amp;gt;host), card-&amp;gt;ext_csd.rev);&lt;/EM&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt; &lt;/TD&gt;&lt;TD&gt;&lt;EM&gt;&amp;nbsp; err = -EINVAL;&lt;/EM&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt; &lt;/TD&gt;&lt;TD&gt;&lt;EM&gt;&amp;nbsp; goto out;&lt;/EM&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;EM&gt;}&lt;/EM&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;I also tried the kernel 3.18 without any modifications and it also seems to work fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I don't need the new features introduced since v4.41, is it safe to use a v5.0 eMMC with the i.MX28?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Feb 2015 13:54:15 GMT</pubDate>
    <dc:creator>spicard</dc:creator>
    <dc:date>2015-02-18T13:54:15Z</dc:date>
    <item>
      <title>iMX28 eMMC v5.0 support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-eMMC-v5-0-support/m-p/381681#M55033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;the datasheet of the iMX28 say that eMMC v4.3 and eMMC v4.4 is supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I use eMMC v5.0 without problems?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will it be possible to use the new features of v5.0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using linux kernel 3.10.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Feb 2015 17:56:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-eMMC-v5-0-support/m-p/381681#M55033</guid>
      <dc:creator>spicard</dc:creator>
      <dc:date>2015-02-17T17:56:18Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 eMMC v5.0 support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-eMMC-v5-0-support/m-p/381682#M55034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately only eMMC v4.3 and eMMC v4.4 are supported by the SSP Module of the i.MX28.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Other community users have successfully used eMMC v5.0 on the i.MX53 and i.MX6 by changing some settings and making the eMMC v5.0 work as eMMC v4.4 like on the following threads.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/325001"&gt;https://community.freescale.com/thread/325001&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="304771" data-objecttype="1" href="https://community.freescale.com/thread/304771"&gt;https://community.freescale.com/thread/304771&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In any case all new features of eMMC v5.0 like HS400 mode and Data Strobe won’t be available&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Feb 2015 21:47:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-eMMC-v5-0-support/m-p/381682#M55034</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-02-17T21:47:48Z</dc:date>
    </item>
    <item>
      <title>Re: Re: iMX28 eMMC v5.0 support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-eMMC-v5-0-support/m-p/381683#M55035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did the following modificat&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;ion in the kernel 3.10 (&lt;SPAN style="color: black; font-size: 10pt;"&gt;drivers\mmc\core\mmc.c)&lt;/SPAN&gt; to skip the error message and the eMMC v5&lt;/SPAN&gt;.0 seems to work fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;EM&gt;if (card-&amp;gt;ext_csd.rev &amp;gt; &lt;STRONG style="color: #ff0000;"&gt;7&lt;/STRONG&gt;) {&lt;/EM&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt; &lt;/TD&gt;&lt;TD&gt;&lt;EM&gt;&amp;nbsp; pr_err("%s: unrecognised EXT_CSD revision %d\n",&lt;/EM&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt; &lt;/TD&gt;&lt;TD&gt;&lt;EM&gt;&amp;nbsp; mmc_hostname(card-&amp;gt;host), card-&amp;gt;ext_csd.rev);&lt;/EM&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt; &lt;/TD&gt;&lt;TD&gt;&lt;EM&gt;&amp;nbsp; err = -EINVAL;&lt;/EM&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt; &lt;/TD&gt;&lt;TD&gt;&lt;EM&gt;&amp;nbsp; goto out;&lt;/EM&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;EM&gt;}&lt;/EM&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;I also tried the kernel 3.18 without any modifications and it also seems to work fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I don't need the new features introduced since v4.41, is it safe to use a v5.0 eMMC with the i.MX28?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Feb 2015 13:54:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-eMMC-v5-0-support/m-p/381683#M55035</guid>
      <dc:creator>spicard</dc:creator>
      <dc:date>2015-02-18T13:54:15Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 eMMC v5.0 support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-eMMC-v5-0-support/m-p/381684#M55036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is not officially supported by the i.MX28 controller but eMMC5.0 is backwards compatible with eMMCv4.4 so as long as it's being used as eMMCv4.4 (not using any v5.0 features) you should be fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Feb 2015 20:10:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-eMMC-v5-0-support/m-p/381684#M55036</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-02-18T20:10:16Z</dc:date>
    </item>
  </channel>
</rss>