<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.Mx6SL</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6SL/m-p/381253#M54975</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"You also need to use the 10.10 or 11.04 64 bit version of&lt;/P&gt;&lt;P&gt;Ubuntu which are the most tested OS for the Android kk4.4.2&lt;/P&gt;&lt;P&gt;build."&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 04 Jan 2015 05:44:30 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-01-04T05:44:30Z</dc:date>
    <item>
      <title>i.Mx6SL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6SL/m-p/381252#M54974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, i have file uimage and zimage then i build kernel, i want to creat file boot.img from both file uimage and zimage, i use command :&lt;/P&gt;&lt;P&gt;~/myandroid/kernel_imx/arch/arm/boot$&amp;nbsp; ./mkbootimg --kernel zImage --ramdisk ramdisk.img --base 0x80800000 --cmdline 'console=ttymxc0,115200 init=/init androidboot.console=ttymxc0 video=mxc_elcdif_fb:bpp=32 androidboot.hardware=freescale csi' -o new-boot.img&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but it appear error:&lt;/P&gt;&lt;P&gt;./mkbootimg: /lib/libc.so.6: version `GLIBC_2.14' not found (required by ./mkbootimg)&lt;/P&gt;&lt;P&gt; Help me for error!, thank everybody!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Dec 2014 02:17:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6SL/m-p/381252#M54974</guid>
      <dc:creator>phamhuynh</dc:creator>
      <dc:date>2014-12-31T02:17:27Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx6SL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6SL/m-p/381253#M54975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"You also need to use the 10.10 or 11.04 64 bit version of&lt;/P&gt;&lt;P&gt;Ubuntu which are the most tested OS for the Android kk4.4.2&lt;/P&gt;&lt;P&gt;build."&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Jan 2015 05:44:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6SL/m-p/381253#M54975</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-01-04T05:44:30Z</dc:date>
    </item>
  </channel>
</rss>