<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX28 Video playback issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Video-playback-issue/m-p/380248#M54836</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;DIVX is not supported because of license restrictions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Dec 2014 08:17:46 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-12-02T08:17:46Z</dc:date>
    <item>
      <title>i.MX28 Video playback issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Video-playback-issue/m-p/380247#M54835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am a video playback test using i.mx28 ref B/D and IMX28 L2.6.35_1.1.0_130130_source code.&lt;BR /&gt;But I can't see video screen only hear MP3 audio.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;lt;Installation Procedure&amp;gt;&lt;BR /&gt;1. ltib is installed Gnome packages using IMX28 L2.6.35_1.1.0_130130_source.&lt;BR /&gt;2. Installed&amp;nbsp; L2.6.35_1.1.0_130130_MM_CODECS_BUNDLE.&lt;BR /&gt;gst-fsl-plugins-3.0.6.tar.gz&lt;BR /&gt;libfslcodec-3.0.6.tar.gz&lt;BR /&gt;libfslparser-3.0.6.tar.gz&lt;BR /&gt;3. ltib -C&lt;BR /&gt;Package list -&amp;gt; Freescale Multimedia Plugins/Codecs&amp;nbsp; ---&amp;gt; [*] gst-fsl-plugins&lt;BR /&gt;4. Video playback test after scouce code complie but can't see video.&lt;/P&gt;&lt;P&gt;But If when I use another demo image file, Video playback is OK.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pls refer to attached file of video playback test log message and mov1.avi video test file.&lt;/P&gt;&lt;P&gt;One is video playback OK.&lt;BR /&gt;Another log file is video playback NG.&lt;BR /&gt;You can see the different library versions.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pls comment helpful for resolve this problem.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-335779"&gt;Video_NG_Image_log.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-335779"&gt;Video_OK_Image_log.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Nov 2014 13:07:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Video-playback-issue/m-p/380247#M54835</guid>
      <dc:creator>powerprince</dc:creator>
      <dc:date>2014-11-28T13:07:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 Video playback issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Video-playback-issue/m-p/380248#M54836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;DIVX is not supported because of license restrictions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Dec 2014 08:17:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-Video-playback-issue/m-p/380248#M54836</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-12-02T08:17:46Z</dc:date>
    </item>
  </channel>
</rss>