<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Poor framerates on iMX6 Solo when decoding H264 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379779#M54639</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I've unbricked my device now and flashed a U-Boot that has all functions that return the CPU revision return 0x61011. The patch in the link did not apply very well at all so I manually edited arch/arm/cpu/armv7/mx6/soc.c so that the revision was returned as a fixed number.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I rebooted the unit, I found that the hardware revision was only set correctly in /proc/cpuinfo when I booted *my* kernel image. When I tried booting the Freescale DEMO kernel image it came up with a "hardware revision" of 0000.&lt;/P&gt;&lt;P&gt;Why would this be? Both kernel images are booting from the same bootloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Oct 2014 14:27:54 GMT</pubDate>
    <dc:creator>ralph__</dc:creator>
    <dc:date>2014-10-23T14:27:54Z</dc:date>
    <item>
      <title>Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379764#M54624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using gstreamer to playback some H264 videos - one is 720p60 and one is 1080p30. The framerates are much worse than expected (the iMX can do 1080p30 and 720p60 allegedly....) and I am certain the hardware is doing the decoding as it only has 1-2% CPU utilisation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are the commands I run to test the video. Either:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;gst-launch-0.10 filesrc location=/usr/sample.mp4 ! qtdemux ! vpudec ! mfw_isink &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;or:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;gplay /usr/sample.mp4&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both lines give me the same end result which is this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1080p30 clip runs at 23fps (reported)&lt;/P&gt;&lt;P&gt;720p60 clip runs at 27fps (reported)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why are the clips running so slowly? If I play back either clip in VLC on Windows the framerates are as expected; i.e. 30fps for the 1080p30 and 60fps for the 1080p60.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks for your help,&lt;/P&gt;&lt;P&gt;Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Oct 2014 10:25:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379764#M54624</guid>
      <dc:creator>ralph__</dc:creator>
      <dc:date>2014-10-09T10:25:42Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379765#M54625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ralph&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest to look at below links where&lt;/P&gt;&lt;P&gt;all video test procedures are well summarized in one place&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-93387/version/4" title="https://community.freescale.com/docs/DOC-93387/version/4"&gt;https://community.freescale.com/docs/DOC-93387/version/4&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Testing things out&lt;/P&gt;&lt;P&gt;&lt;A href="http://boundarydevices.com/mx6-video-acceleration-raring-debian/" title="http://boundarydevices.com/mx6-video-acceleration-raring-debian/"&gt;http://boundarydevices.com/mx6-video-acceleration-raring-debian/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H3&gt;&lt;/H3&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Oct 2014 13:09:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379765#M54625</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-09T13:09:30Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379766#M54626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;I've looked at both those links - thanks for providing them - however none of the mp4-related commands work for me and the "Sintel" clip that they suggest to use isn't even 1080p30! Even then, the "Sintel" clip only runs at 24fps, not at the 30fps that I'd expect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Oct 2014 15:47:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379766#M54626</guid>
      <dc:creator>ralph__</dc:creator>
      <dc:date>2014-10-09T15:47:22Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379767#M54627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ralph&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest to test with Demo Image&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6S&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.0.35_4.1.0_DEMO_IMAGE_BSP&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux Binary Demo Files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One can also try kernel parameters : enable_wait_mode=off, maxcpus=0 (nosmp)&lt;/P&gt;&lt;P&gt;and check if SD (if video is located on it) is high class speed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Oct 2014 09:59:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379767#M54627</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-10T09:59:23Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379768#M54628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I tried those kernel parameters but no luck.&lt;/P&gt;&lt;P&gt;I'll try the demo image and report back.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Oct 2014 13:51:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379768#M54628</guid>
      <dc:creator>ralph__</dc:creator>
      <dc:date>2014-10-14T13:51:29Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379769#M54629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sadly those images are all for the Sabre board (whatever that is) and not the IMX6Solo which is what I have. Here is the boot trace before it hangs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Linux version 3.0.35-2666-gbdde708 (r65388@shlinux3) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #1 SMP PREEMPT Fri Aug 16 10:43:44 CST 2013&lt;/P&gt;&lt;P&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d&lt;/P&gt;&lt;P&gt;CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;/P&gt;&lt;P&gt;Machine: Freescale i.MX 6Quad Sabre-Lite Board&lt;/P&gt;&lt;P&gt;Memory policy: ECC disabled, Data cache writealloc&lt;/P&gt;&lt;P&gt;CPU identified as i.MX6DL/SOLO, silicon rev 1.1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Oct 2014 12:31:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379769#M54629</guid>
      <dc:creator>ralph__</dc:creator>
      <dc:date>2014-10-20T12:31:28Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379770#M54630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ralph&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you are using Sabre-Lite then it is better to&lt;/P&gt;&lt;P&gt;check boundary images, like below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://boundarydevices.com/running-linaro-ubuntu-on-i-mx6-sabre-lite-and-nitrogen6x/" title="http://boundarydevices.com/running-linaro-ubuntu-on-i-mx6-sabre-lite-and-nitrogen6x/"&gt;http://boundarydevices.com/running-linaro-ubuntu-on-i-mx6-sabre-lite-and-nitrogen6x/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Oct 2014 14:44:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379770#M54630</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-20T14:44:48Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379771#M54631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After a reasonably massive struggle, I managed to get the original DEMO image up and running. Sadly, there are no H264 or mp4 files on that image and the gstreamer framework fails when I try to get one of my own mp4 files working that I know work on my own system.&lt;/P&gt;&lt;P&gt;Thanks for the Ubuntu link. I'll try that and see if I have better luck.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2014 14:06:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379771#M54631</guid>
      <dc:creator>ralph__</dc:creator>
      <dc:date>2014-10-21T14:06:47Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379772#M54632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you try a different sink like &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; gst-launch playbin2 uri=file://&lt;SPAN style="font-weight: bold; color: blue;"&gt;/video-file.mp4&lt;/SPAN&gt;&amp;nbsp; video-sink="&lt;SPAN style="font-weight: bold; color: blue;"&gt;mfw_v4lsink&lt;/SPAN&gt;"&lt;/P&gt;&lt;P&gt; to play your clips (change the file name) .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2014 15:20:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379772#M54632</guid>
      <dc:creator>xizhouwang</dc:creator>
      <dc:date>2014-10-21T15:20:18Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379773#M54633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've tried this but all I get is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gst-launch playbin2 uri=file:///nfs/sample.mp4&amp;nbsp; video-sink="mf&lt;/P&gt;&lt;P&gt;MFW_GST_V4LSINK_PLUGIN 3.0.10 build on Mar&amp;nbsp; 2 2014 17:33:04.&lt;/P&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;/P&gt;&lt;P&gt;Pipeline is PREROLLING ...&lt;/P&gt;&lt;P&gt;Aiur: 3.0.10&lt;/P&gt;&lt;P&gt;Core: MPEG4PARSER_06.07.03&amp;nbsp; build on Nov 15 2013 01:36:39&lt;/P&gt;&lt;P&gt;&amp;nbsp; mime: video/quicktime; audio/x-m4a; application/x-3gp&lt;/P&gt;&lt;P&gt;&amp;nbsp; file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm11_elinux.so.3.2&lt;/P&gt;&lt;P&gt;Content Info:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; URI:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; file:///nfs/sample.mp4&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Idx File:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /home/root/.aiur/.nfs.sample.mp4.aidx&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Seekable&amp;nbsp; : Yes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Size(byte): 14621544&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Movie Info:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Seekable&amp;nbsp; : Yes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Live&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : No&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Duration&amp;nbsp; : 0:00:52.209000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ReadMode&amp;nbsp; : Track&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Track&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Track 00 [video_000000] Enabled&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Duration: 0:00:52.208000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Language: und&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mime:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; video/x-h264, parsed=(boolean)true, width=(int)1920, height=(int)1080, framerate&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =(fraction)24/1&lt;/P&gt;&lt;P&gt;[ERR]&amp;nbsp;&amp;nbsp; Error in opening firmware binary file&lt;/P&gt;&lt;P&gt;[ERR]&amp;nbsp;&amp;nbsp; Please put bin file to /lib/firmware/vpu folder or export VPU_FW_PATH env&lt;/P&gt;&lt;P&gt;H264D_ARM11_02.06.03&amp;nbsp; build on Apr 16 2013 13:30:59.&lt;/P&gt;&lt;P&gt;MFW_GST_H264_DECODER_PLUGIN 3.0.10 build on Mar&amp;nbsp; 2 2014 17:33:34.&lt;/P&gt;&lt;P&gt;Track 01 [audio_000000] Enabled&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Duration: 0:00:51.946000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Language: und&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mime:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)48000, bitrate=(int)0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; , framed=(boolean)true, stream-format=(string)raw, codec_data=(buffer)1190&lt;/P&gt;&lt;P&gt;ERROR: from element /GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/MFW_GST_H264DEC_INFO_T:mfw_gst_h264dec_info_t0: fatal error&lt;/P&gt;&lt;P&gt;Additional debug info:&lt;/P&gt;&lt;P&gt;non recoverable error while decoding the H.264 Data&lt;/P&gt;&lt;P&gt;ERROR: pipeline doesn't want to preroll.&lt;/P&gt;&lt;P&gt;Setting pipeline to NULL ...&lt;/P&gt;&lt;P&gt;Total rendered:0&lt;/P&gt;&lt;P&gt;Freeing pipeline ...&lt;/P&gt;&lt;P&gt;[---&amp;gt;FINALIZE v4l_sink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact, I always get the error message "Error in opening firmware binary file" and I've tried loads of different command lines with gstreamer. :-( Here are some of the environment variables I have set up:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;export GST_PLUGIN_PATH="/usr/lib/gstreamer-0.10/:/usr/lib"&lt;/P&gt;&lt;P&gt;export LD_LIBRARY_PATH="/usr/lib/gstreamer-0.10/:/usr/lib"&lt;/P&gt;&lt;P&gt;export VPU_FW_PATH="/usr/lib/gstreamer-0.10/:/usr/lib:/lib/firmware/vpu"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2014 15:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379773#M54633</guid>
      <dc:creator>ralph__</dc:creator>
      <dc:date>2014-10-21T15:25:32Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379774#M54634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;do this&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; gst-inspect |grep mfw&lt;/P&gt;&lt;P&gt;to check what sink are on your system. Here is from one of my fs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt; color: red;"&gt;# gst-inspect |grep mfw&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt;"&gt;ipucsc.imx:&amp;nbsp; mfw_ipucsc: IPU-based video converter&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt;"&gt;v4lsrc.imx:&amp;nbsp; mfw_v4lsrc: v4l2 based camera src&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt;"&gt;mpeg2dec.imx:&amp;nbsp; mfw_mpeg2decoder: mpeg2 video decoder&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt;"&gt;amrdec.imx:&amp;nbsp; mfw_amrdecoder: amr audio decoder&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt;"&gt;aacdec.imx:&amp;nbsp; mfw_aacdecoder: aac audio decoder&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt;"&gt;v4lsink.imx:&amp;nbsp; mfw_v4lsink: v4l2 video sink&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt;"&gt;mpeg4dec.imx:&amp;nbsp; mfw_mpeg4aspdecoder: mpeg4 video decoder&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt;"&gt;audiopeq.imx:&amp;nbsp; mfw_audio_pp: audio post equalizer&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt;"&gt;h264.imx:&amp;nbsp; mfw_h264decoder: h264 video decoder&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt;"&gt;isink.imx:&amp;nbsp; mfw_isink: IPU-based video sink&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt;"&gt;mp3enc.imx:&amp;nbsp; mfw_mp3encoder: mp3 audio encoder&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt;"&gt;vorbisdec.imx:&amp;nbsp; mfw_vorbisdecoder: vorbis audio decoder&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2014 16:02:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379774#M54634</guid>
      <dc:creator>xizhouwang</dc:creator>
      <dc:date>2014-10-21T16:02:02Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379775#M54635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here you go:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@nitrogen6x:~# gst-inspect | grep mfw&lt;/P&gt;&lt;P&gt;ipucsc.imx:&amp;nbsp; mfw_ipucsc: IPU-based video converter&lt;/P&gt;&lt;P&gt;v4lsrc.imx:&amp;nbsp; mfw_v4lsrc: v4l2 based camera src&lt;/P&gt;&lt;P&gt;h264.imx:&amp;nbsp; mfw_h264decoder: h264 video decoder&lt;/P&gt;&lt;P&gt;mp3enc.imx:&amp;nbsp; mfw_mp3encoder: mp3 audio encoder&lt;/P&gt;&lt;P&gt;isink.imx:&amp;nbsp; mfw_isink: IPU-based video sink&lt;/P&gt;&lt;P&gt;amrdec.imx:&amp;nbsp; mfw_amrdecoder: amr audio decoder&lt;/P&gt;&lt;P&gt;v4lsink.imx:&amp;nbsp; mfw_v4lsink: v4l2 video sink&lt;/P&gt;&lt;P&gt;audiopeq.imx:&amp;nbsp; mfw_audio_pp: audio post equalizer&lt;/P&gt;&lt;P&gt;mpeg2dec.imx:&amp;nbsp; mfw_mpeg2decoder: mpeg2 video decoder&lt;/P&gt;&lt;P&gt;mpeg4dec.imx:&amp;nbsp; mfw_mpeg4aspdecoder: mpeg4 video decoder&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried using mfw_v4lsink and mfw_mpeg4aspdecoder in various combinations but no luck.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2014 16:18:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379775#M54635</guid>
      <dc:creator>ralph__</dc:creator>
      <dc:date>2014-10-21T16:18:03Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379776#M54636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This link could be helpful for your firmware ERR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/305396"&gt;Error in opening firmware binary file for i.mx6 solo wandboard&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2014 08:07:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379776#M54636</guid>
      <dc:creator>xizhouwang</dc:creator>
      <dc:date>2014-10-22T08:07:30Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379777#M54637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the link. That looks like it may in fact fix things however after applying the patch in the link, I flashed U-Boot and have currently bricked my board. I'm attempting to unbrick it over USB however it doesn't show up on my PC over USB.... :-(&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2014 16:29:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379777#M54637</guid>
      <dc:creator>ralph__</dc:creator>
      <dc:date>2014-10-22T16:29:52Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379778#M54638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry to hear that and hope you will get it going again soon.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Oct 2014 09:01:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379778#M54638</guid>
      <dc:creator>xizhouwang</dc:creator>
      <dc:date>2014-10-23T09:01:32Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379779#M54639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I've unbricked my device now and flashed a U-Boot that has all functions that return the CPU revision return 0x61011. The patch in the link did not apply very well at all so I manually edited arch/arm/cpu/armv7/mx6/soc.c so that the revision was returned as a fixed number.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I rebooted the unit, I found that the hardware revision was only set correctly in /proc/cpuinfo when I booted *my* kernel image. When I tried booting the Freescale DEMO kernel image it came up with a "hardware revision" of 0000.&lt;/P&gt;&lt;P&gt;Why would this be? Both kernel images are booting from the same bootloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Oct 2014 14:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379779#M54639</guid>
      <dc:creator>ralph__</dc:creator>
      <dc:date>2014-10-23T14:27:54Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379780#M54640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Returns from one of my Solo kit. Hope other expert may have advice on the issues. &lt;/P&gt;&lt;P&gt;root@:~# cat /proc/cpuinfo&lt;/P&gt;&lt;P&gt;Processor&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : ARMv7 Processor rev 10 (v7l)&lt;/P&gt;&lt;P&gt;processor&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0&lt;/P&gt;&lt;P&gt;BogoMIPS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 1581.05&lt;/P&gt;&lt;P&gt;Features&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : swp half thumb fastmult vfp edsp neon vfpv3&lt;/P&gt;&lt;P&gt;CPU implementer : 0x41&lt;/P&gt;&lt;P&gt;CPU architecture: 7&lt;/P&gt;&lt;P&gt;CPU variant&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0x2&lt;/P&gt;&lt;P&gt;CPU part&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0xc09&lt;/P&gt;&lt;P&gt;CPU revision&amp;nbsp;&amp;nbsp;&amp;nbsp; : 10&lt;/P&gt;&lt;P&gt;Hardware&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; :&amp;nbsp; &lt;/P&gt;&lt;P&gt;Revision&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 63000&lt;/P&gt;&lt;P&gt;Serial&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0000000000000000&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Oct 2014 09:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379780#M54640</guid>
      <dc:creator>xizhouwang</dc:creator>
      <dc:date>2014-10-24T09:33:55Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379781#M54641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Okay, I've rebuilt my system and my results are as follows for a 720p60 clip:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;echo "S:1280x720p-60" &amp;gt; /sys/class/graphics/fb0/mode&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;gst-launch filesrc location=/usr/sample720p60_40Mbps.mp4 typefind=true ! qtdemux ! vpudec framedrop=false ! queue max-size-buffers=10 ! mfw_isink sync=false disp-width=1280 disp-height=720&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;gplay /usr/sample720p60_40Mbps.mp4&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both the gplay and gst-launch commands give 56fps. If I then switch to a 1080p30 clip:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;echo "S:1920x1080p-60" &amp;gt; /sys/class/graphics/fb0/mode&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;gplay /usr/sample1080p30_40Mbps.mp4&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I only get 23fps still.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;So I still need to get the 56fps for 720p clips up to 60fps, and I need to get the 23fps up to 30fps for 1080p clips.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've also been trying the daisy, dizzy and master images built from scratch using Yocto. None of these give me the full frame rate results either. :'-(&lt;/P&gt;&lt;P&gt;By the way, if I change the sink to be mfw_v4lsink then I still get the same frame rates. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Nov 2014 13:41:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379781#M54641</guid>
      <dc:creator>ralph__</dc:creator>
      <dc:date>2014-11-07T13:41:24Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379782#M54642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think you should test on Freescale Sabre SD reference board (i.MX6DL procesor)&lt;/P&gt;&lt;P&gt;with latest Demo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.0.101_4.1.1_IM6QDLS_BUNDLE&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux Binary Demo Files. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using SabreLite board please post this on boundary devices forum&lt;/P&gt;&lt;P&gt;since Freescale images may not work good on Sabrelite board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Nov 2014 13:48:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379782#M54642</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-11-07T13:48:38Z</dc:date>
    </item>
    <item>
      <title>Re: Poor framerates on iMX6 Solo when decoding H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379783#M54643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One thing I haven't mentioned is that on my Nitrogen6_lite Boundary Devices board, I have actually had it running at 1080p30 and 720p60 using the LTIB image. Here is the link where I got the image from:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://boundarydevices.com/ltib-on-i-mx6-without-x/" title="http://boundarydevices.com/ltib-on-i-mx6-without-x/"&gt;http://boundarydevices.com/ltib-on-i-mx6-without-x/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;gplay /nfs/sample720p60_40Mbps.mp4&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt; [60fps]&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;echo "S:1920x1080p-60" &amp;gt; /sys/class/graphics/fb0/mode&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;gplay /nfs/sample1080p30_40Mbps.mp4&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt; [30fps]&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are some strange differences between this image and my own. For LTIB, here is some interesting info:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;[kernel boot messages]&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Memory: 384MB = 384MB total&lt;/P&gt;&lt;P&gt;Memory: 381008k/381008k available, 143280k reserved, 0K highmem&lt;/P&gt;&lt;P&gt;Linux version 3.0.35-2026-geaaf30e-02079-g2a4aa352 (ericn@ericsam) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #4 SMP PREEMPT Tue Dec 18 08:40:53 MST 2012&lt;/P&gt;&lt;P&gt;CPU identified as i.MX6DL/SOLO, silicon rev 1.1&lt;/P&gt;&lt;P&gt;Virtual kernel memory layout:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xfff00000 - 0xfffe0000&amp;nbsp;&amp;nbsp; ( 896 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0xf4600000 - 0xffe00000&amp;nbsp;&amp;nbsp; ( 184 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xa0800000 - 0xf2000000&amp;nbsp;&amp;nbsp; (1304 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0x80000000 - 0xa0000000&amp;nbsp;&amp;nbsp; ( 512 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pkmap&amp;nbsp;&amp;nbsp; : 0x7fe00000 - 0x80000000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 2 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0x7f000000 - 0x7fe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 14 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0x80008000 - 0x80038000&amp;nbsp;&amp;nbsp; ( 192 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0x80038000 - 0x806d81b0&amp;nbsp;&amp;nbsp; (6785 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0x806da000 - 0x8072eb20&amp;nbsp;&amp;nbsp; ( 339 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0x8072eb44 - 0x8077a9a0&amp;nbsp;&amp;nbsp; ( 304 kB)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;root@freescale ~$ cat /proc/cpuinfo&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Processor&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : ARMv7 Processor rev 10 (v7l)&lt;/P&gt;&lt;P&gt;processor&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0&lt;/P&gt;&lt;P&gt;BogoMIPS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 1988.28&lt;/P&gt;&lt;P&gt;Features&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : swp half thumb fastmult vfp edsp neon vfpv3&lt;/P&gt;&lt;P&gt;CPU implementer : 0x41&lt;/P&gt;&lt;P&gt;CPU architecture: 7&lt;/P&gt;&lt;P&gt;CPU variant&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0x2&lt;/P&gt;&lt;P&gt;CPU part&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0xc09&lt;/P&gt;&lt;P&gt;CPU revision&amp;nbsp;&amp;nbsp;&amp;nbsp; : 10&lt;/P&gt;&lt;P&gt;Hardware&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : Freescale i.MX 6Quad Sabre-Lite Board&lt;/P&gt;&lt;P&gt;Revision&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 61011&lt;/P&gt;&lt;P&gt;Serial&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0000000000000000&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;root@freescale ~$ cat /proc/meminfo&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;MemTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 381200 kB&lt;/P&gt;&lt;P&gt;MemFree:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 358960 kB&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;VmallocTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp; 1335296 kB&lt;/P&gt;&lt;P&gt;VmallocUsed:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2964 kB&lt;/P&gt;&lt;P&gt;VmallocChunk:&amp;nbsp;&amp;nbsp;&amp;nbsp; 1331744 kB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our kernel parameters are all the same and I have CONFIG_HIGHMEM enabled in my kernel config. For my own board I have this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;[kernel boot messages]&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Memory: 512MB = 512MB total&lt;/P&gt;&lt;P&gt;Memory: 237596k/237596k available, 286692k reserved, 0K highmem&lt;/P&gt;&lt;P&gt;Linux version 3.10.17 (ralphc@waldorf) (gcc version 4.8.1 (Sourcery CodeBench Lite 2013.11-33) ) #4 SMP Fri Nov 7 11:44:20 GMT 2014&lt;/P&gt;&lt;P&gt;CPU identified as i.MX6DL, silicon rev 1.1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xfff00000 - 0xfffe0000&amp;nbsp;&amp;nbsp; ( 896 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xe0800000 - 0xff000000&amp;nbsp;&amp;nbsp; ( 488 MB)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ***LTIB is 1304MB***&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0xc0000000 - 0xe0000000&amp;nbsp;&amp;nbsp; ( 512 MB)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0xbf000000 - 0xc0000000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 16 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0xc0008000 - 0xc0790f9c&amp;nbsp;&amp;nbsp; (7716 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0xc0791000 - 0xc18e6200&amp;nbsp;&amp;nbsp; (17749 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0xc18e8000 - 0xc1924b60&amp;nbsp;&amp;nbsp; ( 243 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0xc1924b60 - 0xc1983dbc&amp;nbsp;&amp;nbsp; ( 381 kB)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;root@freescale ~$ cat /proc/cpuinfo&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;processor&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0&lt;/P&gt;&lt;P&gt;model name&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : ARMv7 Processor rev 10 (v7l)&lt;/P&gt;&lt;P&gt;BogoMIPS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 790.52&lt;/P&gt;&lt;P&gt;Features&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : swp half thumb fastmult vfp edsp neon vfpv3 tls&lt;/P&gt;&lt;P&gt;CPU implementer : 0x41&lt;/P&gt;&lt;P&gt;CPU architecture: 7&lt;/P&gt;&lt;P&gt;CPU variant&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0x2&lt;/P&gt;&lt;P&gt;CPU part&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0xc09&lt;/P&gt;&lt;P&gt;CPU revision&amp;nbsp;&amp;nbsp;&amp;nbsp; : 10&lt;/P&gt;&lt;P&gt;Hardware&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : Freescale i.MX6 Quad/DualLite (Device Tree)&lt;/P&gt;&lt;P&gt;Revision&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 61011&lt;/P&gt;&lt;P&gt;Serial&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0000000000000000&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;# cat /proc/meminfo&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;MemTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 510728 kB&lt;/P&gt;&lt;P&gt;MemFree:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 342616 kB&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;VmallocTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 499712 kB&lt;/P&gt;&lt;P&gt;VmallocUsed:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7212 kB&lt;/P&gt;&lt;P&gt;VmallocChunk:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 316008 kB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I notice that I have no DMA (2MB) or pkmap allocated on mine (184MB) compared to the LTIB board. Also, the LTIB image has more vmalloc memory than there even is on the board!!! (I only have 512MB according to the datasheet). Could the memory allocation setup be the cause of my problems? There is one other difference and that is in the vpu.imx gstreamer component that is used for decoding mp4 is version 3.0.2 for the LTIB board and 3.0.11 for my board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Nov 2014 14:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Poor-framerates-on-iMX6-Solo-when-decoding-H264/m-p/379783#M54643</guid>
      <dc:creator>ralph__</dc:creator>
      <dc:date>2014-11-07T14:01:43Z</dc:date>
    </item>
  </channel>
</rss>