<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX28-x-windows problems</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-x-windows-problems/m-p/170600#M5454</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi...&lt;BR /&gt;i'm working with an imx28 freescale microprocessor and i work with tftp and nfs. I've installed ltib with imx28 configuration..i'm using the freesclae kernel demo.&lt;/P&gt;&lt;P&gt;The kernel go on and the filesystem the same...i come to the loginand after i write "startx" and the answer is:&lt;BR /&gt;XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6&lt;BR /&gt;_XSERVTransOpen: transport open failed for inet6/freescale:0&lt;BR /&gt;_XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6&lt;BR /&gt;(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base&lt;BR /&gt;(EE) XKB: No components provided for device Virtual core keyboard&lt;BR /&gt;(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base&lt;BR /&gt;(EE) XKB: No components provided for device (unnamed keyboard)&lt;BR /&gt;&lt;BR /&gt;some suggests??&lt;/P&gt;&lt;P&gt;Thank you..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 18 Sep 2011 07:33:40 GMT</pubDate>
    <dc:creator>Nico</dc:creator>
    <dc:date>2011-09-18T07:33:40Z</dc:date>
    <item>
      <title>iMX28-x-windows problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-x-windows-problems/m-p/170600#M5454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi...&lt;BR /&gt;i'm working with an imx28 freescale microprocessor and i work with tftp and nfs. I've installed ltib with imx28 configuration..i'm using the freesclae kernel demo.&lt;/P&gt;&lt;P&gt;The kernel go on and the filesystem the same...i come to the loginand after i write "startx" and the answer is:&lt;BR /&gt;XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6&lt;BR /&gt;_XSERVTransOpen: transport open failed for inet6/freescale:0&lt;BR /&gt;_XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6&lt;BR /&gt;(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base&lt;BR /&gt;(EE) XKB: No components provided for device Virtual core keyboard&lt;BR /&gt;(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base&lt;BR /&gt;(EE) XKB: No components provided for device (unnamed keyboard)&lt;BR /&gt;&lt;BR /&gt;some suggests??&lt;/P&gt;&lt;P&gt;Thank you..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Sep 2011 07:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-x-windows-problems/m-p/170600#M5454</guid>
      <dc:creator>Nico</dc:creator>
      <dc:date>2011-09-18T07:33:40Z</dc:date>
    </item>
  </channel>
</rss>