<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: I/O input voltage tolerance</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-O-input-voltage-tolerance/m-p/170587#M5452</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;An I/O supplied with 1.8 V cannot be overdriven at 2.5 V. The i.MX35 is similar to other i.MX devices and should not be overdriven &amp;gt; 0.3 V above the associated I/O supply rail. A change ticket will be submitted to correct the data sheet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Nov 2012 15:04:56 GMT</pubDate>
    <dc:creator>david_babin</dc:creator>
    <dc:date>2012-11-14T15:04:56Z</dc:date>
    <item>
      <title>I/O input voltage tolerance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-O-input-voltage-tolerance/m-p/170585#M5450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; I need to interface to a i.MX35x processor from a 2.5 volt device.&lt;/P&gt;&lt;P&gt;The i.MX35x I/O Supply voltage is @ 1.8 Volt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the tolerance on the i.MX35x I/O's? e.g. can I directly drive the I/O with 2.5 volt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Nov 2012 21:16:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-O-input-voltage-tolerance/m-p/170585#M5450</guid>
      <dc:creator>robertinant</dc:creator>
      <dc:date>2012-11-09T21:16:14Z</dc:date>
    </item>
    <item>
      <title>Re: I/O input voltage tolerance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-O-input-voltage-tolerance/m-p/170586#M5451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the Datasheet Table 7&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/dsp/doc/data_sheet/MCIMX35SR2CEC.pdf?pspll=1" title="http://cache.freescale.com/files/dsp/doc/data_sheet/MCIMX35SR2CEC.pdf?pspll=1"&gt;http://cache.freescale.com/files/dsp/doc/data_sheet/MCIMX35SR2CEC.pdf?pspll=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Supply voltage (I/O) NVCCmax&amp;nbsp;&amp;nbsp; –0.5&amp;nbsp; to 3.6 V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Nov 2012 19:07:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-O-input-voltage-tolerance/m-p/170586#M5451</guid>
      <dc:creator>4guin4g4</dc:creator>
      <dc:date>2012-11-13T19:07:13Z</dc:date>
    </item>
    <item>
      <title>Re: I/O input voltage tolerance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-O-input-voltage-tolerance/m-p/170587#M5452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;An I/O supplied with 1.8 V cannot be overdriven at 2.5 V. The i.MX35 is similar to other i.MX devices and should not be overdriven &amp;gt; 0.3 V above the associated I/O supply rail. A change ticket will be submitted to correct the data sheet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2012 15:04:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-O-input-voltage-tolerance/m-p/170587#M5452</guid>
      <dc:creator>david_babin</dc:creator>
      <dc:date>2012-11-14T15:04:56Z</dc:date>
    </item>
  </channel>
</rss>