<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: J-Link and iMX6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/J-Link-and-iMX6/m-p/379201#M54493</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;J-Link Commander is very simple tool designed just for testing J-Link,&lt;/P&gt;&lt;P&gt;for operation with i.MX6 seems one needs to use full-featured tools as&lt;/P&gt;&lt;P&gt;described below on segger forums:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.segger.com/j-link-commander.html" title="http://www.segger.com/j-link-commander.html"&gt;SEGGER - The Embedded Experts - J-Link Commander&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://forum.segger.com/index.php?page=Thread&amp;amp;threadID=1550" title="http://forum.segger.com/index.php?page=Thread&amp;amp;threadID=1550"&gt;Getting J-Link working with i.MX6Q - J-Link/Flasher related - SEGGER Forum&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Aug 2014 04:55:52 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-08-26T04:55:52Z</dc:date>
    <item>
      <title>J-Link and iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/J-Link-and-iMX6/m-p/379200#M54492</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom board with a Freescale iMX6 Solo CPU, and trying to use J-Link Commander to connect to the device.&lt;/P&gt;&lt;P&gt;I'm getting an error message, as seen in the log below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas what might be the reason for this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/////// Log Start /////&lt;/P&gt;&lt;P&gt;SEGGER J-Link Commander V4.90b ('?' for help)&lt;/P&gt;&lt;P&gt;Compiled Aug 14 2014 09:41:15&lt;/P&gt;&lt;P&gt;DLL version V4.90b, compiled Aug 14 2014 09:40:57&lt;/P&gt;&lt;P&gt;Firmware: J-Link Ultra V4 compiled Jul 28 2014 08:28:13&lt;/P&gt;&lt;P&gt;Hardware: V4.00&lt;/P&gt;&lt;P&gt;S/N: 504301229&lt;/P&gt;&lt;P&gt;Feature(s): RDI, FlashBP, FlashDL, JFlash, GDB&lt;/P&gt;&lt;P&gt;VTarget = 3.116V&lt;/P&gt;&lt;P&gt;Info: TotalIRLen = 13, IRPrint = 0x0101&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WARNING: At least one of the connected devices is not JTAG compliant (IEEE Std 1149.1, 7.1.1.d, IR-cells). (NumDevices = 3, NumBitsSet=2)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Info: ARM AP[0]: 0x44770001, AHB-AP&lt;/P&gt;&lt;P&gt;Info: ARM AP[1]: 0x24770002, APB-AP&lt;/P&gt;&lt;P&gt;Info: Found Cortex-A9 r2p10&lt;/P&gt;&lt;P&gt;Info: 6 code breakpoints, 4 data breakpoints&lt;/P&gt;&lt;P&gt;Info: Debug architecture ARMv7.0&lt;/P&gt;&lt;P&gt;Info: Data endian: little&lt;/P&gt;&lt;P&gt;Info: Main ID register: 0x412FC09A&lt;/P&gt;&lt;P&gt;Info: L1 (I-cache): 32 KB, 256 sets, LineSize 32 bytes, 4-way&lt;/P&gt;&lt;P&gt;Info: L1 (D-cache): 32 KB, 256 sets, LineSize 32 bytes, 4-way&lt;/P&gt;&lt;P&gt;Info: System control register:&lt;/P&gt;&lt;P&gt;Info:&amp;nbsp;&amp;nbsp; Instruction endian: little&lt;/P&gt;&lt;P&gt;Info:&amp;nbsp;&amp;nbsp; Level-1 instruction cache enabled&lt;/P&gt;&lt;P&gt;Info:&amp;nbsp;&amp;nbsp; Level-1 data cache disabled&lt;/P&gt;&lt;P&gt;Info:&amp;nbsp;&amp;nbsp; MMU disabled&lt;/P&gt;&lt;P&gt;Info:&amp;nbsp;&amp;nbsp; Branch prediction disabled&lt;/P&gt;&lt;P&gt;Found 3 JTAG devices, Total IRLen = 13:&lt;/P&gt;&lt;P&gt; #0 Id: 0x4BA00477, IRLen: 04, IRPrint: 0x1, CoreSight JTAG-DP (ARM)&lt;/P&gt;&lt;P&gt; #1 Id: 0x00000001&lt;/P&gt;&lt;P&gt; #2 Id: 0x1891B01D&lt;/P&gt;&lt;P&gt;Cortex-A9 identified.&lt;/P&gt;&lt;P&gt;Target interface speed: 100 kHz&lt;/P&gt;&lt;P&gt;J-Link&amp;gt;r&lt;/P&gt;&lt;P&gt;Reset delay: 0 ms&lt;/P&gt;&lt;P&gt;Reset type NORMAL: Toggle reset pin and halt CPU core.&lt;/P&gt;&lt;P&gt;Info: Cortex-A/R (reset): Re-initializing debug logic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WARNING: CPU not halted after Reset, halting using Halt request&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;****** Error: Bad JTAG communication: Write to IR: Expected 0x1, got 0xF (TAP Command : 10) @ Off 0x5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;//////// End //////////&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Erez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Aug 2014 13:52:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/J-Link-and-iMX6/m-p/379200#M54492</guid>
      <dc:creator>erezsteinberg</dc:creator>
      <dc:date>2014-08-25T13:52:04Z</dc:date>
    </item>
    <item>
      <title>Re: J-Link and iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/J-Link-and-iMX6/m-p/379201#M54493</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;J-Link Commander is very simple tool designed just for testing J-Link,&lt;/P&gt;&lt;P&gt;for operation with i.MX6 seems one needs to use full-featured tools as&lt;/P&gt;&lt;P&gt;described below on segger forums:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.segger.com/j-link-commander.html" title="http://www.segger.com/j-link-commander.html"&gt;SEGGER - The Embedded Experts - J-Link Commander&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://forum.segger.com/index.php?page=Thread&amp;amp;threadID=1550" title="http://forum.segger.com/index.php?page=Thread&amp;amp;threadID=1550"&gt;Getting J-Link working with i.MX6Q - J-Link/Flasher related - SEGGER Forum&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Aug 2014 04:55:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/J-Link-and-iMX6/m-p/379201#M54493</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-08-26T04:55:52Z</dc:date>
    </item>
    <item>
      <title>Re: J-Link and iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/J-Link-and-iMX6/m-p/379202#M54494</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #57595a; font-family: 'Trebuchet MS', Arial, sans-serif;"&gt;I found that for iMX6, the device must be given to J-Link in the command line.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #57595a; font-family: 'Trebuchet MS', Arial, sans-serif;"&gt;E.g. &lt;/P&gt;&lt;P style="color: #57595a; font-family: 'Trebuchet MS', Arial, sans-serif;"&gt;&lt;/P&gt;&lt;P style="color: #57595a; font-family: 'Trebuchet MS', Arial, sans-serif;"&gt;JLINK.EXE -Device MCIMX6S1&lt;/P&gt;&lt;P style="color: #57595a; font-family: 'Trebuchet MS', Arial, sans-serif;"&gt;&lt;/P&gt;&lt;P style="color: #57595a; font-family: 'Trebuchet MS', Arial, sans-serif;"&gt;Then, reset works fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Aug 2014 05:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/J-Link-and-iMX6/m-p/379202#M54494</guid>
      <dc:creator>erezsteinberg</dc:creator>
      <dc:date>2014-08-26T05:38:24Z</dc:date>
    </item>
  </channel>
</rss>