<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB isochronous transfer queries in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-isochronous-transfer-queries/m-p/379176#M54477</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have some queries regarding usb isochronous endpoint operation for device controller. I am referring to the document "IMX6DQRM-Rev1.pdf" section 65.4.5. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. During an isochronous in transfer, does Dqh contain only one Dtd which has only one&amp;nbsp; Iso (micro)frame or does Dqh contain one or multiple linked Dtds which has an input buffer filled with many iso frame/microframe? If multiple then how does device controller identify (micro)frame boundaries in dtds? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Is there any DMA operation involved while moving data between DTD and TX/RX FIFO? If DMA is present then what is the DMA restriction of buffer size and start address alignment? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Barindam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Apr 2015 10:17:49 GMT</pubDate>
    <dc:creator>binaeksarkar</dc:creator>
    <dc:date>2015-04-06T10:17:49Z</dc:date>
    <item>
      <title>USB isochronous transfer queries</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-isochronous-transfer-queries/m-p/379176#M54477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have some queries regarding usb isochronous endpoint operation for device controller. I am referring to the document "IMX6DQRM-Rev1.pdf" section 65.4.5. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. During an isochronous in transfer, does Dqh contain only one Dtd which has only one&amp;nbsp; Iso (micro)frame or does Dqh contain one or multiple linked Dtds which has an input buffer filled with many iso frame/microframe? If multiple then how does device controller identify (micro)frame boundaries in dtds? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Is there any DMA operation involved while moving data between DTD and TX/RX FIFO? If DMA is present then what is the DMA restriction of buffer size and start address alignment? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Barindam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Apr 2015 10:17:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-isochronous-transfer-queries/m-p/379176#M54477</guid>
      <dc:creator>binaeksarkar</dc:creator>
      <dc:date>2015-04-06T10:17:49Z</dc:date>
    </item>
    <item>
      <title>Re: USB isochronous transfer queries</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-isochronous-transfer-queries/m-p/379177#M54478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Barindam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please specify if you still having these queries or you are already on the stage mentioned on your &lt;A _jive_internal="true" href="https://community.nxp.com/thread/351838"&gt;other thread&lt;/A&gt;?&lt;/P&gt;&lt;P&gt;Additionally, you could take a look to application note &lt;A href="http://www.freescale.com/files/32bit/doc/app_note/AN4589.pdf"&gt;AN4589 “Configuring USB on i.MX 6 Series &lt;/A&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&lt;A href="http://www.freescale.com/files/32bit/doc/app_note/AN4589.pdf"&gt;Processors”&lt;/A&gt;, &lt;/SPAN&gt;which provides useful information regarding USB on i.MX6 series.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Apr 2015 23:38:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-isochronous-transfer-queries/m-p/379177#M54478</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-04-09T23:38:53Z</dc:date>
    </item>
  </channel>
</rss>