<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic OV5640 MIPI-CSI2 driver - 60 fps capture? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/OV5640-MIPI-CSI2-driver-60-fps-capture/m-p/378460#M54303</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a OmniVision OV5640 MIPI-CSI2 image sensor with a iMX6 Quad board.&lt;/P&gt;&lt;P&gt;I have seen in the datasheets that 720p60 capture can be done using OV5640. However, the drivers does not seem to support 60 fps capture? What changes must be done to obtain 60 fps capture?&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 05 Apr 2015 15:32:03 GMT</pubDate>
    <dc:creator>abhishekm</dc:creator>
    <dc:date>2015-04-05T15:32:03Z</dc:date>
    <item>
      <title>OV5640 MIPI-CSI2 driver - 60 fps capture?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OV5640-MIPI-CSI2-driver-60-fps-capture/m-p/378460#M54303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a OmniVision OV5640 MIPI-CSI2 image sensor with a iMX6 Quad board.&lt;/P&gt;&lt;P&gt;I have seen in the datasheets that 720p60 capture can be done using OV5640. However, the drivers does not seem to support 60 fps capture? What changes must be done to obtain 60 fps capture?&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Apr 2015 15:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OV5640-MIPI-CSI2-driver-60-fps-capture/m-p/378460#M54303</guid>
      <dc:creator>abhishekm</dc:creator>
      <dc:date>2015-04-05T15:32:03Z</dc:date>
    </item>
    <item>
      <title>Re: OV5640 MIPI-CSI2 driver - 60 fps capture?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OV5640-MIPI-CSI2-driver-60-fps-capture/m-p/378461#M54304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Abhishek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look for answer on below link&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/330744"&gt;OV5640 MIPI-CSI2 driver - why the limitations?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 00:23:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OV5640-MIPI-CSI2-driver-60-fps-capture/m-p/378461#M54304</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-07T00:23:24Z</dc:date>
    </item>
    <item>
      <title>Re: OV5640 MIPI-CSI2 driver - 60 fps capture?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OV5640-MIPI-CSI2-driver-60-fps-capture/m-p/378462#M54305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had gone through that link. Yuri has posted that " it is required to create / support special command sequences (tables) to program&lt;/P&gt;&lt;P style="font-size: 13px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;a camera (say, via I2C) for different modes / frame frequencies". Can you elaborate on this. &lt;/P&gt;&lt;P&gt;I had also gone through the discussion &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 13px;"&gt;on the meta-freescale mailing list. But I could not find the required solution. In the discussion on the &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 13px;"&gt;on the meta-freescale mailing list, I read about changing i2c blobs . I am not aware of it. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-size: 13px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;What are the changes required for 60 fps capture?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 04:35:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OV5640-MIPI-CSI2-driver-60-fps-capture/m-p/378462#M54305</guid>
      <dc:creator>abhishekm</dc:creator>
      <dc:date>2015-04-07T04:35:17Z</dc:date>
    </item>
    <item>
      <title>Re: OV5640 MIPI-CSI2 driver - 60 fps capture?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OV5640-MIPI-CSI2-driver-60-fps-capture/m-p/378463#M54306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Abhishek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seeems these commands are proprietary OmniVision &lt;/P&gt;&lt;P&gt;so would suggest to apply to OmniVision tech support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 07:50:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OV5640-MIPI-CSI2-driver-60-fps-capture/m-p/378463#M54306</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-07T07:50:14Z</dc:date>
    </item>
  </channel>
</rss>