<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: EGL problems</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/EGL-problems/m-p/148093#M543</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Like usual, it takes posting a problem to fix it yourself! :-)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Dec 2010 18:01:21 GMT</pubDate>
    <dc:creator>RobSavoye</dc:creator>
    <dc:date>2010-12-22T18:01:21Z</dc:date>
    <item>
      <title>EGL problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EGL-problems/m-p/148092#M542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to use the OpenVG support in L2.6.31_10.07.11_ER, and as far as I can tell, there is a bug in the lower level EGL support OpenVG depends on. ThIs is on a Freescale Babbage board. Basically eglInitialize() always returns a failure, yet the error code says success! If I force it to continue, it fails on the next EGL call, so it's definetely not initialized. The code I'm using runs on 3 other platforms, so I know it's not a code problem. Even eglinfo fails to initialize.&lt;/P&gt;&lt;P&gt;I'm now downloading the newer ltib sources from Freescale for L2.6.35_10.11.01_ER that I hope solves my problem. I figured it would be good to ask here, incase I'm just doing something stupid. I do have the amd_gpu_bin files installed, and the gpu driver is enabled in my kernel builds. I've also tried both the&lt;/P&gt;&lt;P&gt;gpu_z430 and gsl modules with no luck.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Dec 2010 17:42:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EGL-problems/m-p/148092#M542</guid>
      <dc:creator>RobSavoye</dc:creator>
      <dc:date>2010-12-21T17:42:22Z</dc:date>
    </item>
    <item>
      <title>Re: EGL problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EGL-problems/m-p/148093#M543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Like usual, it takes posting a problem to fix it yourself! :-)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Dec 2010 18:01:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EGL-problems/m-p/148093#M543</guid>
      <dc:creator>RobSavoye</dc:creator>
      <dc:date>2010-12-22T18:01:21Z</dc:date>
    </item>
  </channel>
</rss>