<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQuestion, i.MX28 WINCE6 BSP LAN problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-WINCE6-BSP-LAN-problem/m-p/377988#M54233</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On my customer’s lab, they face the issue that i.MX28 LAN communication could stop in the ESD test.&lt;/P&gt;&lt;P&gt;The test was done according to the ESD standard, IEC610004-4.&lt;/P&gt;&lt;P&gt;The issue could be seen at when fast transient noise was added and LAN traffic was high.&lt;/P&gt;&lt;P&gt;BTW, they use LAN8720A for PHY.&lt;/P&gt;&lt;P&gt;OS they use is based on your WINCE6 BSP(WCE600_10.08.02_SDK).&lt;/P&gt;&lt;P&gt;They did additional test on MCIMX28EVKJ board and found a problem.&lt;/P&gt;&lt;P&gt;The following log was seen when CRC error packets were sent to i.MX28 from network tester.&lt;/P&gt;&lt;P&gt;&amp;gt; Running TouchCalibrate&lt;/P&gt;&lt;P&gt;&amp;gt; Event is successfully created 9d0703&lt;/P&gt;&lt;P&gt;&amp;gt; +OEMSetAlarmTime(3/12/2006 2:0:0.000)&lt;/P&gt;&lt;P&gt;&amp;gt; Alarm to be set is OK:&amp;nbsp; 2006/3/12, 2:0:0&amp;nbsp; Day of week:0 &lt;/P&gt;&lt;P&gt;&amp;gt; Exception 'Data Abort' (4): Thread-Id=02690002(pth=837d130c), Proc-Id=00400002(pprc=81dfb308) 'NK.EXE', VM-active=00db00&lt;/P&gt;&lt;P&gt;&amp;gt; 02(pprc=87fbfd40) 'shell.exe'&lt;/P&gt;&lt;P&gt;&amp;gt; PC=c0a63790(enet.dll+0x00003790) RA=d07f0e8c(???+0xd07f0e8c) SP=d088fdd0, BVA=0000000c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WinCE generated the exception always and the communication stopped.&lt;/P&gt;&lt;P&gt;From the log, they believe that the code in BSP that Freescale provided contains a incorrect code.&lt;/P&gt;&lt;P&gt;That is;&lt;/P&gt;&lt;P&gt;When the CRC error packets are received, it should be ignored or retry request should be created, it should not generate exception.&lt;/P&gt;&lt;P&gt;Could you give your comment on that?&lt;/P&gt;&lt;P&gt;If you have a patch code, could you provide it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Feb 2015 10:49:41 GMT</pubDate>
    <dc:creator>Aemj</dc:creator>
    <dc:date>2015-02-16T10:49:41Z</dc:date>
    <item>
      <title>Question, i.MX28 WINCE6 BSP LAN problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-WINCE6-BSP-LAN-problem/m-p/377988#M54233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On my customer’s lab, they face the issue that i.MX28 LAN communication could stop in the ESD test.&lt;/P&gt;&lt;P&gt;The test was done according to the ESD standard, IEC610004-4.&lt;/P&gt;&lt;P&gt;The issue could be seen at when fast transient noise was added and LAN traffic was high.&lt;/P&gt;&lt;P&gt;BTW, they use LAN8720A for PHY.&lt;/P&gt;&lt;P&gt;OS they use is based on your WINCE6 BSP(WCE600_10.08.02_SDK).&lt;/P&gt;&lt;P&gt;They did additional test on MCIMX28EVKJ board and found a problem.&lt;/P&gt;&lt;P&gt;The following log was seen when CRC error packets were sent to i.MX28 from network tester.&lt;/P&gt;&lt;P&gt;&amp;gt; Running TouchCalibrate&lt;/P&gt;&lt;P&gt;&amp;gt; Event is successfully created 9d0703&lt;/P&gt;&lt;P&gt;&amp;gt; +OEMSetAlarmTime(3/12/2006 2:0:0.000)&lt;/P&gt;&lt;P&gt;&amp;gt; Alarm to be set is OK:&amp;nbsp; 2006/3/12, 2:0:0&amp;nbsp; Day of week:0 &lt;/P&gt;&lt;P&gt;&amp;gt; Exception 'Data Abort' (4): Thread-Id=02690002(pth=837d130c), Proc-Id=00400002(pprc=81dfb308) 'NK.EXE', VM-active=00db00&lt;/P&gt;&lt;P&gt;&amp;gt; 02(pprc=87fbfd40) 'shell.exe'&lt;/P&gt;&lt;P&gt;&amp;gt; PC=c0a63790(enet.dll+0x00003790) RA=d07f0e8c(???+0xd07f0e8c) SP=d088fdd0, BVA=0000000c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WinCE generated the exception always and the communication stopped.&lt;/P&gt;&lt;P&gt;From the log, they believe that the code in BSP that Freescale provided contains a incorrect code.&lt;/P&gt;&lt;P&gt;That is;&lt;/P&gt;&lt;P&gt;When the CRC error packets are received, it should be ignored or retry request should be created, it should not generate exception.&lt;/P&gt;&lt;P&gt;Could you give your comment on that?&lt;/P&gt;&lt;P&gt;If you have a patch code, could you provide it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Feb 2015 10:49:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-WINCE6-BSP-LAN-problem/m-p/377988#M54233</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-02-16T10:49:41Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX28 WINCE6 BSP LAN problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-WINCE6-BSP-LAN-problem/m-p/377989#M54234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Per the Exception Data Abort it looks like you need to initialize a global environment variable for ENET such as:&lt;/P&gt;&lt;P&gt;BSP_ENET1= 1&lt;/P&gt;&lt;P&gt;BSP_ENET2= 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or you should try and test the &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;WCE600_10.08_SDK_PATCH&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Alfredo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Feb 2015 16:52:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-WINCE6-BSP-LAN-problem/m-p/377989#M54234</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2015-02-19T16:52:52Z</dc:date>
    </item>
  </channel>
</rss>