<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: UART as wake up source</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UART-as-wake-up-source/m-p/377963#M54225</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vishakh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;first byte may be missed, this is expected behaviour,&lt;/P&gt;&lt;P&gt;if you are using dma (dma is made up of a 36-byte fifo), below patches are recommended.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/304428"&gt;iMX53 dma and uart&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 27 Dec 2014 11:27:57 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-12-27T11:27:57Z</dc:date>
    <item>
      <title>UART as wake up source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-as-wake-up-source/m-p/377962#M54224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using UART as wake up source in linux kernel 2.6.35.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I send 300 bytes from the system to the board when board is in low power state, in board side first 36 bytes are missing after system wake up.&lt;/P&gt;&lt;P&gt;Is this the expected behavior or else will I be&amp;nbsp; able to receive all the data sent while resuming from low power mode to normal mode? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Vishakh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 Dec 2014 09:36:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-as-wake-up-source/m-p/377962#M54224</guid>
      <dc:creator>vishakh</dc:creator>
      <dc:date>2014-12-27T09:36:41Z</dc:date>
    </item>
    <item>
      <title>Re: UART as wake up source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-as-wake-up-source/m-p/377963#M54225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vishakh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;first byte may be missed, this is expected behaviour,&lt;/P&gt;&lt;P&gt;if you are using dma (dma is made up of a 36-byte fifo), below patches are recommended.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/304428"&gt;iMX53 dma and uart&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 Dec 2014 11:27:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-as-wake-up-source/m-p/377963#M54225</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-12-27T11:27:57Z</dc:date>
    </item>
    <item>
      <title>Re: UART as wake up source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-as-wake-up-source/m-p/377964#M54226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to increase the UART3_DMA_RXBUFSIZE&amp;nbsp; to 2048. But this is not solving the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I increase the baud rate, more bytes are missing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will you please let me know is there any other way to solve this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It will be helpful if you explain how UART will receive the data on imx53 while resuming from the suspended state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Vishakh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jan 2015 12:49:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-as-wake-up-source/m-p/377964#M54226</guid>
      <dc:creator>vishakh</dc:creator>
      <dc:date>2015-01-05T12:49:56Z</dc:date>
    </item>
    <item>
      <title>Re: UART as wake up source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-as-wake-up-source/m-p/377965#M54227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vishakh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;are you using flow control for DMA ?&lt;/P&gt;&lt;P&gt;UART flow control should be used for DMA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jan 2015 15:14:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-as-wake-up-source/m-p/377965#M54227</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-05T15:14:18Z</dc:date>
    </item>
  </channel>
</rss>