<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Configuring the parallel camera IO pins. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-the-parallel-camera-IO-pins/m-p/377172#M54123</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Awesome, thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One other related question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Although the camera interface will be operated in 16-bit mode, we only have 14 bits of data from the camera, so will be setting the two most-significant bits to 0.&lt;/P&gt;&lt;P&gt;If we instead just configure those pins for alternate functions, instead of connecting them to ground, what values would the camera interface read for those bits when they aren't physically connected to the pads via the IOmux?&amp;nbsp; We've almost run out of spare pins, so getting two more pins back for use as GPIOs would be fantastic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Camz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Sep 2014 17:45:00 GMT</pubDate>
    <dc:creator>camz</dc:creator>
    <dc:date>2014-09-18T17:45:00Z</dc:date>
    <item>
      <title>Configuring the parallel camera IO pins.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-the-parallel-camera-IO-pins/m-p/377170#M54121</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm helping design a board based on the i.MX6Q processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The design has a parallel camera that will use the Bayer/Raw data mode to receive 16-bits of camera data.&lt;/P&gt;&lt;P&gt;I have planned to use the CSI0_DAT0 thru CSI0_DAT15 inputs, but in looking at the Sabre for Smart Devices reference schematic, the connection of the OV5642 parallel camera uses CSI0_DAT12 thru CSI0_DAT19 for an 8-bit input stream.&amp;nbsp; When not using all 20-bits for input, should I be using the high bits, or the low bits?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The i.MX6Q reference manual skims over the various modes and leaves out a lot of details on how to configure and hook up camera inputs, if there is a document that describes this, I'd appreciate being pointed in the right direction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Camz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2014 19:17:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-the-parallel-camera-IO-pins/m-p/377170#M54121</guid>
      <dc:creator>camz</dc:creator>
      <dc:date>2014-09-17T19:17:08Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring the parallel camera IO pins.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-the-parallel-camera-IO-pins/m-p/377171#M54122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When not using all 20-bits for input, one should use the high bits.&lt;/P&gt;&lt;P&gt;Regarding docs please check i.MX_6Dual6Quad_BSP_Porting_Guide.pdf,&lt;/P&gt;&lt;P&gt;i.MX_6Dual6Quad_Linux_Reference_Manual.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fasp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz"&gt;L3.0.35_4.1.0_LINUX_DOCS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For software examples it is better to look for Community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2014 23:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-the-parallel-camera-IO-pins/m-p/377171#M54122</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-09-17T23:46:52Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring the parallel camera IO pins.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-the-parallel-camera-IO-pins/m-p/377172#M54123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Awesome, thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One other related question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Although the camera interface will be operated in 16-bit mode, we only have 14 bits of data from the camera, so will be setting the two most-significant bits to 0.&lt;/P&gt;&lt;P&gt;If we instead just configure those pins for alternate functions, instead of connecting them to ground, what values would the camera interface read for those bits when they aren't physically connected to the pads via the IOmux?&amp;nbsp; We've almost run out of spare pins, so getting two more pins back for use as GPIOs would be fantastic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Camz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Sep 2014 17:45:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-the-parallel-camera-IO-pins/m-p/377172#M54123</guid>
      <dc:creator>camz</dc:creator>
      <dc:date>2014-09-18T17:45:00Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring the parallel camera IO pins.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-the-parallel-camera-IO-pins/m-p/377173#M54124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid that internally they will be floating,&lt;/P&gt;&lt;P&gt;so camera interface will read random data for those bits.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Sep 2014 23:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-the-parallel-camera-IO-pins/m-p/377173#M54124</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-09-18T23:46:59Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring the parallel camera IO pins.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-the-parallel-camera-IO-pins/m-p/377174#M54125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Sep 2014 13:13:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-the-parallel-camera-IO-pins/m-p/377174#M54125</guid>
      <dc:creator>camz</dc:creator>
      <dc:date>2014-09-19T13:13:40Z</dc:date>
    </item>
  </channel>
</rss>