<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Key Generation</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Key-Generation/m-p/377169#M54120</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Apoorva&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think one can look at SDK (caam_test.c)&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX 6Series Platform SDK&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : Bare-metal SDK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also i.MX_6_Linux_Reference_Manual.pdf sect.51.5 API Interface Level&lt;/P&gt;&lt;P&gt;from &lt;A href="https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fasp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz"&gt;L3.0.35_4.1.0_LINUX_DOCS&lt;/A&gt; &lt;/P&gt;&lt;P&gt;gives option with usage caamrng module and /dev/hw_random&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Dec 2014 11:28:42 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-12-26T11:28:42Z</dc:date>
    <item>
      <title>Key Generation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Key-Generation/m-p/377167#M54118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on iMX6 and have written the code to generate the random numbers. Now, I need to generate the keys and store them (but not perform any encryption yet). Like for Random Number Generation we have, we had RNG. Do we have a similar thing for generation of keys? (i.e. like I know the keys are generated when encryption is being performed using any of the algorithms. But is it possible to only generate a key without using any encryption algorithm?)&lt;BR /&gt;I hope my query is clear. :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Dec 2014 08:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Key-Generation/m-p/377167#M54118</guid>
      <dc:creator>apoorvabhatia</dc:creator>
      <dc:date>2014-12-26T08:57:29Z</dc:date>
    </item>
    <item>
      <title>Re: Key Generation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Key-Generation/m-p/377168#M54119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Basically, does key derivation function (KDF) which will derive the key from the Master key is provided by CAAM or do we have to write it at software level?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Dec 2014 09:20:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Key-Generation/m-p/377168#M54119</guid>
      <dc:creator>apoorvabhatia</dc:creator>
      <dc:date>2014-12-26T09:20:43Z</dc:date>
    </item>
    <item>
      <title>Re: Key Generation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Key-Generation/m-p/377169#M54120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Apoorva&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think one can look at SDK (caam_test.c)&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX 6Series Platform SDK&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : Bare-metal SDK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also i.MX_6_Linux_Reference_Manual.pdf sect.51.5 API Interface Level&lt;/P&gt;&lt;P&gt;from &lt;A href="https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fasp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz"&gt;L3.0.35_4.1.0_LINUX_DOCS&lt;/A&gt; &lt;/P&gt;&lt;P&gt;gives option with usage caamrng module and /dev/hw_random&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Dec 2014 11:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Key-Generation/m-p/377169#M54120</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-12-26T11:28:42Z</dc:date>
    </item>
  </channel>
</rss>