<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX53 Low power VDDA in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Low-power-VDDA/m-p/376079#M53949</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp;&amp;nbsp; Please use the recent i.MX53 Datasheet(s) regarding hardware specs.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;In particular&amp;nbsp; :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;VDDA - Memory arrays voltage – should be in range 1.25 - 1.35 V under normal&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;operation, and it should be in range 0.9 - 1.35 V is STOP mode.&lt;BR /&gt;The same statement takes place for VDDAL1 (L1 Cache Memory &lt;BR /&gt;arrays voltage). There are no other restrictions.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Apr 2015 06:49:39 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-04-07T06:49:39Z</dc:date>
    <item>
      <title>i.MX53 Low power VDDA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Low-power-VDDA/m-p/376078#M53948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am having problems understanding what should be done with VDDA on i.MX535 for low power state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The referernce manual 9.5 says:&lt;/P&gt;&lt;P&gt;"All the memories' array supply (VDDA/VDDAL1) and VDD_STATE are connected to a&lt;/P&gt;&lt;P&gt;dedicated supply pin on i.MX53 this is done due to the fact that the memories array&lt;/P&gt;&lt;P&gt;supply does not support a voltage lower then 1.08V. So during DVFS the periphery&lt;/P&gt;&lt;P&gt;supply is lowered along with the rest of the chip."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However the recommended value in stop mode given in AN4604 "Interfacing the MC34709 with the i.MX53" is 0.95V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Furthermore the reference manual also says&lt;/P&gt;&lt;P&gt;"The dedicated array supply needs to be lowered to support a&lt;/P&gt;&lt;P&gt;maximal difference between VDDA/VDDAL1 and VDD of&lt;/P&gt;&lt;P&gt;300mV."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is not clear what supply is meant by VDD. I presume this refers to the i.MX53 peripheral supply (VCC)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When VDDA is not supplied by the PMIC but via the i.MX53 internal 1.2V LDO (VDD_DIG_PLL) (as recommended in AN4604) the voltage reduction of the VDDA has to be done by software *before* stop mode is entered and the PMIC reduces VDDC. This means that, for a short time:&lt;/P&gt;&lt;P&gt;VDDA = 0.95&lt;/P&gt;&lt;P&gt;VCC = 1.3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hence difference = 350mV&amp;nbsp; &amp;gt; 300mV&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, is it OK to reduce VDDA to 0.95V while the processor is still running?&lt;/P&gt;&lt;P&gt;Unless, VDDA is connected to a dedicated PMIC supply there doesn't seem to be an alternative...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Apr 2015 08:25:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Low-power-VDDA/m-p/376078#M53948</guid>
      <dc:creator>mfuzzey</dc:creator>
      <dc:date>2015-04-03T08:25:13Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 Low power VDDA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Low-power-VDDA/m-p/376079#M53949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp;&amp;nbsp; Please use the recent i.MX53 Datasheet(s) regarding hardware specs.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;In particular&amp;nbsp; :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;VDDA - Memory arrays voltage – should be in range 1.25 - 1.35 V under normal&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;operation, and it should be in range 0.9 - 1.35 V is STOP mode.&lt;BR /&gt;The same statement takes place for VDDAL1 (L1 Cache Memory &lt;BR /&gt;arrays voltage). There are no other restrictions.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 06:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Low-power-VDDA/m-p/376079#M53949</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-04-07T06:49:39Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 Low power VDDA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Low-power-VDDA/m-p/376080#M53950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for this information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So this means that it is not possible to reduce VDDA below 1.25V whilst respecting the constraints if VDDA is supplied from the internal LDO (as suggested in &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;AN4604) because we have to program the i.MX53 IOMUXC GPR1 by software *before* entering STOP mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If a dedicated supply from the PMIC is used then this does not apply since the voltage can be reduced by hardware handshake with the PMIC *after* entering stop mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 09:02:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Low-power-VDDA/m-p/376080#M53950</guid>
      <dc:creator>mfuzzey</dc:creator>
      <dc:date>2015-04-07T09:02:08Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 Low power VDDA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Low-power-VDDA/m-p/376081#M53951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Yes, an external PMIC is required for STOP mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Apr 2015 05:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Low-power-VDDA/m-p/376081#M53951</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-04-08T05:32:03Z</dc:date>
    </item>
  </channel>
</rss>