<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Copy entire folder structure using Mfgtool</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Copy-entire-folder-structure-using-Mfgtool/m-p/375585#M53835</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Apparently the write command in the WinCE (nk.nb0) does not support full folder directory, and the only way of fixing this is to modify the image to allow it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Oct 2014 10:22:19 GMT</pubDate>
    <dc:creator>stephenhewitson</dc:creator>
    <dc:date>2014-10-20T10:22:19Z</dc:date>
    <item>
      <title>Copy entire folder structure using Mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Copy-entire-folder-structure-using-Mfgtool/m-p/375583#M53833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use mfgtool to push a WinCE image ("nk.nb0") to an iMX28. As part of this process I also want to send the application we will be running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently we are required to plug a USB stick containing the application into the product and copy the *.cab file across manually, followed by unpacking the application.&lt;/P&gt;&lt;P&gt;I've seen that it might be possible to call &amp;lt;CMD type="push" body="mkdir /test"/&amp;gt; to create a folder, but is it possible to define a &lt;SPAN style="text-decoration: line-through;"&gt;file&lt;/SPAN&gt; (or entire unpacked folder structure) that is copied across by mfgtool?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT:&lt;/P&gt;&lt;P&gt;Ok, so I can send individual files using&lt;/P&gt;&lt;PRE __default_attr="xml" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_14087049081356346" jivemacro_uid="_14087049081356346" modifiedtitle="true"&gt;
&lt;P style="margin-top: 6.0pt; margin-bottom: 6.0pt;"&gt;&amp;lt;CMD type="push" body="filename:NANDFlash\\sandy.mp3"&amp;gt;Specify the file name and path in the board.&amp;lt;/CMD&amp;gt;&lt;/P&gt;
&lt;P style="margin-top: 6.0pt; margin-bottom: 6.0pt;"&gt;&amp;lt;CMD type="push" body="send" file="files/sandy.mp3"&amp;gt;Sending a file from the host.&amp;lt;/CMD&amp;gt;&lt;/P&gt;
&lt;/PRE&gt;&lt;P style="margin-top: 6.0pt; margin-bottom: 6.0pt;"&gt;I'd still be interested if an entire folder structure (subfolders and files) was possible, without having to send each file separately.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Aug 2014 10:52:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Copy-entire-folder-structure-using-Mfgtool/m-p/375583#M53833</guid>
      <dc:creator>stephenhewitson</dc:creator>
      <dc:date>2014-08-22T10:52:29Z</dc:date>
    </item>
    <item>
      <title>Re: Copy entire folder structure using Mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Copy-entire-folder-structure-using-Mfgtool/m-p/375584#M53834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, so I can definitely push a file across, but I've not managed to create a subfolder yet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone managed to do this, or at least could point me in the right direction?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Aug 2014 15:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Copy-entire-folder-structure-using-Mfgtool/m-p/375584#M53834</guid>
      <dc:creator>stephenhewitson</dc:creator>
      <dc:date>2014-08-26T15:41:21Z</dc:date>
    </item>
    <item>
      <title>Re: Copy entire folder structure using Mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Copy-entire-folder-structure-using-Mfgtool/m-p/375585#M53835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Apparently the write command in the WinCE (nk.nb0) does not support full folder directory, and the only way of fixing this is to modify the image to allow it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Oct 2014 10:22:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Copy-entire-folder-structure-using-Mfgtool/m-p/375585#M53835</guid>
      <dc:creator>stephenhewitson</dc:creator>
      <dc:date>2014-10-20T10:22:19Z</dc:date>
    </item>
  </channel>
</rss>