<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6Sololite EVK Board Cannot Install Apps</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Sololite-EVK-Board-Cannot-Install-Apps/m-p/374715#M53664</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Nicholas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using ADB to install the APK?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Apr 2015 13:32:21 GMT</pubDate>
    <dc:creator>SergioSolis</dc:creator>
    <dc:date>2015-04-14T13:32:21Z</dc:date>
    <item>
      <title>i.MX6Sololite EVK Board Cannot Install Apps</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Sololite-EVK-Board-Cannot-Install-Apps/m-p/374713#M53662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Android 4.0.4 image that comes packaged with the EVK board can install APK files from the internet as long as I enable "unknown sources" under security settings and "usb debugging" under developer options.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I built a version of Android 4.0.4 loosely following the instructions in file 13.5.0_Android_User_Guide from IMX6_R13.5_ANDROID_DOCS_BUNDLE. The built Android seems to work; however, whenever I try to install a downloaded APK file it fails with on-screen message "Application not installed". No serial output is generated when the application fails to install. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help me debug and fix this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2015 17:41:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Sololite-EVK-Board-Cannot-Install-Apps/m-p/374713#M53662</guid>
      <dc:creator>nicholassaulnie</dc:creator>
      <dc:date>2015-04-02T17:41:12Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Sololite EVK Board Cannot Install Apps</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Sololite-EVK-Board-Cannot-Install-Apps/m-p/374714#M53663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible that the system would generate an error when it failed to install the app? If so, where would I look to see this error?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 15:46:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Sololite-EVK-Board-Cannot-Install-Apps/m-p/374714#M53663</guid>
      <dc:creator>nicholassaulnie</dc:creator>
      <dc:date>2015-04-07T15:46:42Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Sololite EVK Board Cannot Install Apps</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Sololite-EVK-Board-Cannot-Install-Apps/m-p/374715#M53664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Nicholas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using ADB to install the APK?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2015 13:32:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Sololite-EVK-Board-Cannot-Install-Apps/m-p/374715#M53664</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2015-04-14T13:32:21Z</dc:date>
    </item>
  </channel>
</rss>