<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: lcd drive strength and linux device tree settings</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/lcd-drive-strength-and-linux-device-tree-settings/m-p/374503#M53642</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrew&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;correct is Quad description but next rev.2 i.MX6 Solo&lt;/P&gt;&lt;P&gt;reference manual will be updated soon.&lt;/P&gt;&lt;P&gt;Low drive makes sense since strong may cause reflections and&lt;/P&gt;&lt;P&gt;strong EMI, however this is board dependent.&lt;/P&gt;&lt;P&gt;About comments you can suggest it to yocto community:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FSL Community BSP Release Notes 1.7 documentation&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://freescale.github.io/doc/release-notes/1.7/index.html" target="_blank"&gt;http://freescale.github.io/doc/release-notes/1.7/index.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 25 Jan 2015 11:56:27 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-01-25T11:56:27Z</dc:date>
    <item>
      <title>lcd drive strength and linux device tree settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/lcd-drive-strength-and-linux-device-tree-settings/m-p/374502#M53641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was looking at an issue with our board driving our parallel LCD and noticed a couple of things:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) the speed and drive strength fields of registers like IOMUXC_SW_PAD_CTL_PAD_DI0_DISP_CLK are documented differently in the i.MX6 Solo reference manual and the i.MX6 Quad reference manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example for the Solo SPEED field it says&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5em; font-size: 10pt; font-family: terminal, monaco;"&gt;00 RESERVED0 — Reserved&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco;"&gt;01 50MHZ — Low (50 MHz)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco;"&gt;10 100MHZ — Medium (100 MHz)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco;"&gt;11 200MHZ — Maximum (200 MHz&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for the Quad it says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5em; font-size: 10pt; font-family: terminal, monaco;"&gt;00 LOW — Low frequency (50 MHz)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco;"&gt;01 MEDIUM — Medium frequency (100, 150 MHz)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco;"&gt;10 MEDIUM — Medium frequency (100, 150 MHz)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco;"&gt;11 MAXIMUM — Maximum frequency (100, 150, 200 MHz)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this something that got revised only in the Quad manual?&amp;nbsp; Are they really different?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) the device tree files for the 3.10.17 kernel set most of the LCD IO to use a value of 0x10 for the IOMIXC PAD_CTL registers.&amp;nbsp; Depending on which reference manual you read this is either an invalid value or this is a 75Ohm/3.3V driver and low speed.&amp;nbsp; This seems like a very low drive, especially for the clock.&amp;nbsp; I realize this is very board and LCD dependent, but I would suggest it would be good policy to put a note in the .dtsi file marking this as something that needs attention.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Jan 2015 03:13:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/lcd-drive-strength-and-linux-device-tree-settings/m-p/374502#M53641</guid>
      <dc:creator>andrewdyer</dc:creator>
      <dc:date>2015-01-24T03:13:05Z</dc:date>
    </item>
    <item>
      <title>Re: lcd drive strength and linux device tree settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/lcd-drive-strength-and-linux-device-tree-settings/m-p/374503#M53642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrew&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;correct is Quad description but next rev.2 i.MX6 Solo&lt;/P&gt;&lt;P&gt;reference manual will be updated soon.&lt;/P&gt;&lt;P&gt;Low drive makes sense since strong may cause reflections and&lt;/P&gt;&lt;P&gt;strong EMI, however this is board dependent.&lt;/P&gt;&lt;P&gt;About comments you can suggest it to yocto community:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FSL Community BSP Release Notes 1.7 documentation&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://freescale.github.io/doc/release-notes/1.7/index.html" target="_blank"&gt;http://freescale.github.io/doc/release-notes/1.7/index.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 25 Jan 2015 11:56:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/lcd-drive-strength-and-linux-device-tree-settings/m-p/374503#M53642</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-25T11:56:27Z</dc:date>
    </item>
  </channel>
</rss>