<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Booting issue in imx6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373872#M53535</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igorpadykov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The document you sent does not help in debugging the problem for the code hang at the time of login prompt.&lt;/P&gt;&lt;P&gt;Also we have changed the number of CPU's to 2 for Dual processor but still it reads IMX6Q id from the register.&lt;/P&gt;&lt;P&gt;We have removed all the irrelevant drivers from the code.&lt;/P&gt;&lt;P&gt;Also we have tested the code on the reference board with 256MB of DDR, on reference board it is working fine.&lt;/P&gt;&lt;P&gt;Can you provide us some other relevant document or debugging steps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adding some more information :&lt;/P&gt;&lt;P&gt;We are using yocto 1.6 Daisy tool chain with kernel 3.10-17 and u-boot-2014.01 .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Sep 2014 12:29:12 GMT</pubDate>
    <dc:creator>parveenkumaryad</dc:creator>
    <dc:date>2014-09-17T12:29:12Z</dc:date>
    <item>
      <title>Booting issue in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373868#M53531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using a board based on imx6d-sabresd reference board in our project. The only difference between our board and reference board is that we used SD2 interface for the SD card booting and UART2 for the console(ttymxc1).&lt;/P&gt;&lt;P&gt;Also we have decreased the RAM size to 256 MB from 1 GB in reference board.&lt;/P&gt;&lt;P&gt;The board always boots up but it hangs just before the login prompt but when we send an interrupt signal from keyboard(ctrl+c) login prompt comes sometimes.&lt;/P&gt;&lt;P&gt;Can anyone provide us the steps to debug the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The booting logs on the console is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2014.01 (Sep 16 2014 - 15:43:58)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6Q rev1.2 at 792 MHz &lt;SPAN style="color: #ff0000;"&gt;&amp;lt;&lt;STRONG&gt;we are using dual core processor but it is showing IMX6Q. Is there any configuration do we need to change for dual core processor&lt;/STRONG&gt;&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Reset cause: POR&lt;/P&gt;&lt;P&gt;Board: VELU_WMSD&lt;/P&gt;&lt;P&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; 256 MiB&lt;/P&gt;&lt;P&gt;usdhc3 changes for mmc1 (wifi)MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;/P&gt;&lt;P&gt;No panel detected: default to Hannstar-XGA&lt;/P&gt;&lt;P&gt;Display: Hannstar-XGA (1024x768)&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Net:&amp;nbsp;&amp;nbsp; CPU Net Initialization Failed&lt;/P&gt;&lt;P&gt;No ethernet found.&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 0 &lt;/P&gt;&lt;P&gt;mmc0 is current device&lt;/P&gt;&lt;P&gt;reading boot.scr&lt;/P&gt;&lt;P&gt;** Unable to read file boot.scr **&lt;/P&gt;&lt;P&gt;reading uImage&lt;/P&gt;&lt;P&gt;4833712 bytes read in 231 ms (20 MiB/s)&lt;/P&gt;&lt;P&gt;Booting from mmc ...&lt;/P&gt;&lt;P&gt;reading imx6q-sabresd-ldo.dtb&lt;/P&gt;&lt;P&gt;41853 bytes read in 19 ms (2.1 MiB/s)&lt;/P&gt;&lt;P&gt;## Booting kernel from Legacy Image at 12000000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Linux-3.10.17-1.0.1_ga+gdac46dc&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux Kernel Image (uncompressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 4833648 Bytes = 4.6 MiB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 10008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 10008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;## Flattened Device Tree blob at 18000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Booting using the fdt blob at 0x18000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Loading Kernel Image ... OK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Using Device Tree in place at 18000000, end 1800d37c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0x0&lt;/P&gt;&lt;P&gt;Linux version 3.10.17-1.0.1_ga+gdac46dc (alok@Alok) (gcc version 4.8.2 (GCC) ) #8 SMP PREEMPT Wed Sep 17 10:17:13 IST 2014&lt;/P&gt;&lt;P&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d&lt;/P&gt;&lt;P&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;/P&gt;&lt;P&gt;Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Quad SABRE Smart Device Board&lt;/P&gt;&lt;P&gt;Memory policy: ECC disabled, Data cache writealloc&lt;/P&gt;&lt;P&gt;PERCPU: Embedded 8 pages/cpu @80e47000 s8896 r8192 d15680 u32768&lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 65024&lt;/P&gt;&lt;P&gt;Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk0p2 rootwait rw init=/bin/sh&lt;/P&gt;&lt;P&gt;PID hash table entries: 1024 (order: 0, 4096 bytes)&lt;/P&gt;&lt;P&gt;Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;/P&gt;&lt;P&gt;Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)&lt;/P&gt;&lt;P&gt;Memory: 256MB = 256MB total&lt;/P&gt;&lt;P&gt;Memory: 247196k/247196k available, 14948k reserved, 0K highmem&lt;/P&gt;&lt;P&gt;Virtual kernel memory layout:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xfff00000 - 0xfffe0000&amp;nbsp;&amp;nbsp; ( 896 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0x90800000 - 0xff000000&amp;nbsp;&amp;nbsp; (1768 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0x80000000 - 0x90000000&amp;nbsp;&amp;nbsp; ( 256 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pkmap&amp;nbsp;&amp;nbsp; : 0x7fe00000 - 0x80000000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 2 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0x7f000000 - 0x7fe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 14 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0x80008000 - 0x80b3e8f8&amp;nbsp;&amp;nbsp; (11483 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0x80b3f000 - 0x80b7f2c0&amp;nbsp;&amp;nbsp; ( 257 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0x80b80000 - 0x80bcbe80&amp;nbsp;&amp;nbsp; ( 304 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0x80bcbe80 - 0x80c33d0c&amp;nbsp;&amp;nbsp; ( 416 kB)&lt;/P&gt;&lt;P&gt;SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1&lt;/P&gt;&lt;P&gt;Preemptible hierarchical RCU implementation.&lt;/P&gt;&lt;P&gt;NR_IRQS:16 nr_irqs:16 16&lt;/P&gt;&lt;P&gt;L310 cache controller enabled&lt;/P&gt;&lt;P&gt;l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B&lt;/P&gt;&lt;P&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms&lt;/P&gt;&lt;P&gt;CPU identified as i.MX6Q, silicon rev 1.2&lt;/P&gt;&lt;P&gt;Console: colour dummy device 80x30&lt;/P&gt;&lt;P&gt;Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)&lt;/P&gt;&lt;P&gt;pid_max: default: 32768 minimum: 301&lt;/P&gt;&lt;P&gt;Mount-cache hash table entries: 512&lt;/P&gt;&lt;P&gt;CPU: Testing write buffer coherency: ok&lt;/P&gt;&lt;P&gt;CPU0: thread -1, cpu 0, socket 0, mpidr 80000000&lt;/P&gt;&lt;P&gt;Setting up static identity map for 0x8058ff98 - 0x8058fff0&lt;/P&gt;&lt;P&gt;CPU1: Booted secondary processor&lt;/P&gt;&lt;P&gt;CPU1: thread -1, cpu 1, socket 0, mpidr 80000001&lt;/P&gt;&lt;P&gt;Brought up 2 CPUs&lt;/P&gt;&lt;P&gt;SMP: Total of 2 processors activated (3162.11 BogoMIPS).&lt;/P&gt;&lt;P&gt;CPU: All CPU(s) started in SVC mode.&lt;/P&gt;&lt;P&gt;devtmpfs: initialized&lt;/P&gt;&lt;P&gt;pinctrl core: initialized pinctrl subsystem&lt;/P&gt;&lt;P&gt;regulator-dummy: no parameters&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 16&lt;/P&gt;&lt;P&gt;DMA: preallocated 256 KiB pool for atomic coherent allocations&lt;/P&gt;&lt;P&gt;Use WDOG1 as reset source&lt;/P&gt;&lt;P&gt;syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered&lt;/P&gt;&lt;P&gt;vdd1p1: 800 &amp;lt;--&amp;gt; 1375 mV at 1125 mV &lt;/P&gt;&lt;P&gt;vdd3p0: 2800 &amp;lt;--&amp;gt; 3150 mV at 3000 mV &lt;/P&gt;&lt;P&gt;vdd2p5: 2000 &amp;lt;--&amp;gt; 2750 mV at 2425 mV &lt;/P&gt;&lt;P&gt;cpu: 725 &amp;lt;--&amp;gt; 1450 mV at 1100 mV &lt;/P&gt;&lt;P&gt;vddpu: 725 &amp;lt;--&amp;gt; 1450 mV at 1100 mV &lt;/P&gt;&lt;P&gt;vddsoc: 725 &amp;lt;--&amp;gt; 1450 mV at 1175 mV &lt;/P&gt;&lt;P&gt;syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered&lt;/P&gt;&lt;P&gt;syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered&lt;/P&gt;&lt;P&gt;hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.&lt;/P&gt;&lt;P&gt;hw-breakpoint: maximum watchpoint size is 4 bytes.&lt;/P&gt;&lt;P&gt;imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver&lt;/P&gt;&lt;P&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;/P&gt;&lt;P&gt;mxs-dma 110000.dma-apbh: initialized&lt;/P&gt;&lt;P&gt;wilink_wl_en: 1800 mV &lt;/P&gt;&lt;P&gt;usb_otg_vbus: 5000 mV &lt;/P&gt;&lt;P&gt;usb_h1_vbus: 5000 mV &lt;/P&gt;&lt;P&gt;wm8962-supply: no parameters&lt;/P&gt;&lt;P&gt;mipi_dsi_pwr_on: no parameters&lt;/P&gt;&lt;P&gt;sensor-supply: 3300 mV &lt;/P&gt;&lt;P&gt;i2c-core: driver [max17135] using legacy suspend method&lt;/P&gt;&lt;P&gt;i2c-core: driver [max17135] using legacy resume method&lt;/P&gt;&lt;P&gt;SCSI subsystem initialized&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbfs&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver hub&lt;/P&gt;&lt;P&gt;usbcore: registered new device driver usb&lt;/P&gt;&lt;P&gt;i2c i2c-0: IMX I2C adapter registered&lt;/P&gt;&lt;P&gt;i2c i2c-1: IMX I2C adapter registered&lt;/P&gt;&lt;P&gt;i2c i2c-2: IMX I2C adapter registered&lt;/P&gt;&lt;P&gt;Linux video capture interface: v2.00&lt;/P&gt;&lt;P&gt;pps_core: LinuxPPS API ver. 1 registered&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:giometti@linux.it"&gt;giometti@linux.it&lt;/A&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;PTP clock support registered&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)&lt;/P&gt;&lt;P&gt;imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)&lt;/P&gt;&lt;P&gt;mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed&lt;/P&gt;&lt;P&gt;mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a&lt;/P&gt;&lt;P&gt;MIPI CSI2 driver module loaded&lt;/P&gt;&lt;P&gt;Advanced Linux Sound Architecture Driver Initialized.&lt;/P&gt;&lt;P&gt;Switching to clocksource mxc_timer1&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 2&lt;/P&gt;&lt;P&gt;TCP established hash table entries: 2048 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;TCP bind hash table entries: 2048 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;TCP: Hash tables configured (established 2048 bind 2048)&lt;/P&gt;&lt;P&gt;TCP: reno registered&lt;/P&gt;&lt;P&gt;UDP hash table entries: 256 (order: 1, 8192 bytes)&lt;/P&gt;&lt;P&gt;UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 1&lt;/P&gt;&lt;P&gt;RPC: Registered named UNIX socket transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered udp transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered tcp transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;/P&gt;&lt;P&gt;hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available&lt;/P&gt;&lt;P&gt;pureg-dummy: no parameters&lt;/P&gt;&lt;P&gt;imx6_busfreq busfreq.15: DDR medium rate not supported.&lt;/P&gt;&lt;P&gt;Bus freq driver module loaded&lt;/P&gt;&lt;P&gt;VFS: Disk quotas dquot_6.5.2&lt;/P&gt;&lt;P&gt;Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)&lt;/P&gt;&lt;P&gt;NFS: Registering the id_resolver key type&lt;/P&gt;&lt;P&gt;Key type id_resolver registered&lt;/P&gt;&lt;P&gt;Key type id_legacy registered&lt;/P&gt;&lt;P&gt;jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.&lt;/P&gt;&lt;P&gt;fuse init (API version 7.22)&lt;/P&gt;&lt;P&gt;msgmni has been set to 482&lt;/P&gt;&lt;P&gt;io scheduler noop registered&lt;/P&gt;&lt;P&gt;io scheduler deadline registered&lt;/P&gt;&lt;P&gt;io scheduler cfq registered (default)&lt;/P&gt;&lt;P&gt;imx-weim 21b8000.weim: WEIM driver registered.&lt;/P&gt;&lt;P&gt;MIPI DSI driver module loaded&lt;/P&gt;&lt;P&gt;mxc_sdc_fb fb.31: register mxc display driver ldb&lt;/P&gt;&lt;P&gt;mxc_sdc_fb fb.31: NO mxc display driver found!&lt;/P&gt;&lt;P&gt;mxc_sdc_fb fb.32: register mxc display driver hdmi&lt;/P&gt;&lt;P&gt;mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1&lt;/P&gt;&lt;P&gt;fbcvt: 1920x1080@60: CVT Name - 2.073M9&lt;/P&gt;&lt;P&gt;Console: switching to colour frame buffer device 240x67&lt;/P&gt;&lt;P&gt;mxc_sdc_fb fb.33: register mxc display driver lcd&lt;/P&gt;&lt;P&gt;mxc_sdc_fb fb.33: ipu0-di0 already in use&lt;/P&gt;&lt;P&gt;mxc_sdc_fb: probe of fb.33 failed with error -16&lt;/P&gt;&lt;P&gt;mxc_sdc_fb fb.34: register mxc display driver ldb&lt;/P&gt;&lt;P&gt;mxc_sdc_fb fb.34: NO mxc display driver found!&lt;/P&gt;&lt;P&gt;imx-sdma 20ec000.sdma: no iram assigned, using external mem&lt;/P&gt;&lt;P&gt;imx-sdma 20ec000.sdma: loaded firmware 1.1&lt;/P&gt;&lt;P&gt;imx-sdma 20ec000.sdma: initialized&lt;/P&gt;&lt;P&gt;pfuze100-regulator 1-0008: unrecognized pfuze chip ID!&lt;/P&gt;&lt;P&gt;pfuze100-regulator: probe of 1-0008 failed with error -5&lt;/P&gt;&lt;P&gt;Serial: IMX driver&lt;/P&gt;&lt;P&gt;21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX&lt;/P&gt;&lt;P&gt;console [ttymxc1] enabled&lt;/P&gt;&lt;P&gt;serial: Freescale lpuart driver&lt;/P&gt;&lt;P&gt;[drm] Initialized drm 1.1.0 20060810&lt;/P&gt;&lt;P&gt;brd: module loaded&lt;/P&gt;&lt;P&gt;loop: module loaded&lt;/P&gt;&lt;P&gt;CAN device driver interface&lt;/P&gt;&lt;P&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usb-storage&lt;/P&gt;&lt;P&gt;ci_hdrc ci_hdrc.1: doesn't support gadget&lt;/P&gt;&lt;P&gt;ci_hdrc ci_hdrc.1: EHCI Host Controller&lt;/P&gt;&lt;P&gt;ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1&lt;/P&gt;&lt;P&gt;ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: USB hub found&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: 1 port detected&lt;/P&gt;&lt;P&gt;mousedev: PS/2 mouse device common for all mice&lt;/P&gt;&lt;P&gt;elan-touch 2-0010: elan - Read Hello Packet Failed&lt;/P&gt;&lt;P&gt;elan-touch: probe of 2-0010 failed with error -22&lt;/P&gt;&lt;P&gt;egalax_ts 2-0004: Failed to read firmware version&lt;/P&gt;&lt;P&gt;egalax_ts: probe of 2-0004 failed with error -5&lt;/P&gt;&lt;P&gt;input: max11801_ts as /devices/soc0/soc.1/2100000.aips-bus/21a4000.i2c/i2c-1/1-0048/input/input0&lt;/P&gt;&lt;P&gt;i2c-core: driver [isl29023] using legacy suspend method&lt;/P&gt;&lt;P&gt;i2c-core: driver [isl29023] using legacy resume method&lt;/P&gt;&lt;P&gt;snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0&lt;/P&gt;&lt;P&gt;i2c /dev entries driver&lt;/P&gt;&lt;P&gt;mxc_v4l2_output v4l2_out.39: V4L2 device registered as video16&lt;/P&gt;&lt;P&gt;mxc_v4l2_output v4l2_out.39: V4L2 device registered as video17&lt;/P&gt;&lt;P&gt;mag3110 2-000e: check mag3110 chip ID&lt;/P&gt;&lt;P&gt;mag3110 2-000e: read chip ID 0xfffffffb is not equal to 0xc4!&lt;/P&gt;&lt;P&gt;mag3110: probe of 2-000e failed with error -22&lt;/P&gt;&lt;P&gt;i2c-core: driver [mag3110] using legacy suspend method&lt;/P&gt;&lt;P&gt;i2c-core: driver [mag3110] using legacy resume method&lt;/P&gt;&lt;P&gt;mma8451 0-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!&lt;/P&gt;&lt;P&gt;mma8451: probe of 0-001c failed with error -22&lt;/P&gt;&lt;P&gt;imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)&lt;/P&gt;&lt;P&gt;cpuidle: using governor ladder&lt;/P&gt;&lt;P&gt;cpuidle: using governor menu&lt;/P&gt;&lt;P&gt;sdhci: Secure Digital Host Controller Interface driver&lt;/P&gt;&lt;P&gt;sdhci: Copyright(c) Pierre Ossman&lt;/P&gt;&lt;P&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;/P&gt;&lt;P&gt;mmc0: no vqmmc regulator found&lt;/P&gt;&lt;P&gt;mmc0: no vmmc regulator found&lt;/P&gt;&lt;P&gt;mmc0: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA&lt;/P&gt;&lt;P&gt;mmc0: mmc_rescan_try_freq: Trying to init card at 400000 Hz&lt;/P&gt;&lt;P&gt;sdhci-esdhc-imx 2198000.usdhc: could not get ultra high speed state, work on normal mode&lt;/P&gt;&lt;P&gt;mmc1: no vqmmc regulator found&lt;/P&gt;&lt;P&gt;mmc0: host does not support reading read-only switch. assuming write-enable.&lt;/P&gt;&lt;P&gt;mmc0: new high speed SDHC card at address aaaa&lt;/P&gt;&lt;P&gt;mmcblk0: mmc0:aaaa SU04G 3.69 GiB &lt;/P&gt;&lt;P&gt; mmcblk0: p1 p2&lt;/P&gt;&lt;P&gt;mmc1: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA&lt;/P&gt;&lt;P&gt;------------[ cut here ]------------&lt;/P&gt;&lt;P&gt;WARNING: at mm/page_alloc.c:2412 __alloc_pages_nodemask+0x180/0x7c4()&lt;/P&gt;&lt;P&gt;mmc1: mmc_rescan_try_freq: Trying to init card at 400000 Hz&lt;/P&gt;&lt;P&gt;Modules linked in:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.10.17-1.0.1_ga+gdac46dc #8&lt;/P&gt;&lt;P&gt;[&amp;lt;80013ae0&amp;gt;] (unwind_backtrace+0x0/0xf4) from [&amp;lt;80011504&amp;gt;] (show_stack+0x10/0x14)&lt;/P&gt;&lt;P&gt;[&amp;lt;80011504&amp;gt;] (show_stack+0x10/0x14) from [&amp;lt;80025d6c&amp;gt;] (warn_slowpath_common+0x54/0x6c)&lt;/P&gt;&lt;P&gt;[&amp;lt;80025d6c&amp;gt;] (warn_slowpath_common+0x54/0x6c) from [&amp;lt;80025e20&amp;gt;] (warn_slowpath_null+0x1c/0x24)&lt;/P&gt;&lt;P&gt;[&amp;lt;80025e20&amp;gt;] (warn_slowpath_null+0x1c/0x24) from [&amp;lt;8008fa48&amp;gt;] (__alloc_pages_nodemask+0x180/0x7c4)&lt;/P&gt;&lt;P&gt;[&amp;lt;8008fa48&amp;gt;] (__alloc_pages_nodemask+0x180/0x7c4) from [&amp;lt;80017b28&amp;gt;] (__dma_alloc_buffer.isra.20+0x2c/0x198)&lt;/P&gt;&lt;P&gt;[&amp;lt;80017b28&amp;gt;] (__dma_alloc_buffer.isra.20+0x2c/0x198) from [&amp;lt;80017ca8&amp;gt;] (__alloc_remap_buffer.isra.23+0x14/0xb4)&lt;/P&gt;&lt;P&gt;[&amp;lt;80017ca8&amp;gt;] (__alloc_remap_buffer.isra.23+0x14/0xb4) from [&amp;lt;80017e94&amp;gt;] (__dma_alloc+0x14c/0x25c)&lt;/P&gt;&lt;P&gt;[&amp;lt;80017e94&amp;gt;] (__dma_alloc+0x14c/0x25c) from [&amp;lt;800180e8&amp;gt;] (arm_dma_alloc+0x9c/0xa4)&lt;/P&gt;&lt;P&gt;[&amp;lt;800180e8&amp;gt;] (arm_dma_alloc+0x9c/0xa4) from [&amp;lt;8041ec38&amp;gt;] (gpu_probe+0x1d8/0x734)&lt;/P&gt;&lt;P&gt;[&amp;lt;8041ec38&amp;gt;] (gpu_probe+0x1d8/0x734) from [&amp;lt;803081b8&amp;gt;] (platform_drv_probe+0x18/0x1c)&lt;/P&gt;&lt;P&gt;[&amp;lt;803081b8&amp;gt;] (platform_drv_probe+0x18/0x1c) from [&amp;lt;80306f64&amp;gt;] (driver_probe_device+0x10c/0x228)&lt;/P&gt;&lt;P&gt;mmc1: mmc_rescan_try_freq: Trying to init card at 300000 Hz&lt;/P&gt;&lt;P&gt;[&amp;lt;80306f64&amp;gt;] (driver_probe_device+0x10c/0x228) from [&amp;lt;80307150&amp;gt;] (__driver_attach+0x8c/0x90)&lt;/P&gt;&lt;P&gt;[&amp;lt;80307150&amp;gt;] (__driver_attach+0x8c/0x90) from [&amp;lt;80305480&amp;gt;] (bus_for_each_dev+0x60/0x94)&lt;/P&gt;&lt;P&gt;[&amp;lt;80305480&amp;gt;] (bus_for_each_dev+0x60/0x94) from [&amp;lt;80306728&amp;gt;] (bus_add_driver+0x1c0/0x24c)&lt;/P&gt;&lt;P&gt;[&amp;lt;80306728&amp;gt;] (bus_add_driver+0x1c0/0x24c) from [&amp;lt;8030772c&amp;gt;] (driver_register+0x78/0x140)&lt;/P&gt;&lt;P&gt;[&amp;lt;8030772c&amp;gt;] (driver_register+0x78/0x140) from [&amp;lt;80008704&amp;gt;] (do_one_initcall+0x108/0x158)&lt;/P&gt;&lt;P&gt;[&amp;lt;80008704&amp;gt;] (do_one_initcall+0x108/0x158) from [&amp;lt;80b3fbe0&amp;gt;] (kernel_init_freeable+0x138/0x1d8)&lt;/P&gt;&lt;P&gt;[&amp;lt;80b3fbe0&amp;gt;] (kernel_init_freeable+0x138/0x1d8) from [&amp;lt;80584b9c&amp;gt;] (kernel_init+0x8/0x158)&lt;/P&gt;&lt;P&gt;[&amp;lt;80584b9c&amp;gt;] (kernel_init+0x8/0x158) from [&amp;lt;8000e118&amp;gt;] (ret_from_fork+0x14/0x3c)&lt;/P&gt;&lt;P&gt;---[ end trace af522e87092d768d ]---&lt;/P&gt;&lt;P&gt;galcore 130000.gpu: Failed to allocate contiguous memory&lt;/P&gt;&lt;P&gt;galcore: probe of 130000.gpu failed with error -12&lt;/P&gt;&lt;P&gt;mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed&lt;/P&gt;&lt;P&gt;mxc_asrc 2034000.asrc: mxc_asrc registered&lt;/P&gt;&lt;P&gt;mxc_vpu 2040000.vpu: VPU initialized&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbhid&lt;/P&gt;&lt;P&gt;usbhid: USB HID core driver&lt;/P&gt;&lt;P&gt;i2c-core: driver [cs42888] using legacy suspend method&lt;/P&gt;&lt;P&gt;i2c-core: driver [cs42888] using legacy resume method&lt;/P&gt;&lt;P&gt;mmc1: mmc_rescan_try_freq: Trying to init card at 200000 Hz&lt;/P&gt;&lt;P&gt;wm8962 0-001a: Failed to read ID register&lt;/P&gt;&lt;P&gt;wm8962: probe of 0-001a failed with error -5&lt;/P&gt;&lt;P&gt;imx-wm8962 sound.29: audmux internal port setup failed&lt;/P&gt;&lt;P&gt;imx-wm8962: probe of sound.29 failed with error -22&lt;/P&gt;&lt;P&gt;imx-audio-hdmi sound-hdmi.30:&amp;nbsp; hdmi-hifi &amp;lt;-&amp;gt; hdmi_audio.16 mapping ok&lt;/P&gt;&lt;P&gt;TCP: cubic registered&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 10&lt;/P&gt;&lt;P&gt;sit: IPv6 over IPv4 tunneling driver&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 17&lt;/P&gt;&lt;P&gt;can: controller area network core (rev 20120528 abi 9)&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 29&lt;/P&gt;&lt;P&gt;can: raw protocol (rev 20120528)&lt;/P&gt;&lt;P&gt;can: broadcast manager protocol (rev 20120528 t)&lt;/P&gt;&lt;P&gt;can: netlink gateway (rev 20130117) max_hops=1&lt;/P&gt;&lt;P&gt;8021q: 802.1Q VLAN Support v1.8&lt;/P&gt;&lt;P&gt;Key type dns_resolver registered&lt;/P&gt;&lt;P&gt;VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4&lt;/P&gt;&lt;P&gt;vddpu: disabling&lt;/P&gt;&lt;P&gt;snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)&lt;/P&gt;&lt;P&gt;ALSA device list:&lt;/P&gt;&lt;P&gt;&amp;nbsp; #0: imx-hdmi-soc&lt;/P&gt;&lt;P&gt;kjournald starting.&amp;nbsp; Commit interval 5 seconds&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p2): using internal journal&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p2): recovery complete&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode&lt;/P&gt;&lt;P&gt;VFS: Mounted root (ext3 filesystem) on device 179:2.&lt;/P&gt;&lt;P&gt;devtmpfs: mounted&lt;/P&gt;&lt;P&gt;Freeing unused kernel memory: 256K (80b3f000 - 80b7f000)&lt;/P&gt;&lt;P&gt;mmc1: mmc_rescan_try_freq: Trying to init card at 100000 Hz&lt;/P&gt;&lt;P&gt;udevd[122]: starting version 182 &lt;/P&gt;&lt;P&gt;Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory &lt;/P&gt;&lt;P&gt;bootlogd. &lt;/P&gt;&lt;P&gt;Populating dev cache &lt;/P&gt;&lt;P&gt;Wed Sep 17 05:10:00 UTC 2014&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="color: #ff0000;"&gt;&amp;lt;console hangs here&amp;gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2014 06:27:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373868#M53531</guid>
      <dc:creator>parveenkumaryad</dc:creator>
      <dc:date>2014-09-17T06:27:11Z</dc:date>
    </item>
    <item>
      <title>Re: Booting issue in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373869#M53532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Parveen&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can try to allocate to gpu reasonable memory&lt;/P&gt;&lt;P&gt;with parameter "mem" and set "maxcpus"=2 for Dual processor&lt;/P&gt;&lt;P&gt;as shown in attached document p.9.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2014 08:41:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373869#M53532</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-09-17T08:41:17Z</dc:date>
    </item>
    <item>
      <title>Re: Booting issue in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373870#M53533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igorpadykov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you forgot to attach the document...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2014 09:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373870#M53533</guid>
      <dc:creator>parveenkumaryad</dc:creator>
      <dc:date>2014-09-17T09:19:39Z</dc:date>
    </item>
    <item>
      <title>Re: Booting issue in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373871#M53534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i.MX_6_SABRE-SD_Linux_Release_Notes.pdf&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.0_LINUX_DOCS&amp;amp;appType=license&amp;amp;location=null&amp;amp;fasp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz"&gt;L3.10.17_1.0.0_LINUX_DOCS&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2014 09:59:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373871#M53534</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-09-17T09:59:52Z</dc:date>
    </item>
    <item>
      <title>Re: Booting issue in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373872#M53535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igorpadykov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The document you sent does not help in debugging the problem for the code hang at the time of login prompt.&lt;/P&gt;&lt;P&gt;Also we have changed the number of CPU's to 2 for Dual processor but still it reads IMX6Q id from the register.&lt;/P&gt;&lt;P&gt;We have removed all the irrelevant drivers from the code.&lt;/P&gt;&lt;P&gt;Also we have tested the code on the reference board with 256MB of DDR, on reference board it is working fine.&lt;/P&gt;&lt;P&gt;Can you provide us some other relevant document or debugging steps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adding some more information :&lt;/P&gt;&lt;P&gt;We are using yocto 1.6 Daisy tool chain with kernel 3.10-17 and u-boot-2014.01 .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2014 12:29:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373872#M53535</guid>
      <dc:creator>parveenkumaryad</dc:creator>
      <dc:date>2014-09-17T12:29:12Z</dc:date>
    </item>
    <item>
      <title>Re: Booting issue in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373873#M53536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We were able to boot the board after few menuconfig changes.&lt;/P&gt;&lt;P&gt;We disabled the RTC clock and made some changes in power management in the menuconfig and after that we were able to boot the board without hanging issue in the kernel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Sep 2014 10:37:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373873#M53536</guid>
      <dc:creator>parveenkumaryad</dc:creator>
      <dc:date>2014-09-18T10:37:22Z</dc:date>
    </item>
    <item>
      <title>Re: Booting issue in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373874#M53537</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Praveen,&lt;/P&gt;&lt;P&gt;What are the power management changes which you have done in make menuconfig?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Nov 2015 06:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373874#M53537</guid>
      <dc:creator>JithCR</dc:creator>
      <dc:date>2015-11-03T06:26:48Z</dc:date>
    </item>
    <item>
      <title>Re: Booting issue in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373875#M53538</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi PRaveen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are also facing same issue, please let us know the power management changes which you have done in make menuconfig.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Nov 2015 08:33:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373875#M53538</guid>
      <dc:creator>ambika</dc:creator>
      <dc:date>2015-11-04T08:33:22Z</dc:date>
    </item>
    <item>
      <title>Re: Booting issue in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373876#M53539</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If the problem is reproduced only with DDR50 SD cards (e.g. like one above Sandisk SE16G, which RCA is aaaa), I believe the described problem may be related to a missing timing delay after host controller timing switch, see Dong Aisheng's change ENGR00324668 as a workaround.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2016 10:14:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-in-imx6/m-p/373876#M53539</guid>
      <dc:creator>vladimirzapolsk</dc:creator>
      <dc:date>2016-01-15T10:14:19Z</dc:date>
    </item>
  </channel>
</rss>