<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックDDR3 Write Leveling</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Write-Leveling/m-p/373378#M53437</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; What the conditions will we use the DDR3 Write Leveling features？we dont know why we need to fix the following Data pin ,in other word, D0 is connected to DRAM_D8 not DRAM_D0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 12.0pt;"&gt;FSL review command as below:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 12.0pt;"&gt;==============================================================&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The review was finished. One comment about DDR3 data swapping of the review,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hardware write leveling – lowest order bit within byte lane must remain on lowest order bit of lane&lt;/P&gt;&lt;P&gt;by JEDEC compliance (see the “Write Leveling” section in JESD79-3E)&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 宋体;"&gt;—&lt;/SPAN&gt; D0, D8, D16, D24, D32, D40, D48, and D56 are fixed&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 宋体;"&gt;—&lt;/SPAN&gt; Other data lines free to swap within byte lane&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, DQ0 of U3 should connect to net-label DRAM_D8.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Apr 2015 11:32:18 GMT</pubDate>
    <dc:creator>tony_l_cai</dc:creator>
    <dc:date>2015-04-02T11:32:18Z</dc:date>
    <item>
      <title>DDR3 Write Leveling</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Write-Leveling/m-p/373378#M53437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; What the conditions will we use the DDR3 Write Leveling features？we dont know why we need to fix the following Data pin ,in other word, D0 is connected to DRAM_D8 not DRAM_D0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 12.0pt;"&gt;FSL review command as below:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 12.0pt;"&gt;==============================================================&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The review was finished. One comment about DDR3 data swapping of the review,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hardware write leveling – lowest order bit within byte lane must remain on lowest order bit of lane&lt;/P&gt;&lt;P&gt;by JEDEC compliance (see the “Write Leveling” section in JESD79-3E)&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 宋体;"&gt;—&lt;/SPAN&gt; D0, D8, D16, D24, D32, D40, D48, and D56 are fixed&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 宋体;"&gt;—&lt;/SPAN&gt; Other data lines free to swap within byte lane&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, DQ0 of U3 should connect to net-label DRAM_D8.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2015 11:32:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Write-Leveling/m-p/373378#M53437</guid>
      <dc:creator>tony_l_cai</dc:creator>
      <dc:date>2015-04-02T11:32:18Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Write Leveling</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-Write-Leveling/m-p/373379#M53438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please look at section 11 (Write Leveling) of app note AN4467.&lt;/P&gt;&lt;P&gt;"i.MX 6 Series DDR Calibration"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/app_note/AN4467.pdf" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4467.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2015 11:51:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-Write-Leveling/m-p/373379#M53438</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-04-02T11:51:52Z</dc:date>
    </item>
  </channel>
</rss>