<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 i.MX6 8 bit Parallel Camera to 20 Bit CSI mapping</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-8-bit-Parallel-Camera-to-20-Bit-CSI-mapping/m-p/372905#M53340</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hopefully a simple question, but I can't seem to find a concise answer.&amp;nbsp; Simply put, when mapping an 8 bit parallel gray scale sensor to the 20 bit parallel CSI port, what are the mapping options.&amp;nbsp; I see the SDB board uses the top 8 bits (D12:D19) of the CSI port.&amp;nbsp; I recall reading somewhere that the next 8 bits down (D4:D11) are also supported.&amp;nbsp; I think I've also seen the low 8 bits used. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just want to capture a byte oriented frame buffer without any overhead so I want to be sure I pick a mapping that doesn't force me to capture 16 or 32 bit words.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I assume whatever mapping restrictions there are they are the same for all i.MX6?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Oct 2014 14:26:11 GMT</pubDate>
    <dc:creator>DavidLundquist</dc:creator>
    <dc:date>2014-10-07T14:26:11Z</dc:date>
    <item>
      <title>i.MX6 8 bit Parallel Camera to 20 Bit CSI mapping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-8-bit-Parallel-Camera-to-20-Bit-CSI-mapping/m-p/372905#M53340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hopefully a simple question, but I can't seem to find a concise answer.&amp;nbsp; Simply put, when mapping an 8 bit parallel gray scale sensor to the 20 bit parallel CSI port, what are the mapping options.&amp;nbsp; I see the SDB board uses the top 8 bits (D12:D19) of the CSI port.&amp;nbsp; I recall reading somewhere that the next 8 bits down (D4:D11) are also supported.&amp;nbsp; I think I've also seen the low 8 bits used. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just want to capture a byte oriented frame buffer without any overhead so I want to be sure I pick a mapping that doesn't force me to capture 16 or 32 bit words.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I assume whatever mapping restrictions there are they are the same for all i.MX6?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2014 14:26:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-8-bit-Parallel-Camera-to-20-Bit-CSI-mapping/m-p/372905#M53340</guid>
      <dc:creator>DavidLundquist</dc:creator>
      <dc:date>2014-10-07T14:26:11Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 8 bit Parallel Camera to 20 Bit CSI mapping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-8-bit-Parallel-Camera-to-20-Bit-CSI-mapping/m-p/372906#M53341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;only supported formats are given in&lt;/P&gt;&lt;P&gt;Table 66. Camera Input Signal Cross Reference, Format, and Bits Per Cycle&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQCEC&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From sect.37.4.3.2.1 Parallel Interface &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQRM&lt;/A&gt; :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"..according to configuration of DATA_WIDTH. If DATA_WIDTH is configured to N,&lt;/P&gt;&lt;P&gt;then 20-N LSB bits are ignored."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2014 23:42:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-8-bit-Parallel-Camera-to-20-Bit-CSI-mapping/m-p/372906#M53341</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-07T23:42:12Z</dc:date>
    </item>
  </channel>
</rss>