<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6 without linux OS</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-without-linux-OS/m-p/372664#M53299</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use imx6_platform_sdk_v1.1.0. for your requirement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Oct 2014 12:42:04 GMT</pubDate>
    <dc:creator>saurabh206</dc:creator>
    <dc:date>2014-10-07T12:42:04Z</dc:date>
    <item>
      <title>imx6 without linux OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-without-linux-OS/m-p/372663#M53298</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to run a small custom boot application on the imx6, with for example a main loop. &lt;/P&gt;&lt;P&gt;And not a linux distribution as OS. So I have full control over the Firmware that is running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to use the imx6 in an aviation application. For that reason the firmware running on the device needs to be certified and a LINUX distro is not certified.&lt;/P&gt;&lt;P&gt;So is it possible to boot the imx6 without an thirdparty OS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2014 12:13:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-without-linux-OS/m-p/372663#M53298</guid>
      <dc:creator>peterc</dc:creator>
      <dc:date>2014-10-07T12:13:21Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 without linux OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-without-linux-OS/m-p/372664#M53299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use imx6_platform_sdk_v1.1.0. for your requirement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2014 12:42:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-without-linux-OS/m-p/372664#M53299</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-10-07T12:42:04Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 without linux OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-without-linux-OS/m-p/372665#M53300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;its bare metal but yes, the SDK is your option:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Under "Software Development Tools" &amp;gt;&amp;gt; Software development kits"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2014 14:36:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-without-linux-OS/m-p/372665#M53300</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2014-10-07T14:36:45Z</dc:date>
    </item>
  </channel>
</rss>