<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Way to fast peripheral input? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Way-to-fast-peripheral-input/m-p/372012#M53166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQRM&lt;/A&gt; &lt;/P&gt;&lt;P&gt;i.MX 6Dual/6Quad Applications Processor Reference Manual&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Jan 2015 11:00:52 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-01-30T11:00:52Z</dc:date>
    <item>
      <title>Way to fast peripheral input?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Way-to-fast-peripheral-input/m-p/372009#M53163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello. I need the way to input from 7MHz parallel data stream (&amp;gt;7MByte per second) to i.MX6Q. &lt;/P&gt;&lt;P&gt;As I've heard there is no way to make GPIO work on such high frequencies on Linux. Maybe you can advice another, faster interface, that can do such high frequencies?&lt;/P&gt;&lt;P&gt;I am thinking about using USB on 480MHz speed, but i can not find fast enough multiplexer from gpio to usb.&lt;BR /&gt;Also memory sharing, but it will be not an easy issue for DDR3.&lt;/P&gt;&lt;P&gt;Maybe there is another, faster way without excessive difficulties? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 10:58:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Way-to-fast-peripheral-input/m-p/372009#M53163</guid>
      <dc:creator>olegpereverzev</dc:creator>
      <dc:date>2015-01-23T10:58:32Z</dc:date>
    </item>
    <item>
      <title>Re: Way to fast peripheral input?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Way-to-fast-peripheral-input/m-p/372010#M53164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oleg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can consider IPU CSI interface, probably using fpga for&lt;/P&gt;&lt;P&gt;providing necessary waveforms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 12:53:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Way-to-fast-peripheral-input/m-p/372010#M53164</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-23T12:53:51Z</dc:date>
    </item>
    <item>
      <title>Re: Way to fast peripheral input?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Way-to-fast-peripheral-input/m-p/372011#M53165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. Thaks, but I though it translates data straight into IPU, so it can be video/photo from camera only. Or there is a way to save it somewhere in memory before it hits IPU, or make IPU work as a dummy that will translate bytes unconverted to some memory address? Where my programmer can read about such things?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jan 2015 10:38:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Way-to-fast-peripheral-input/m-p/372011#M53165</guid>
      <dc:creator>olegpereverzev</dc:creator>
      <dc:date>2015-01-30T10:38:26Z</dc:date>
    </item>
    <item>
      <title>Re: Way to fast peripheral input?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Way-to-fast-peripheral-input/m-p/372012#M53166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQRM&lt;/A&gt; &lt;/P&gt;&lt;P&gt;i.MX 6Dual/6Quad Applications Processor Reference Manual&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jan 2015 11:00:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Way-to-fast-peripheral-input/m-p/372012#M53166</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-30T11:00:52Z</dc:date>
    </item>
  </channel>
</rss>