<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Avoiding cross-compilation</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Avoiding-cross-compilation/m-p/371833#M53099</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with the i.mx53 Quick Start Board. To speed up development, I would like to be able to compile directly on the board, instead of cross-compiling on a computer then transferring the program.&lt;/P&gt;&lt;P&gt;On the provided Ubuntu image, generic programs compile and work, but the libraries for using the hardware (such as SPI) don't seem to be installed. Any idea where to find them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have also found advice about trying Linaro, but it seems all links to their hardware packages for i.mx53 are now dead.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Nov 2014 08:51:26 GMT</pubDate>
    <dc:creator>bogdanbeju</dc:creator>
    <dc:date>2014-11-26T08:51:26Z</dc:date>
    <item>
      <title>Avoiding cross-compilation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Avoiding-cross-compilation/m-p/371833#M53099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with the i.mx53 Quick Start Board. To speed up development, I would like to be able to compile directly on the board, instead of cross-compiling on a computer then transferring the program.&lt;/P&gt;&lt;P&gt;On the provided Ubuntu image, generic programs compile and work, but the libraries for using the hardware (such as SPI) don't seem to be installed. Any idea where to find them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have also found advice about trying Linaro, but it seems all links to their hardware packages for i.mx53 are now dead.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Nov 2014 08:51:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Avoiding-cross-compilation/m-p/371833#M53099</guid>
      <dc:creator>bogdanbeju</dc:creator>
      <dc:date>2014-11-26T08:51:26Z</dc:date>
    </item>
    <item>
      <title>Re: Avoiding cross-compilation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Avoiding-cross-compilation/m-p/371834#M53100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can find some libraries on host machine in /opt/freescale/pkgs/imx-lib-*.tar.gz&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;I hope it is what you need.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Nov 2014 09:35:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Avoiding-cross-compilation/m-p/371834#M53100</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2014-11-26T09:35:22Z</dc:date>
    </item>
    <item>
      <title>Re: Avoiding cross-compilation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Avoiding-cross-compilation/m-p/371835#M53101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did check out imx-lib-*. Unfortunately it only contains some specialized libraries, such as for using the VPU. The parts for using GPIO for example are not there.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Nov 2014 12:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Avoiding-cross-compilation/m-p/371835#M53101</guid>
      <dc:creator>bogdanbeju</dc:creator>
      <dc:date>2014-11-26T12:18:30Z</dc:date>
    </item>
  </channel>
</rss>